<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Motor Control Software on RT1064 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Motor-Control-Software-on-RT1064/m-p/1238192#M170170</link>
    <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;When I’m trying to create my SDK in MCUExpresso SDK Builder, the “Motor Control Software” is not available as an option. However, it is supported for the RT1062. Are there any differences between the two processors here that I have missed? Is the Motor Control Software not supported for RT1064, and in that case why?&lt;/P&gt;</description>
    <pubDate>Mon, 01 Mar 2021 20:58:16 GMT</pubDate>
    <dc:creator>Carlio</dc:creator>
    <dc:date>2021-03-01T20:58:16Z</dc:date>
    <item>
      <title>Motor Control Software on RT1064</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Motor-Control-Software-on-RT1064/m-p/1238192#M170170</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;When I’m trying to create my SDK in MCUExpresso SDK Builder, the “Motor Control Software” is not available as an option. However, it is supported for the RT1062. Are there any differences between the two processors here that I have missed? Is the Motor Control Software not supported for RT1064, and in that case why?&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 20:58:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Motor-Control-Software-on-RT1064/m-p/1238192#M170170</guid>
      <dc:creator>Carlio</dc:creator>
      <dc:date>2021-03-01T20:58:16Z</dc:date>
    </item>
    <item>
      <title>Re: Motor Control Software on RT1064</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Motor-Control-Software-on-RT1064/m-p/1239731#M170307</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/183977"&gt;@Carlio&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I also think that this middleware should be able for both MCUs, let me check internally if there's a reason that this software is missing.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Wed, 03 Mar 2021 22:23:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Motor-Control-Software-on-RT1064/m-p/1239731#M170307</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2021-03-03T22:23:40Z</dc:date>
    </item>
    <item>
      <title>Re: Motor Control Software on RT1064</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Motor-Control-Software-on-RT1064/m-p/1240672#M170376</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/183977"&gt;@Carlio&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Meanwhile, you can use any of the motor control examples found in the SDK for the RT1060 in the RT1064.&lt;/P&gt;</description>
      <pubDate>Fri, 05 Mar 2021 03:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Motor-Control-Software-on-RT1064/m-p/1240672#M170376</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2021-03-05T03:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: Motor Control Software on RT1064</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Motor-Control-Software-on-RT1064/m-p/1241014#M170423</link>
      <description>&lt;P&gt;Thank you&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167559"&gt;@Alexis_A&lt;/a&gt;&amp;nbsp;! Will do.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Mar 2021 13:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Motor-Control-Software-on-RT1064/m-p/1241014#M170423</guid>
      <dc:creator>Carlio</dc:creator>
      <dc:date>2021-03-05T13:15:32Z</dc:date>
    </item>
  </channel>
</rss>