<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックGPT DBGEN Bit</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GPT-DBGEN-Bit/m-p/1238160#M170169</link>
    <description>&lt;P&gt;According to iMX8QM_RM_Rev_E Section 7.10.4.2.5:&lt;BR /&gt;If DBGEN bit is not set for GPT_CR register then GPT timer is halted.&lt;BR /&gt;But in my case GPT Timer counter continue running even though DBGEN is 0 and code execution is stopped using debugger.&amp;nbsp;&lt;BR /&gt;What could be the reason?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 01 Mar 2021 19:05:25 GMT</pubDate>
    <dc:creator>sohaib_sulehri</dc:creator>
    <dc:date>2021-03-01T19:05:25Z</dc:date>
    <item>
      <title>GPT DBGEN Bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPT-DBGEN-Bit/m-p/1238160#M170169</link>
      <description>&lt;P&gt;According to iMX8QM_RM_Rev_E Section 7.10.4.2.5:&lt;BR /&gt;If DBGEN bit is not set for GPT_CR register then GPT timer is halted.&lt;BR /&gt;But in my case GPT Timer counter continue running even though DBGEN is 0 and code execution is stopped using debugger.&amp;nbsp;&lt;BR /&gt;What could be the reason?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 19:05:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPT-DBGEN-Bit/m-p/1238160#M170169</guid>
      <dc:creator>sohaib_sulehri</dc:creator>
      <dc:date>2021-03-01T19:05:25Z</dc:date>
    </item>
    <item>
      <title>Re: GPT DBGEN Bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPT-DBGEN-Bit/m-p/1333817#M179483</link>
      <description>&lt;P&gt;In debug mode, PWM has the option of continuing to run or be halted.&lt;BR /&gt;If the DBGEN bit is not set in the PWM_PWMCR, the PWM is halted.&lt;BR /&gt;If the DBGEN bit is set, then the PWM will continue to run in the debug mode.&lt;/P&gt;</description>
      <pubDate>Thu, 02 Sep 2021 05:24:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPT-DBGEN-Bit/m-p/1333817#M179483</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2021-09-02T05:24:20Z</dc:date>
    </item>
  </channel>
</rss>