<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: J-Link Interface and IMX8QM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/J-Link-Interface-and-IMX8QM/m-p/1237983#M170158</link>
    <description>&lt;P&gt;I found that there is already a pending Patch for imx8qm config. Which is until now not on the mainline openocd.&lt;/P&gt;&lt;P&gt;&lt;A href="http://openocd.zylin.com/#/c/5042/1/tcl/target/imx8qm.cfg" target="_blank" rel="noopener"&gt;http://openocd.zylin.com/#/c/5042/1/tcl/target/imx8qm.cfg&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Using that patch and with a few modifications in nxp_mcimx8m-evk.cfg it is working for me.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;</description>
    <pubDate>Mon, 01 Mar 2021 13:54:33 GMT</pubDate>
    <dc:creator>olivergraute</dc:creator>
    <dc:date>2021-03-01T13:54:33Z</dc:date>
    <item>
      <title>J-Link Interface and IMX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/J-Link-Interface-and-IMX8QM/m-p/1229903#M169389</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I got an J-Link Base Adapter from Segger and I would like to check if the JTAG Interface on the IMX8QM is working. Is there some Documentation how to use a J-LINK Adapter on IMX8QM with such an Adapter?&lt;/P&gt;&lt;P&gt;Further I want to disable JTAG by fusing the fuses and verify if that operation truely disabled the JTAG Interface.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/How-to-disable-USB-and-JTAG-by-fuses-on-IMX8QM/td-p/1186024" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/How-to-disable-USB-and-JTAG-by-fuses-on-IMX8QM/td-p/1186024&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;</description>
      <pubDate>Thu, 11 Feb 2021 14:02:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/J-Link-Interface-and-IMX8QM/m-p/1229903#M169389</guid>
      <dc:creator>olivergraute</dc:creator>
      <dc:date>2021-02-11T14:02:21Z</dc:date>
    </item>
    <item>
      <title>Re: J-Link Interface and IMX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/J-Link-Interface-and-IMX8QM/m-p/1232433#M169635</link>
      <description>&lt;P&gt;Hello, &lt;BR /&gt;&lt;BR /&gt;For the i.MX8QM the JTAG debugger tested are:&lt;BR /&gt;Cortex-M -&amp;gt; Lauterbatch/J-LINK plus&lt;BR /&gt;Cortex-A -&amp;gt; Lauterbatch/DSStream&lt;BR /&gt;&lt;BR /&gt;You may also refer to the following guide:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12631.pdf" target="_blank"&gt;Normal and Secure Debug for i.MX8/8X Family of Applications Processors&amp;nbsp;&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 01:46:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/J-Link-Interface-and-IMX8QM/m-p/1232433#M169635</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-02-18T01:46:33Z</dc:date>
    </item>
    <item>
      <title>Re: J-Link Interface and IMX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/J-Link-Interface-and-IMX8QM/m-p/1232797#M169661</link>
      <description>&lt;P&gt;Unfortunately I don't have access to the Lauterbach software.&lt;/P&gt;&lt;P&gt;I would like to the use the free and open source software "openocd" instead.&lt;/P&gt;&lt;P&gt;But until now there is no support for imx8qm. As far as I oversee this there is missing some board/target configuration files for imx8qm.&lt;/P&gt;&lt;P&gt;Is it possible that NXP can provide the necessary informations that we can try to&amp;nbsp; implement this in openocd?&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 10:45:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/J-Link-Interface-and-IMX8QM/m-p/1232797#M169661</guid>
      <dc:creator>olivergraute</dc:creator>
      <dc:date>2021-02-18T10:45:49Z</dc:date>
    </item>
    <item>
      <title>Re: J-Link Interface and IMX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/J-Link-Interface-and-IMX8QM/m-p/1237983#M170158</link>
      <description>&lt;P&gt;I found that there is already a pending Patch for imx8qm config. Which is until now not on the mainline openocd.&lt;/P&gt;&lt;P&gt;&lt;A href="http://openocd.zylin.com/#/c/5042/1/tcl/target/imx8qm.cfg" target="_blank" rel="noopener"&gt;http://openocd.zylin.com/#/c/5042/1/tcl/target/imx8qm.cfg&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Using that patch and with a few modifications in nxp_mcimx8m-evk.cfg it is working for me.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 13:54:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/J-Link-Interface-and-IMX8QM/m-p/1237983#M170158</guid>
      <dc:creator>olivergraute</dc:creator>
      <dc:date>2021-03-01T13:54:33Z</dc:date>
    </item>
  </channel>
</rss>