<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCIe Endpoint Doorbell or Interrupt in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-Endpoint-Doorbell-or-Interrupt/m-p/1237893#M170147</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;The following discussion - hope - helps.&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Endpoint-Interrupt-via-PCIe/m-p/250595" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Endpoint-Interrupt-via-PCIe/m-p/250595&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 01 Mar 2021 10:14:45 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2021-03-01T10:14:45Z</dc:date>
    <item>
      <title>PCIe Endpoint Doorbell or Interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-Endpoint-Doorbell-or-Interrupt/m-p/476070#M75507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is common for a PCIe add-in card to have a "doorbell" register or similar functionality (eg, a queue tail pointer) that the host system can write to start an I/O operation.&amp;nbsp; I haven't found a way to trigger an ARM interrupt as a result of an inbound PCIe write transaction with the i.MX6 operating in endpoint mode.&amp;nbsp; I'm currently stuck polling on memory locations which is a really ugly solution.&amp;nbsp; Is there a way to implement this type of behavior that doesn't rely on polling?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Carl&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jan 2016 17:43:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-Endpoint-Doorbell-or-Interrupt/m-p/476070#M75507</guid>
      <dc:creator>carlpii</dc:creator>
      <dc:date>2016-01-29T17:43:13Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe Endpoint Doorbell or Interrupt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIe-Endpoint-Doorbell-or-Interrupt/m-p/1237893#M170147</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;The following discussion - hope - helps.&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Endpoint-Interrupt-via-PCIe/m-p/250595" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Endpoint-Interrupt-via-PCIe/m-p/250595&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 10:14:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIe-Endpoint-Doorbell-or-Interrupt/m-p/1237893#M170147</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-03-01T10:14:45Z</dc:date>
    </item>
  </channel>
</rss>