<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to modify the IMX8 Android's default resolution(the default value in Physical size of 'wm si in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-modify-the-IMX8-Android-s-default-resolution-the-default/m-p/1237590#M170118</link>
    <description>&lt;P&gt;You may need to change the default resolution in the bootargs. Please refer to the Chapter 6.2 and 8.1 in the Android User's Guide for more details.&lt;/P&gt;</description>
    <pubDate>Sun, 28 Feb 2021 19:56:35 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2021-02-28T19:56:35Z</dc:date>
    <item>
      <title>How to modify the IMX8 Android's default resolution(the default value in Physical size of 'wm size')</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-modify-the-IMX8-Android-s-default-resolution-the-default/m-p/1237106#M170056</link>
      <description>&lt;P&gt;We're running Andorid9 on IMX8mini, the default resolution is 1920x1080, we want to let this default to 1280x720&lt;/P&gt;&lt;P&gt;We already knew this can be done by 'wm size 1280x720', or use overlay. Both of these methods are for overlay way, i.e, when I execute 'wm size', it would show the Physical size is not changed:&lt;/P&gt;&lt;P&gt;# wm size&lt;BR /&gt;Physical size: 1920x1080&lt;BR /&gt;Override size: 1280x720&lt;/P&gt;&lt;P&gt;When I execute 'wm size reset', it would go back to the original 1920x1080.&lt;/P&gt;&lt;P&gt;So, I want to let the Physical size be 1280x720, can anyone help me? Because all what I searched are the 'wm size xxxxxx', this is not what I wanted.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Feb 2021 07:21:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-modify-the-IMX8-Android-s-default-resolution-the-default/m-p/1237106#M170056</guid>
      <dc:creator>13614278</dc:creator>
      <dc:date>2021-02-26T07:21:28Z</dc:date>
    </item>
    <item>
      <title>Re: How to modify the IMX8 Android's default resolution(the default value in Physical size of 'wm si</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-modify-the-IMX8-Android-s-default-resolution-the-default/m-p/1237590#M170118</link>
      <description>&lt;P&gt;You may need to change the default resolution in the bootargs. Please refer to the Chapter 6.2 and 8.1 in the Android User's Guide for more details.&lt;/P&gt;</description>
      <pubDate>Sun, 28 Feb 2021 19:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-modify-the-IMX8-Android-s-default-resolution-the-default/m-p/1237590#M170118</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2021-02-28T19:56:35Z</dc:date>
    </item>
  </channel>
</rss>