<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX8MPlus crashes during video streaming</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-crashes-during-video-streaming/m-p/1234582#M169833</link>
    <description>&lt;P&gt;Hello Alex,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1) From the log looks like the original source video(video-from-imx8mm.avi ) is already h264 then whey it is being decoded and then encoded again to h264 ?&lt;/P&gt;
&lt;P&gt;2) If there is a real need to decode and encode change decodebin to vpudec. As decodebin will not use the HW acceleration and rather use the CPU&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 22 Feb 2021 21:07:33 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2021-02-22T21:07:33Z</dc:date>
    <item>
      <title>i.MX8MPlus crashes during video streaming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-crashes-during-video-streaming/m-p/1232902#M169670</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using&amp;nbsp;NXP i.MX8MPlus LPDDR4 EVK board with&amp;nbsp;5.4.70-2.3.0+g4f2631b022d8 BSP.&lt;/P&gt;&lt;P&gt;1. Streaming a video file with HW acceleration via gstreamer constantly causes a process stall. The stall can be recovered only by resetting the board. See an attached imx_stall.log&lt;/P&gt;&lt;P&gt;2. After changing the caps parameters and trying to stream once more, the target OS has crashed and could be recovered only by the HW reset. See attached *_crash.log&lt;/P&gt;&lt;P&gt;* Video files captured from the WebCam on the same board don't cause any issues.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 14:13:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-crashes-during-video-streaming/m-p/1232902#M169670</guid>
      <dc:creator>Alex_Sh</dc:creator>
      <dc:date>2021-02-18T14:13:14Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MPlus crashes during video streaming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-crashes-during-video-streaming/m-p/1234582#M169833</link>
      <description>&lt;P&gt;Hello Alex,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1) From the log looks like the original source video(video-from-imx8mm.avi ) is already h264 then whey it is being decoded and then encoded again to h264 ?&lt;/P&gt;
&lt;P&gt;2) If there is a real need to decode and encode change decodebin to vpudec. As decodebin will not use the HW acceleration and rather use the CPU&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 21:07:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MPlus-crashes-during-video-streaming/m-p/1234582#M169833</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-02-22T21:07:33Z</dc:date>
    </item>
  </channel>
</rss>