<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic kobs-ng parameters in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/kobs-ng-parameters/m-p/1231261#M169526</link>
    <description>&lt;P&gt;I don't suppose there is some way of getting the ONFI parameters and converting them for kobs-ng parameters?&lt;/P&gt;&lt;P&gt;The Linux kernel is supposed to be able to read the ONFI parameters. I suppose I could change it to dump the parameters?&amp;nbsp; But then could I line them up with the kobs-ng parameters?&lt;/P&gt;&lt;P&gt;For instance address_setup_time?&amp;nbsp; Might that be ALE setup time in Micron's manual?&lt;BR /&gt;&lt;BR /&gt;data_sample_time is not in the spec sheet that I have from Micron.&lt;BR /&gt;&lt;BR /&gt;what is row_address_size, column_address_size?&lt;BR /&gt;&lt;BR /&gt;What is boot_stream_version, boot_stream_minor_version, boot_stream_sub_version, ncb_version?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NCB is mentioned in IMX6ULLRM, but I have not been able to find the layout.&amp;nbsp; Is the ncb_version assigned to a CPU?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there another document that describes these fields?&lt;/P&gt;</description>
    <pubDate>Tue, 16 Feb 2021 01:50:22 GMT</pubDate>
    <dc:creator>JohnKlug</dc:creator>
    <dc:date>2021-02-16T01:50:22Z</dc:date>
    <item>
      <title>kobs-ng parameters</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/kobs-ng-parameters/m-p/1231261#M169526</link>
      <description>&lt;P&gt;I don't suppose there is some way of getting the ONFI parameters and converting them for kobs-ng parameters?&lt;/P&gt;&lt;P&gt;The Linux kernel is supposed to be able to read the ONFI parameters. I suppose I could change it to dump the parameters?&amp;nbsp; But then could I line them up with the kobs-ng parameters?&lt;/P&gt;&lt;P&gt;For instance address_setup_time?&amp;nbsp; Might that be ALE setup time in Micron's manual?&lt;BR /&gt;&lt;BR /&gt;data_sample_time is not in the spec sheet that I have from Micron.&lt;BR /&gt;&lt;BR /&gt;what is row_address_size, column_address_size?&lt;BR /&gt;&lt;BR /&gt;What is boot_stream_version, boot_stream_minor_version, boot_stream_sub_version, ncb_version?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NCB is mentioned in IMX6ULLRM, but I have not been able to find the layout.&amp;nbsp; Is the ncb_version assigned to a CPU?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there another document that describes these fields?&lt;/P&gt;</description>
      <pubDate>Tue, 16 Feb 2021 01:50:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/kobs-ng-parameters/m-p/1231261#M169526</guid>
      <dc:creator>JohnKlug</dc:creator>
      <dc:date>2021-02-16T01:50:22Z</dc:date>
    </item>
    <item>
      <title>Re: kobs-ng parameters</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/kobs-ng-parameters/m-p/1231831#M169587</link>
      <description>&lt;P&gt;Hi JohnKlug&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;regarding these fields, there is no need to extract them from nand datasheets,&lt;/P&gt;
&lt;P&gt;as kobs-ng utility makes necessary programming automatically.&lt;/P&gt;
&lt;P&gt;One can refer to sect.5.3 Manual step-by-step flashing to NAND flash&lt;/P&gt;
&lt;P&gt;&lt;A href="https://variwiki.com/index.php?title=Yocto_NAND_Flash_Burning" target="_blank"&gt;https://variwiki.com/index.php?title=Yocto_NAND_Flash_Burning&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;or uuu sample script example_kernel_nand.uuu included in Demo Images on link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;Is there another document that describes these fields?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;sorry such documentation is not available.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 17 Feb 2021 04:47:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/kobs-ng-parameters/m-p/1231831#M169587</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-02-17T04:47:41Z</dc:date>
    </item>
    <item>
      <title>Re: kobs-ng parameters</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/kobs-ng-parameters/m-p/1234541#M169828</link>
      <description>&lt;P&gt;I tried this, and got U-Boot to load from NAND on power-up:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;kobs-ng init -x -v --chip_0_device_path=/dev/mtd0 $FILE&lt;/LI-CODE&gt;</description>
      <pubDate>Mon, 22 Feb 2021 18:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/kobs-ng-parameters/m-p/1234541#M169828</guid>
      <dc:creator>JohnKlug</dc:creator>
      <dc:date>2021-02-22T18:22:37Z</dc:date>
    </item>
  </channel>
</rss>