<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8M booting options in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-booting-options/m-p/1230777#M169475</link>
    <description>&lt;P&gt;Hi Luishernandez1,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Reviewing the datasheet from the NAND and the iIMX8M nano it should be compatible with no further problems, also one can check the reference manual on the chapter 6.1.5 Boot devices (internal boot), please take a look on the fragment from the manual:&lt;/P&gt;
&lt;P&gt;- Raw NAND (MLC and SLC), and Toggle-mode NAND flash through GPMI-2&lt;BR /&gt;interface, located at CS0. Page sizes of 2 KB, 4 KB, and 8 KB. The bus widths of 8-&lt;BR /&gt;bit with 2 through 62-bit BCH hardware ECC (Error Correction) are supported.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel H.&lt;/P&gt;</description>
    <pubDate>Mon, 15 Feb 2021 00:18:46 GMT</pubDate>
    <dc:creator>nxf63675</dc:creator>
    <dc:date>2021-02-15T00:18:46Z</dc:date>
    <item>
      <title>IMX8M booting options</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-booting-options/m-p/1230774#M169474</link>
      <description>&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow word-break-ie11"&gt;Hi everyone,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow word-break-ie11"&gt;Want to confirm that the IMX8M Nano supports booting off the below linked NAND through the GPMI interface.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow word-break-ie11"&gt;&lt;A href="https://4donline.ihs.com/images/VipMasterIC/IC/FASL/FASLS03878/FASLS03878-1.pdf?hkey=52A5661711E402568146F3353EA87419" target="_blank"&gt;https://4donline.ihs.com/images/VipMasterIC/IC/FASL/FASLS03878/FASLS03878-1.pdf?hkey=52A5661711E402568146F3353EA87419&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow word-break-ie11"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow word-break-ie11"&gt;Israel H.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 14 Feb 2021 23:52:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-booting-options/m-p/1230774#M169474</guid>
      <dc:creator>Luishernandez1</dc:creator>
      <dc:date>2021-02-14T23:52:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M booting options</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-booting-options/m-p/1230777#M169475</link>
      <description>&lt;P&gt;Hi Luishernandez1,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Reviewing the datasheet from the NAND and the iIMX8M nano it should be compatible with no further problems, also one can check the reference manual on the chapter 6.1.5 Boot devices (internal boot), please take a look on the fragment from the manual:&lt;/P&gt;
&lt;P&gt;- Raw NAND (MLC and SLC), and Toggle-mode NAND flash through GPMI-2&lt;BR /&gt;interface, located at CS0. Page sizes of 2 KB, 4 KB, and 8 KB. The bus widths of 8-&lt;BR /&gt;bit with 2 through 62-bit BCH hardware ECC (Error Correction) are supported.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel H.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Feb 2021 00:18:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-booting-options/m-p/1230777#M169475</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-02-15T00:18:46Z</dc:date>
    </item>
  </channel>
</rss>