<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUSB i.MX6 ULL</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-i-MX6-ULL/m-p/1230773#M169473</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Is it possible to connect to a PC via USB just by turning on the power, without starting up (SD card, eMMC, etc.) and without rewriting the registers?&lt;/P&gt;&lt;P&gt;I would like to do DDR3 calibration.&lt;/P&gt;&lt;P&gt;best regard&lt;/P&gt;</description>
    <pubDate>Sun, 14 Feb 2021 23:49:39 GMT</pubDate>
    <dc:creator>ban45</dc:creator>
    <dc:date>2021-02-14T23:49:39Z</dc:date>
    <item>
      <title>USB i.MX6 ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-i-MX6-ULL/m-p/1230773#M169473</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Is it possible to connect to a PC via USB just by turning on the power, without starting up (SD card, eMMC, etc.) and without rewriting the registers?&lt;/P&gt;&lt;P&gt;I would like to do DDR3 calibration.&lt;/P&gt;&lt;P&gt;best regard&lt;/P&gt;</description>
      <pubDate>Sun, 14 Feb 2021 23:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-i-MX6-ULL/m-p/1230773#M169473</guid>
      <dc:creator>ban45</dc:creator>
      <dc:date>2021-02-14T23:49:39Z</dc:date>
    </item>
    <item>
      <title>Re: USB i.MX6 ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-i-MX6-ULL/m-p/1234616#M169834</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/172436"&gt;@ban45&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Actually, it has to be at least a U-boot image to get started, if you boot without anything your device will be not recognize by the system.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel H.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Feb 2021 00:24:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-i-MX6-ULL/m-p/1234616#M169834</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-02-23T00:24:35Z</dc:date>
    </item>
  </channel>
</rss>