<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAHAB Application Programming Interface Reference Manual for the IMX8X</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/AHAB-Application-Programming-Interface-Reference-Manual-for-the/m-p/1230049#M169406</link>
    <description>&lt;P&gt;Do you have a specific link or download for the AHAB Application Programming Interface Reference Manual if one exists.&amp;nbsp; If not, then the HAB Version 4 Application Programming Interface Reference Manual and is there difference to be noted for AHAB?&lt;/P&gt;</description>
    <pubDate>Thu, 11 Feb 2021 20:25:31 GMT</pubDate>
    <dc:creator>Gandalf-kern</dc:creator>
    <dc:date>2021-02-11T20:25:31Z</dc:date>
    <item>
      <title>AHAB Application Programming Interface Reference Manual for the IMX8X</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AHAB-Application-Programming-Interface-Reference-Manual-for-the/m-p/1230049#M169406</link>
      <description>&lt;P&gt;Do you have a specific link or download for the AHAB Application Programming Interface Reference Manual if one exists.&amp;nbsp; If not, then the HAB Version 4 Application Programming Interface Reference Manual and is there difference to be noted for AHAB?&lt;/P&gt;</description>
      <pubDate>Thu, 11 Feb 2021 20:25:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AHAB-Application-Programming-Interface-Reference-Manual-for-the/m-p/1230049#M169406</guid>
      <dc:creator>Gandalf-kern</dc:creator>
      <dc:date>2021-02-11T20:25:31Z</dc:date>
    </item>
    <item>
      <title>Re: AHAB Application Programming Interface Reference Manual for the IMX8X</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AHAB-Application-Programming-Interface-Reference-Manual-for-the/m-p/1230076#M169408</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The App note for the secure boot using AHAB for the i.MX8X is available at the following link:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12312.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12312.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;And you can refer to the security reference manual after request in the following link:&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=IMX8QXPSRM&amp;amp;appType=moderatedWithoutFAE" target="_blank"&gt;https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=IMX8QXPSRM&amp;amp;appType=moderatedWithoutFAE&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it helps!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Ivan.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Feb 2021 22:06:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AHAB-Application-Programming-Interface-Reference-Manual-for-the/m-p/1230076#M169408</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2021-02-11T22:06:05Z</dc:date>
    </item>
  </channel>
</rss>