<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Using ASRC from within Android</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-ASRC-from-within-Android/m-p/229465#M16937</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Joseph,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ALSA in android does't use alsa config to control sound card like in linux. It's controls are all in ALSA HAL (tinyalsa._hal.c). So if you want to expend functions, you should add code in ALSA HAL .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ALSA in android also uses alsa-lib , So your expened function should also be based on API in alsa-lib.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Dec 2013 04:08:36 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2013-12-03T04:08:36Z</dc:date>
    <item>
      <title>Using ASRC from within Android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-ASRC-from-within-Android/m-p/229464#M16936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are trying to use the ASRC for clock domain synchronization within a daemon in the Android system. This is a similar use-case as in this post: &lt;A href="https://community.nxp.com/message/332039"&gt;i.MX6 ASRC audio support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here we see that a plugin for ALSA can be used to configure the ASRC. However, on Android we only have tinyALSA, which I don't think supports these features. Is there some way this can be integrated with tinyALSA? Or perhaps there could be a setup with ioctl to the ASRC to configure it from there?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Joe Pentland&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2013 16:22:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-ASRC-from-within-Android/m-p/229464#M16936</guid>
      <dc:creator>josephpentland</dc:creator>
      <dc:date>2013-11-26T16:22:10Z</dc:date>
    </item>
    <item>
      <title>Re: Using ASRC from within Android</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-ASRC-from-within-Android/m-p/229465#M16937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Joseph,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ALSA in android does't use alsa config to control sound card like in linux. It's controls are all in ALSA HAL (tinyalsa._hal.c). So if you want to expend functions, you should add code in ALSA HAL .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ALSA in android also uses alsa-lib , So your expened function should also be based on API in alsa-lib.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Dec 2013 04:08:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-ASRC-from-within-Android/m-p/229465#M16937</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2013-12-03T04:08:36Z</dc:date>
    </item>
  </channel>
</rss>