<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ISO/IEC 7816 UART support on MIMX8MN6DVTJZ in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ISO-IEC-7816-UART-support-on-MIMX8MN6DVTJZ/m-p/1229202#M169287</link>
    <description>&lt;P&gt;Dear NXP Community Forum!&lt;/P&gt;&lt;P&gt;We are currently developing&amp;nbsp;a product around the i.MX 8M Nano processor MIMX8MN6DVTJZ. We need to include a Smart Card reader in the design, and we want to use the MIMX8MN6DVTJZ as much as possible - i.e. using as few additional components as possible.Therefore, we would be very thankful, if someone could tell us:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;1.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Does the MIMX8MN6DVTJZ support ISO/IEC 7816 UART? (We couldn’t find anything about it in the documentation, and we would like to be sure.)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;2.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;If not, do you have any design suggestions that would satisfy our initial statement? (I.e. use the fewest possible additional components for running a Smart Card reader.)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;The mediathand development team.&lt;/P&gt;</description>
    <pubDate>Wed, 10 Feb 2021 09:25:22 GMT</pubDate>
    <dc:creator>naoufalmed</dc:creator>
    <dc:date>2021-02-10T09:25:22Z</dc:date>
    <item>
      <title>ISO/IEC 7816 UART support on MIMX8MN6DVTJZ</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ISO-IEC-7816-UART-support-on-MIMX8MN6DVTJZ/m-p/1229202#M169287</link>
      <description>&lt;P&gt;Dear NXP Community Forum!&lt;/P&gt;&lt;P&gt;We are currently developing&amp;nbsp;a product around the i.MX 8M Nano processor MIMX8MN6DVTJZ. We need to include a Smart Card reader in the design, and we want to use the MIMX8MN6DVTJZ as much as possible - i.e. using as few additional components as possible.Therefore, we would be very thankful, if someone could tell us:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;1.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Does the MIMX8MN6DVTJZ support ISO/IEC 7816 UART? (We couldn’t find anything about it in the documentation, and we would like to be sure.)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;2.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;If not, do you have any design suggestions that would satisfy our initial statement? (I.e. use the fewest possible additional components for running a Smart Card reader.)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;The mediathand development team.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Feb 2021 09:25:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ISO-IEC-7816-UART-support-on-MIMX8MN6DVTJZ/m-p/1229202#M169287</guid>
      <dc:creator>naoufalmed</dc:creator>
      <dc:date>2021-02-10T09:25:22Z</dc:date>
    </item>
    <item>
      <title>Re: ISO/IEC 7816 UART support on MIMX8MN6DVTJZ</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ISO-IEC-7816-UART-support-on-MIMX8MN6DVTJZ/m-p/1229276#M169295</link>
      <description>&lt;P&gt;The i.MX8MNano processor has no special support for the ISO/IEC 7816 interface.&amp;nbsp;The possible solution is to use a regular UART (connecting the TX and RX pins&amp;nbsp;together) and an external Smart Card PHY IC, such as the following ones:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/security-and-authentication/contact-readers:MC_42001#/" target="_blank"&gt;https://www.nxp.com/products/security-and-authentication/contact-readers:MC_42001#/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Some non-standard baud rates may be required, so, you have to adjust the UART&amp;nbsp;baudrate clock appropriately within the i.MX8MNano processor.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
      <pubDate>Wed, 10 Feb 2021 11:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ISO-IEC-7816-UART-support-on-MIMX8MN6DVTJZ/m-p/1229276#M169295</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2021-02-10T11:58:14Z</dc:date>
    </item>
    <item>
      <title>Re: ISO/IEC 7816 UART support on MIMX8MN6DVTJZ</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ISO-IEC-7816-UART-support-on-MIMX8MN6DVTJZ/m-p/1229331#M169304</link>
      <description>Thank you very much!</description>
      <pubDate>Wed, 10 Feb 2021 14:25:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ISO-IEC-7816-UART-support-on-MIMX8MN6DVTJZ/m-p/1229331#M169304</guid>
      <dc:creator>naoufalmed</dc:creator>
      <dc:date>2021-02-10T14:25:02Z</dc:date>
    </item>
  </channel>
</rss>