<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MIPI CSI-2 color data format is wrong in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-color-data-format-is-wrong/m-p/1228661#M169216</link>
    <description>&lt;P&gt;It was missconfiguration in Xillinx IP Core MIPI CSI2 TX especialy continoius clock.&lt;/P&gt;</description>
    <pubDate>Tue, 09 Feb 2021 09:09:07 GMT</pubDate>
    <dc:creator>dimitarmaznekov</dc:creator>
    <dc:date>2021-02-09T09:09:07Z</dc:date>
    <item>
      <title>MIPI CSI-2 color data format is wrong</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-color-data-format-is-wrong/m-p/1224429#M168780</link>
      <description>&lt;P&gt;We are working trying to receive RGB888 video on MIPI CSI-2 interface from custom sensor.&lt;BR /&gt;We are using VAR-DT6CustomBoard with DART-MX6 SOM.&lt;BR /&gt;We are running linux imx_4.14.78_1.0.0_ga_var01 with modified ov5640_mipi driver to receive video from our custom sensor.&lt;BR /&gt;Currently we are capable of receiving video over MIPI interface, but it seems like the color data format is wrong.&lt;BR /&gt;We've set MIPI_DT_RGB888 format in the ov5640 driver. We added debug prints in ipu_csi_enc.c and the format in csi_enc_setup() function is set to IPU_PIX_FMT_UYVY&lt;/P&gt;&lt;P&gt;It's our custom sensor. It's implemented using FPGA transmitting MIPI CSI-2 at 160Mb/s (80Mhz physical clk) in RGB888 format. We can confirm the signal integrity with oscilloscope.&lt;/P&gt;&lt;P&gt;We are trying to receive the MIPI signal with RGB888 format using modified ov5640 mipi driver, but it seems like its not supporting this format (its default is V4L2_PIX_FMT_UYVY).&lt;BR /&gt;Do you have MIPI driver that supports capturing RGB888 (V4L2_PIX_FMT_RGB24) we can use or help us modify the existing one?&lt;/P&gt;</description>
      <pubDate>Tue, 02 Feb 2021 09:12:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-color-data-format-is-wrong/m-p/1224429#M168780</guid>
      <dc:creator>dimitarmaznekov</dc:creator>
      <dc:date>2021-02-02T09:12:34Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI CSI-2 color data format is wrong</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-color-data-format-is-wrong/m-p/1225369#M168865</link>
      <description>&lt;P&gt;pls refer to the debug mipi document as below:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Debug-steps-for-customer-MIPI-sensor-docx/ta-p/1120244" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Debug-steps-for-customer-MIPI-sensor-docx/ta-p/1120244&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Feb 2021 08:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-color-data-format-is-wrong/m-p/1225369#M168865</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-02-03T08:31:56Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI CSI-2 color data format is wrong</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-color-data-format-is-wrong/m-p/1228661#M169216</link>
      <description>&lt;P&gt;It was missconfiguration in Xillinx IP Core MIPI CSI2 TX especialy continoius clock.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Feb 2021 09:09:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-2-color-data-format-is-wrong/m-p/1228661#M169216</guid>
      <dc:creator>dimitarmaznekov</dc:creator>
      <dc:date>2021-02-09T09:09:07Z</dc:date>
    </item>
  </channel>
</rss>