<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx8qxp m4 hangs at linux boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1228649#M169215</link>
    <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;re-adding here, tested&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;i tested&amp;nbsp;imx_5.4.70_2.3.0 with&amp;nbsp; &amp;nbsp;fdt_file=imx8qxp-mek-dsi-rm67191-rpmsg.dtb , still M4 stops to run at kernel boot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;i tested now&amp;nbsp;imx_4.19.35_1.1.0, it does not stop M4 at boot.&lt;/P&gt;&lt;P&gt;So issue is related to imx_5.4.70_2.3.0.&amp;nbsp; Please let me know if this is an open&amp;nbsp; issue on&amp;nbsp;imx_5.4.70_2.3.0.&lt;/P&gt;</description>
    <pubDate>Tue, 09 Feb 2021 08:51:36 GMT</pubDate>
    <dc:creator>angelo_d</dc:creator>
    <dc:date>2021-02-09T08:51:36Z</dc:date>
    <item>
      <title>imx8qxp m4 hangs at linux boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1227550#M169085</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;once loaded a cortex M4 image at u-boot (bootaux) and checked it works by interacting on the M4 console, i boot linux (boot cmd) and suddenly M4 stops to work. Is this normal ? Is there a way to keep M4 running over Linux boot ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 07 Feb 2021 09:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1227550#M169085</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2021-02-07T09:06:34Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp m4 hangs at linux boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1227601#M169095</link>
      <description>&lt;P&gt;Hi spectrum&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;what bsp used in the case, one can try with latest Linux 5.4.70_2.3.0​, use below dts&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qxp-mek-dsi-rm67191-rpmsg.dts?h=imx_5.4.70_2.3.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qxp-mek-dsi-rm67191-rpmsg.dts?h=imx_5.4.70_2.3.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;linux documentation&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sun, 07 Feb 2021 23:07:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1227601#M169095</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-02-07T23:07:39Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp m4 hangs at linux boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1227845#M169125</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;thanks for the feedback, but issue is still the same: at the moment when linux boots, M4 application stops to run.&lt;BR /&gt;I tested a mainline kernel, and it does not stops M4 at boot.&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;&lt;/P&gt;&lt;P&gt;imx_5.4.70_2.3.0&lt;BR /&gt;imx8qxp-mek-dsi-rm67191.dtb&lt;/P&gt;&lt;P&gt;On M4, i am keeping running&amp;nbsp; power_mode_switch app, that allows to use an interactive menu on M4 console, and i can see if M4 is running.&lt;/P&gt;&lt;P&gt;From u-boot, i do :&lt;/P&gt;&lt;P&gt;fatload mmc 1:1 ${loadaddr} power_mode_switch.bin &amp;amp;&amp;amp; dcache flush &amp;amp;&amp;amp; bootaux ${loadaddr} 0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(M4 demo works just after fw loading)&lt;/P&gt;&lt;P&gt;command line: console=ttyLP0,115200 root=/dev/mmcblk1p2 rootwait rw&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As defconfig using one based on imx_v8_defconfig.&lt;/P&gt;&lt;P&gt;If any help, welcome.&lt;/P&gt;&lt;P&gt;Angelo&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 09:30:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1227845#M169125</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2021-02-08T09:30:53Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp m4 hangs at linux boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1228480#M169197</link>
      <description>&lt;P&gt;Hi Angelo&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;could you try imx8qxp-mek-dsi-rm67191-rpmsg.dts as was suggested.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Feb 2021 04:07:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1228480#M169197</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-02-09T04:07:17Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp m4 hangs at linux boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1228627#M169212</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;sorry, should have been a typo, i tested with&amp;nbsp; &amp;nbsp;fdt_file=imx8qxp-mek-dsi-rm67191-rpmsg.dtb&amp;nbsp;&lt;/P&gt;&lt;P&gt;Same issue, M4 app stops to work as soon as the kernel boots, as some clocks or power is cut.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Feb 2021 08:24:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1228627#M169212</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2021-02-09T08:24:52Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp m4 hangs at linux boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1228649#M169215</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;re-adding here, tested&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;i tested&amp;nbsp;imx_5.4.70_2.3.0 with&amp;nbsp; &amp;nbsp;fdt_file=imx8qxp-mek-dsi-rm67191-rpmsg.dtb , still M4 stops to run at kernel boot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;i tested now&amp;nbsp;imx_4.19.35_1.1.0, it does not stop M4 at boot.&lt;/P&gt;&lt;P&gt;So issue is related to imx_5.4.70_2.3.0.&amp;nbsp; Please let me know if this is an open&amp;nbsp; issue on&amp;nbsp;imx_5.4.70_2.3.0.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Feb 2021 08:51:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1228649#M169215</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2021-02-09T08:51:36Z</dc:date>
    </item>
    <item>
      <title>Re: imx8qxp m4 hangs at linux boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1229029#M169255</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;seems something related my image built on dunfell and meta-freescale was causing the issue.&lt;BR /&gt;Probably something related to SCU fw.&lt;/P&gt;&lt;P&gt;Building using meta-nxp stuff (zeus, using 5.4.70_2.3.0)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;MACHINE=imx8qxpmek source imx-setup-release.sh -b initial_build_dir&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;All seems to work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Tue, 09 Feb 2021 22:27:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8qxp-m4-hangs-at-linux-boot/m-p/1229029#M169255</guid>
      <dc:creator>angelo_d</dc:creator>
      <dc:date>2021-02-09T22:27:30Z</dc:date>
    </item>
  </channel>
</rss>