<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: modbus on yocto kernel for imx6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/modbus-on-yocto-kernel-for-imx6/m-p/1227894#M169134</link>
    <description>&lt;P&gt;You can refer to this &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Add-support-RS485-half-duplex/ta-p/1128042" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Add-support-RS485-half-duplex/ta-p/1128042&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 08 Feb 2021 10:31:35 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2021-02-08T10:31:35Z</dc:date>
    <item>
      <title>modbus on yocto kernel for imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/modbus-on-yocto-kernel-for-imx6/m-p/1196242#M166183</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I need to inlcude the modbus via uart 485 feature on my custom board.&lt;/P&gt;&lt;P&gt;My board is based on imx6 and kernel generated by Yocto project.&lt;/P&gt;&lt;P&gt;Is it possible to include that feature in the kernel directly by menu configuration?&lt;/P&gt;&lt;P&gt;Is there any document or manual or application note for that?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Fabio&lt;/P&gt;</description>
      <pubDate>Wed, 09 Dec 2020 09:37:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/modbus-on-yocto-kernel-for-imx6/m-p/1196242#M166183</guid>
      <dc:creator>fabio_poiatti</dc:creator>
      <dc:date>2020-12-09T09:37:04Z</dc:date>
    </item>
    <item>
      <title>Re: modbus on yocto kernel for imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/modbus-on-yocto-kernel-for-imx6/m-p/1227894#M169134</link>
      <description>&lt;P&gt;You can refer to this &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Add-support-RS485-half-duplex/ta-p/1128042" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Add-support-RS485-half-duplex/ta-p/1128042&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 10:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/modbus-on-yocto-kernel-for-imx6/m-p/1227894#M169134</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-02-08T10:31:35Z</dc:date>
    </item>
  </channel>
</rss>