<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX8QM QSPI Slave in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-QSPI-Slave/m-p/1226641#M168967</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm looking to interface an iMX8QM to an external MCU which provides a QSPI interface as the Master. I found &lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX8M-i-MX8X-support-QSPI-FlexSPI-slave-mode/m-p/826698" target="_blank" rel="noopener"&gt;this&lt;/A&gt; question from 2018 regarding QSPI slave on the iMX8QM, but have been unable to find anything in the documentation which states that the QSPI interface only supports Master mode. Is QSPI Slave mode possible with the iMX8QM controller? Any clarification would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Thu, 04 Feb 2021 22:13:52 GMT</pubDate>
    <dc:creator>jars121</dc:creator>
    <dc:date>2021-02-04T22:13:52Z</dc:date>
    <item>
      <title>iMX8QM QSPI Slave</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-QSPI-Slave/m-p/1226641#M168967</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm looking to interface an iMX8QM to an external MCU which provides a QSPI interface as the Master. I found &lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX8M-i-MX8X-support-QSPI-FlexSPI-slave-mode/m-p/826698" target="_blank" rel="noopener"&gt;this&lt;/A&gt; question from 2018 regarding QSPI slave on the iMX8QM, but have been unable to find anything in the documentation which states that the QSPI interface only supports Master mode. Is QSPI Slave mode possible with the iMX8QM controller? Any clarification would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 22:13:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-QSPI-Slave/m-p/1226641#M168967</guid>
      <dc:creator>jars121</dc:creator>
      <dc:date>2021-02-04T22:13:52Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QM QSPI Slave</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-QSPI-Slave/m-p/1226751#M168979</link>
      <description>&lt;P&gt;Hi jars121&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;QSPI Slave mode possible with the iMX8QM controller&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;sorry it is not supported, in particular FlexSPI has not special master/slave setting like ecspi&lt;/P&gt;
&lt;P&gt;ECSPIx_CONREG(CHANNEL_MODE).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Fri, 05 Feb 2021 03:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-QSPI-Slave/m-p/1226751#M168979</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-02-05T03:05:14Z</dc:date>
    </item>
  </channel>
</rss>