<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックError hciattach QCA9377 Bluetooth</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-hciattach-QCA9377-Bluetooth/m-p/1222751#M168600</link>
    <description>&lt;P&gt;I use a pico-imx7(qca9377 wifi/bt) on a pico-nymph baseboard with a Yocto image (Dunfell 3.1, Kernel 5.4).&lt;BR /&gt;The wifi work's but I have a error when I attach a UART to the bluetooth stack as HCI interface.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;root@imx7d-pico:~# hciattach -t 30 /dev/ttymxc6 any 115200 flow&lt;BR /&gt;Device setup complete&lt;BR /&gt;root@imx7d-pico:~# [ 976.554963] Bluetooth: hci0: command 0x1003 tx timeout&lt;BR /&gt;[ 978.634975] Bluetooth: hci0: command 0x1001 tx timeout&lt;BR /&gt;[ 980.714945] Bluetooth: hci0: command 0x1009 tx timeout&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;And when I read the Kernel's messages (dmesg or during boot), I found this error :&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;[ 5.756177] ar6k_wlan mmc1:0001:1: Direct firmware load for wlan/qca9377/wlan_mac.bin failed with error -2&lt;BR /&gt;[ 5.765929] ar6k_wlan mmc1:0001:1: Falling back to sysfs fallback for: wlan/qca9377/wlan_mac.bin&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I don't have the file firmware wlan_mac.bin.&lt;/P&gt;&lt;P&gt;If I print informations of bluetooth device, my MAC address is null.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;root@imx7d-pico:~# hciconfig&lt;BR /&gt;hci0: Type: Primary Bus: UART&lt;BR /&gt;BD Address: 00:00:00:00:00:00 ACL MTU: 0:0 SCO MTU: 0:0&lt;BR /&gt;DOWN&lt;BR /&gt;RX bytes:0 acl:0 sco:0 events:0 errors:0&lt;BR /&gt;TX bytes:12 acl:0 sco:0 commands:3 errors:0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Can you help me ? Thank you in advance.&lt;/P&gt;</description>
    <pubDate>Thu, 28 Jan 2021 15:46:24 GMT</pubDate>
    <dc:creator>lecureux</dc:creator>
    <dc:date>2021-01-28T15:46:24Z</dc:date>
    <item>
      <title>Error hciattach QCA9377 Bluetooth</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-hciattach-QCA9377-Bluetooth/m-p/1222751#M168600</link>
      <description>&lt;P&gt;I use a pico-imx7(qca9377 wifi/bt) on a pico-nymph baseboard with a Yocto image (Dunfell 3.1, Kernel 5.4).&lt;BR /&gt;The wifi work's but I have a error when I attach a UART to the bluetooth stack as HCI interface.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;root@imx7d-pico:~# hciattach -t 30 /dev/ttymxc6 any 115200 flow&lt;BR /&gt;Device setup complete&lt;BR /&gt;root@imx7d-pico:~# [ 976.554963] Bluetooth: hci0: command 0x1003 tx timeout&lt;BR /&gt;[ 978.634975] Bluetooth: hci0: command 0x1001 tx timeout&lt;BR /&gt;[ 980.714945] Bluetooth: hci0: command 0x1009 tx timeout&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;And when I read the Kernel's messages (dmesg or during boot), I found this error :&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;[ 5.756177] ar6k_wlan mmc1:0001:1: Direct firmware load for wlan/qca9377/wlan_mac.bin failed with error -2&lt;BR /&gt;[ 5.765929] ar6k_wlan mmc1:0001:1: Falling back to sysfs fallback for: wlan/qca9377/wlan_mac.bin&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I don't have the file firmware wlan_mac.bin.&lt;/P&gt;&lt;P&gt;If I print informations of bluetooth device, my MAC address is null.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;root@imx7d-pico:~# hciconfig&lt;BR /&gt;hci0: Type: Primary Bus: UART&lt;BR /&gt;BD Address: 00:00:00:00:00:00 ACL MTU: 0:0 SCO MTU: 0:0&lt;BR /&gt;DOWN&lt;BR /&gt;RX bytes:0 acl:0 sco:0 events:0 errors:0&lt;BR /&gt;TX bytes:12 acl:0 sco:0 commands:3 errors:0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Can you help me ? Thank you in advance.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jan 2021 15:46:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-hciattach-QCA9377-Bluetooth/m-p/1222751#M168600</guid>
      <dc:creator>lecureux</dc:creator>
      <dc:date>2021-01-28T15:46:24Z</dc:date>
    </item>
    <item>
      <title>Re: Error hciattach QCA9377 Bluetooth</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-hciattach-QCA9377-Bluetooth/m-p/1223317#M168665</link>
      <description>&lt;P&gt;Hello lecurex,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You need to check the wlan_mac.bin with pico manufacturer, in this case yocto don´t have the proper driver for it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Jan 2021 13:54:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-hciattach-QCA9377-Bluetooth/m-p/1223317#M168665</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-01-29T13:54:17Z</dc:date>
    </item>
  </channel>
</rss>