<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Error when trying to build u-boot through Yocto project in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-when-trying-to-build-u-boot-through-Yocto-project/m-p/1221585#M168463</link>
    <description>&lt;P&gt;refer to the yocto user guide, The recommended minimum Ubuntu version is 18.04 or later&lt;/P&gt;</description>
    <pubDate>Wed, 27 Jan 2021 02:39:11 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2021-01-27T02:39:11Z</dc:date>
    <item>
      <title>Error when trying to build u-boot through Yocto project</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-when-trying-to-build-u-boot-through-Yocto-project/m-p/1221555#M168459</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am trying to build u-boot from the yocto setup. I followed the steps mentioned in IMXLXYOCTOUG Rev. L5.4.70_2.3.0 — 31 December 2020 to setup the yocto project.&lt;/P&gt;&lt;P&gt;When i run the command&amp;nbsp; " $MACHINE=imx8qxpmek bitbake -c deploy u-boot-imx "&lt;/P&gt;&lt;P&gt;i get the following error "&lt;/P&gt;&lt;P&gt;ERROR: OE-core's config sanity checker detected a potential misconfiguration.&lt;BR /&gt;Either fix the cause of this error or at your own risk disable the checker (see sanity.conf).&lt;BR /&gt;Following is the list of potential problems / advisories:&lt;/P&gt;&lt;P&gt;MACHINE=imx8qxpmek is invalid. Please set a valid MACHINE in your local.conf, environment or other configuration file.&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;I am using a Ubuntu 16.04 machine. How to fix this issue?&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Ramprakash&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jan 2021 01:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-when-trying-to-build-u-boot-through-Yocto-project/m-p/1221555#M168459</guid>
      <dc:creator>Ramprakash</dc:creator>
      <dc:date>2021-01-27T01:43:40Z</dc:date>
    </item>
    <item>
      <title>Re: Error when trying to build u-boot through Yocto project</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-when-trying-to-build-u-boot-through-Yocto-project/m-p/1221585#M168463</link>
      <description>&lt;P&gt;refer to the yocto user guide, The recommended minimum Ubuntu version is 18.04 or later&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jan 2021 02:39:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-when-trying-to-build-u-boot-through-Yocto-project/m-p/1221585#M168463</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-01-27T02:39:11Z</dc:date>
    </item>
    <item>
      <title>Re: Error when trying to build u-boot through Yocto project</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-when-trying-to-build-u-boot-through-Yocto-project/m-p/1222215#M168522</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Yes, I did go through the yocto guide and I saw ubuntu 16.04 LTS are one of the build system. Anyway I'll try again with Ubuntu 18.04 LTS.&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Ramprakash&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jan 2021 22:27:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-when-trying-to-build-u-boot-through-Yocto-project/m-p/1222215#M168522</guid>
      <dc:creator>Ramprakash</dc:creator>
      <dc:date>2021-01-27T22:27:31Z</dc:date>
    </item>
  </channel>
</rss>