<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピック【IMX8QXP，SJA1105Q】device tree config</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-SJA1105Q-device-tree-config/m-p/1220909#M168375</link>
    <description>&lt;P&gt;Dear friend&lt;/P&gt;&lt;P&gt;My platform is i.MX8QXP, SJA1105, Yocto L5.4.70_2.3.0.&lt;/P&gt;&lt;P&gt;description：&lt;/P&gt;&lt;P&gt;1）SJA1105's port0 connect to i.MX8QXP's&amp;nbsp;ethphy0，&lt;/P&gt;&lt;P&gt;2）SJA1105's SPI connect to i.MX8QXP's LSPI2;&lt;/P&gt;&lt;P&gt;Question：&lt;/P&gt;&lt;P&gt;1）can you provide an device tree example for SJA1105 connected to i.MX8QXP according to my description?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;----&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;</description>
    <pubDate>Tue, 26 Jan 2021 01:45:02 GMT</pubDate>
    <dc:creator>jianwei_lan</dc:creator>
    <dc:date>2021-01-26T01:45:02Z</dc:date>
    <item>
      <title>【IMX8QXP，SJA1105Q】device tree config</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-SJA1105Q-device-tree-config/m-p/1220909#M168375</link>
      <description>&lt;P&gt;Dear friend&lt;/P&gt;&lt;P&gt;My platform is i.MX8QXP, SJA1105, Yocto L5.4.70_2.3.0.&lt;/P&gt;&lt;P&gt;description：&lt;/P&gt;&lt;P&gt;1）SJA1105's port0 connect to i.MX8QXP's&amp;nbsp;ethphy0，&lt;/P&gt;&lt;P&gt;2）SJA1105's SPI connect to i.MX8QXP's LSPI2;&lt;/P&gt;&lt;P&gt;Question：&lt;/P&gt;&lt;P&gt;1）can you provide an device tree example for SJA1105 connected to i.MX8QXP according to my description?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;----&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jan 2021 01:45:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-SJA1105Q-device-tree-config/m-p/1220909#M168375</guid>
      <dc:creator>jianwei_lan</dc:creator>
      <dc:date>2021-01-26T01:45:02Z</dc:date>
    </item>
    <item>
      <title>Re: 【IMX8QXP，SJA1105Q】device tree config</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-SJA1105Q-device-tree-config/m-p/1221759#M168482</link>
      <description>&lt;P&gt;all of SJA1105Q materials you can find from the link as below, you can refer to the dts file as below:&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://source.codeaurora.org/external/autoivnsw/sja1105x_linux_switchdev/tree/doc/device_tree" target="_blank"&gt;https://source.codeaurora.org/external/autoivnsw/sja1105x_linux_switchdev/tree/doc/device_tree&lt;/A&gt;"&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jan 2021 07:56:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-SJA1105Q-device-tree-config/m-p/1221759#M168482</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-01-27T07:56:59Z</dc:date>
    </item>
  </channel>
</rss>