<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX 7D can't get kernel image!</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX-7D-can-t-get-kernel-image/m-p/1220463#M168349</link>
    <description>&lt;P&gt;Have you set right kernel command line in u-boot?&lt;/P&gt;</description>
    <pubDate>Mon, 25 Jan 2021 10:41:21 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2021-01-25T10:41:21Z</dc:date>
    <item>
      <title>IMX 7D can't get kernel image!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-7D-can-t-get-kernel-image/m-p/1197914#M166327</link>
      <description>&lt;P&gt;Hello all, Now I meet "can't get kernel image!".&lt;/P&gt;&lt;P&gt;introduce as below:&lt;/P&gt;&lt;P&gt;Project background:&lt;BR /&gt;Under /work path, successfully operate as below:&lt;BR /&gt;repo init -u &lt;A href="https://source.codeaurora.org/external/imx/imx-manifest" target="_blank"&gt;https://source.codeaurora.org/external/imx/imx-manifest&lt;/A&gt; -b imx-linux-zeus -m imx-5.4.47-2.2.0.xml&lt;BR /&gt;DISTRO=fsl-imx-fb MACHINE=imx7dsabresd source imx-setup-release.sh -b fsl-imx-fb&lt;BR /&gt;cd fsl-imx-fb&lt;BR /&gt;bitbake core-image-base&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Then step as below:&lt;BR /&gt;1， FDISK&lt;BR /&gt;Operate as below:&lt;BR /&gt;fdisk /dev/sdb&lt;BR /&gt;p&lt;BR /&gt;d&lt;BR /&gt;n&lt;BR /&gt;p&lt;BR /&gt;1&lt;BR /&gt;20480&lt;BR /&gt;1044479&lt;BR /&gt;t&lt;BR /&gt;L&lt;BR /&gt;c&lt;BR /&gt;p&lt;BR /&gt;n&lt;BR /&gt;p&lt;BR /&gt;2&lt;BR /&gt;1228800&lt;BR /&gt;&amp;lt;enter&amp;gt;&lt;BR /&gt;p&lt;BR /&gt;w&lt;BR /&gt;Information as below:&lt;BR /&gt;/dev/sdb1 20480 1044479 1024000 500M c W95 FAT32 (LBA)&lt;BR /&gt;/dev/sdb2 1228800 31116287 29887488 14.3G 83 Linux&lt;/P&gt;&lt;P&gt;2， Burd UBOOT&lt;BR /&gt;under the /work/yocto/fsl-imx-fb/tmp/deploy/images/imx7dsabresd path,Operate as below:&lt;BR /&gt;dd if=u-boot-sd-optee-2020.04-r0.imx of=/dev/sdb bs=1k seek=1 conv=fsync&lt;/P&gt;&lt;P&gt;3， Burd IMAGE&lt;BR /&gt;Operate as below:&lt;BR /&gt;First under the /work/yocto/fsl-imx-fb/tmp/deploy/images/imx7dsabresd path&lt;BR /&gt;cp zImage--5.4-r0-imx7dsabresd-20201210051308.bin /mnt&lt;BR /&gt;cp imx7d-sdb-reva--5.4-r0-imx7dsabresd-20201210051308.dtb&lt;/P&gt;&lt;P&gt;Under the /mnt path&lt;BR /&gt;mov zImage--5.4-r0-imx7dsabresd-20201210051308.bin zImage&lt;BR /&gt;mov imx7d-sdb-reva--5.4-r0-imx7dsabresd-20201210051308.dtb imx7d-sdb.dtb&lt;/P&gt;&lt;P&gt;mkfs.vfat /dev/sdb1&lt;BR /&gt;mount /dev/sdb1 /mnt/mountpoint&lt;BR /&gt;cp zImage /mnt/mountpoint&lt;BR /&gt;cp imx7d-sdb.dtb /mnt/mountpoint&lt;BR /&gt;umount /mnt/mountpoint&lt;BR /&gt;sync&lt;/P&gt;&lt;P&gt;4， Terminal Info as below:&lt;BR /&gt;U-Boot 2020.04-5.4.47-2.2.0+gffc3fbe7e5 (Dec 02 2020 - 13:15:02 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX7D rev1.3 1000 MHz (running at 792 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 31C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: i.MX7 SabreSD Board&lt;BR /&gt;Board: i.MX7D SABRESD RevA in secure mode&lt;BR /&gt;DRAM: 1 GiB&lt;BR /&gt;PMIC: PFUZE3000 DEV_ID=0x30 REV_ID=0x11&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0 (480 x 272)&lt;BR /&gt;[0] lcdif@30730000, video&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;flash target is MMC:0&lt;BR /&gt;Net:&lt;BR /&gt;Warning: ethernet@30be0000 using MAC address from ROM&lt;BR /&gt;eth0: ethernet@30be0000 [PRIME]Get shared mii bus on ethernet@30bf0000&lt;/P&gt;&lt;P&gt;Warning: ethernet@30bf0000 using MAC address from ROM&lt;BR /&gt;, eth1: ethernet@30bf0000&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;9004184 bytes read in 399 ms (21.5 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;48702 bytes read in 21 ms (2.2 MiB/s)&lt;BR /&gt;Wrong Image Format for bootm command&lt;BR /&gt;ERROR: can't get kernel image!&lt;BR /&gt;=&amp;gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 07:30:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-7D-can-t-get-kernel-image/m-p/1197914#M166327</guid>
      <dc:creator>1844350626</dc:creator>
      <dc:date>2020-12-11T07:30:30Z</dc:date>
    </item>
    <item>
      <title>Re: IMX 7D can't get kernel image!</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-7D-can-t-get-kernel-image/m-p/1220463#M168349</link>
      <description>&lt;P&gt;Have you set right kernel command line in u-boot?&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 10:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-7D-can-t-get-kernel-image/m-p/1220463#M168349</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-01-25T10:41:21Z</dc:date>
    </item>
  </channel>
</rss>