<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX8 Generate a cold reboot to refresh bootloader .text/.data section in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Generate-a-cold-reboot-to-refresh-bootloader-text-data/m-p/1219581#M168235</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26366"&gt;@weidong_sun&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This behavior was not observed with Linux&amp;nbsp;&lt;SPAN&gt;4.14 and appears in 5.4 release.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Also board are already shipped and can't be modify.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Clement&lt;/P&gt;</description>
    <pubDate>Fri, 22 Jan 2021 11:03:20 GMT</pubDate>
    <dc:creator>clementperon</dc:creator>
    <dc:date>2021-01-22T11:03:20Z</dc:date>
    <item>
      <title>i.MX8 Generate a cold reboot to refresh bootloader .text/.data section</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Generate-a-cold-reboot-to-refresh-bootloader-text-data/m-p/1218717#M168153</link>
      <description>&lt;P&gt;Hi NXP Community,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are looking to update the bootloader of i.MX8QM remotely on the field for board that's are always powered-on.&lt;BR /&gt;&lt;BR /&gt;Unfortunately right now when you update the bootloader and then reboot from Linux the bootloader and SPL aren't reloaded:&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;&lt;I&gt;When doing partition reboot, the boot image won't be reloaded by ROM,&lt;/I&gt;&lt;I&gt;it is just CPU reset to boot entry. The SW has to keep the boot image&lt;/I&gt;&lt;I&gt;inside the RAM unchanged. It includes both the TEXT section and DATA&lt;/I&gt;&lt;I&gt;section.&lt;/I&gt;&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;As I said the board are always powered and can't be unplug/replug easily to generate a cold reboot.&lt;/P&gt;&lt;P&gt;Do you see any solution to generate a cold reboot from linux?&lt;/P&gt;&lt;P&gt;Thanks for your help,&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jan 2021 09:29:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Generate-a-cold-reboot-to-refresh-bootloader-text-data/m-p/1218717#M168153</guid>
      <dc:creator>clementperon</dc:creator>
      <dc:date>2021-01-21T09:29:37Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Generate a cold reboot to refresh bootloader .text/.data section</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Generate-a-cold-reboot-to-refresh-bootloader-text-data/m-p/1218781#M168161</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; what I refer to is imx8qm-mek design files.&lt;/P&gt;
&lt;P&gt;Linux reboot executes the PMIC_WDOG_IN network on the hardware, and PMIC_WDOG_IN is connected to the WDI pin of the PMIC. If you want cold reset, we must reset PMIC. Therefore, you can try it like this:&lt;BR /&gt;1. Connect R63 and R66 together with a wire&lt;BR /&gt;2. Connect R110 and R113 together with a wire&lt;BR /&gt;The purpose is to pull down the PWRON pin when WDOG sends a LOW level to reset the PMIC.&lt;/P&gt;
&lt;P&gt;If this method fails to achieve your goal, it is difficult to find a better way.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this information is helpful to you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;
&lt;P&gt;B.R,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jan 2021 10:45:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Generate-a-cold-reboot-to-refresh-bootloader-text-data/m-p/1218781#M168161</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2021-01-21T10:45:49Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8 Generate a cold reboot to refresh bootloader .text/.data section</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Generate-a-cold-reboot-to-refresh-bootloader-text-data/m-p/1219581#M168235</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26366"&gt;@weidong_sun&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This behavior was not observed with Linux&amp;nbsp;&lt;SPAN&gt;4.14 and appears in 5.4 release.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Also board are already shipped and can't be modify.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Clement&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jan 2021 11:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8-Generate-a-cold-reboot-to-refresh-bootloader-text-data/m-p/1219581#M168235</guid>
      <dc:creator>clementperon</dc:creator>
      <dc:date>2021-01-22T11:03:20Z</dc:date>
    </item>
  </channel>
</rss>