<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic One wire problem in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/One-wire-problem/m-p/153519#M1681</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi, I am working with 1kb EEPROM DS2431 one wire device in IMX51 processor. By default the processor itself supports one wire. I loaded the slave module first and then the master module. For reading/writing to the device, the 1-wire driver provides a binary attribute inside the sysfs. In the case of the DS2431, this attribute is placed under the following path and with the following attributes ls /sys/devices/w1_bus_master1/bus/devices/2d-0000015db4d0/ The 2d-0000015db4d0 is the unique device id that will appear after the master detects the slave device. In my case I connected two devices in parallel but only one device is detected in sysfs. I googled but I didnt find any clue why the 2nd device is not detected. Did I miss anything?  Thanks in advance for your help&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Apr 2012 05:02:26 GMT</pubDate>
    <dc:creator>sountharya1z</dc:creator>
    <dc:date>2012-04-12T05:02:26Z</dc:date>
    <item>
      <title>One wire problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/One-wire-problem/m-p/153519#M1681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi, I am working with 1kb EEPROM DS2431 one wire device in IMX51 processor. By default the processor itself supports one wire. I loaded the slave module first and then the master module. For reading/writing to the device, the 1-wire driver provides a binary attribute inside the sysfs. In the case of the DS2431, this attribute is placed under the following path and with the following attributes ls /sys/devices/w1_bus_master1/bus/devices/2d-0000015db4d0/ The 2d-0000015db4d0 is the unique device id that will appear after the master detects the slave device. In my case I connected two devices in parallel but only one device is detected in sysfs. I googled but I didnt find any clue why the 2nd device is not detected. Did I miss anything?  Thanks in advance for your help&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Apr 2012 05:02:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/One-wire-problem/m-p/153519#M1681</guid>
      <dc:creator>sountharya1z</dc:creator>
      <dc:date>2012-04-12T05:02:26Z</dc:date>
    </item>
  </channel>
</rss>