<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic [IMX8M Mini] Using GPIO1_IO14 as CLKO1 with 48MHz frequency in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-Using-GPIO1-IO14-as-CLKO1-with-48MHz-frequency/m-p/1217829#M168075</link>
    <description>&lt;LI-SPOILER&gt;&lt;LI-SPOILER&gt;&amp;nbsp;&lt;/LI-SPOILER&gt; &lt;/LI-SPOILER&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to use the GPIO1_IO14 in IMX8M Mini as CLKO1 clock source for an external module. This clock rates need to be 48MHz.&lt;/P&gt;&lt;P&gt;Does GPIO1_IO14 support 48Mhz clock rate?&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Naman Thaker&lt;/P&gt;</description>
    <pubDate>Wed, 20 Jan 2021 09:55:49 GMT</pubDate>
    <dc:creator>namanthaker</dc:creator>
    <dc:date>2021-01-20T09:55:49Z</dc:date>
    <item>
      <title>[IMX8M Mini] Using GPIO1_IO14 as CLKO1 with 48MHz frequency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-Using-GPIO1-IO14-as-CLKO1-with-48MHz-frequency/m-p/1217829#M168075</link>
      <description>&lt;LI-SPOILER&gt;&lt;LI-SPOILER&gt;&amp;nbsp;&lt;/LI-SPOILER&gt; &lt;/LI-SPOILER&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to use the GPIO1_IO14 in IMX8M Mini as CLKO1 clock source for an external module. This clock rates need to be 48MHz.&lt;/P&gt;&lt;P&gt;Does GPIO1_IO14 support 48Mhz clock rate?&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Naman Thaker&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jan 2021 09:55:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-Mini-Using-GPIO1-IO14-as-CLKO1-with-48MHz-frequency/m-p/1217829#M168075</guid>
      <dc:creator>namanthaker</dc:creator>
      <dc:date>2021-01-20T09:55:49Z</dc:date>
    </item>
  </channel>
</rss>