<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: About Quad SPI in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-Quad-SPI/m-p/1217714#M168066</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In DDR mode, the data is updated with half clock,&lt;/P&gt;&lt;P&gt;so do you think SCK = (1/76MHz)/2 = 6.57ns&amp;gt; Tis + Tih should be set?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="goto11_0-1611128459314.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135278iD19DCCD740BE128A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="goto11_0-1611128459314.png" alt="goto11_0-1611128459314.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;best regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Goto&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 20 Jan 2021 07:47:32 GMT</pubDate>
    <dc:creator>goto11</dc:creator>
    <dc:date>2021-01-20T07:47:32Z</dc:date>
    <item>
      <title>About Quad SPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-Quad-SPI/m-p/1212918#M167878</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am designing a circuit with DDR mode with internal sampling with Quad SPI.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;I have two questions.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;No1&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;The following is described in the NOTE of 10.2.12 Output timing in DDR mode of i.MX 7Dual Applications Processor Reference Manual.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Where is TX_DDR_DELAY_EN the Field of the register?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;TX_DDR_DELAY_EN should be set to 1 for DDR mode.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;No2&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;The Serial Clock Frequency in Table 6-50 (Quad SPI configuration parameters) can be set up to 76 MHz in DDR mode.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;The half cycle of 76MHz is 6.57ns.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;((1 / 76MHz) / 2)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;On the other hand, the TIS of Table 82 (Quad SPI Input / Read Timing) of the data sheet states that it is min 8.67ns.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Since the half cycle of 76MHz is shorter than 8.67ns, can't it be used at 76MHz?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Is my way of thinking wrong?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;best regards&lt;BR /&gt;Goto&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jan 2021 03:39:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-Quad-SPI/m-p/1212918#M167878</guid>
      <dc:creator>goto11</dc:creator>
      <dc:date>2021-01-18T03:39:57Z</dc:date>
    </item>
    <item>
      <title>About Quad SPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-Quad-SPI/m-p/1217700#M168064</link>
      <description>&lt;P&gt;1) refer to the chapter 51.13.1 Module Configuration Register (QuadSPIx_MCR) of imx6sx reference manual, you can find bit 29 TX_DDR_DELAY_EN, I think imx7d should be same&lt;/P&gt;
&lt;P&gt;2) if &lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Serial Clock Frequency&lt;/SPAN&gt;&lt;/SPAN&gt; is 76Mhz, then ths SCK=1/76=13.15ns&amp;gt; Tis+Tih, so I think this is ok&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jan 2021 07:23:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-Quad-SPI/m-p/1217700#M168064</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-01-20T07:23:12Z</dc:date>
    </item>
    <item>
      <title>Re: About Quad SPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-Quad-SPI/m-p/1217714#M168066</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In DDR mode, the data is updated with half clock,&lt;/P&gt;&lt;P&gt;so do you think SCK = (1/76MHz)/2 = 6.57ns&amp;gt; Tis + Tih should be set?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="goto11_0-1611128459314.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135278iD19DCCD740BE128A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="goto11_0-1611128459314.png" alt="goto11_0-1611128459314.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;best regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Goto&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jan 2021 07:47:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-Quad-SPI/m-p/1217714#M168066</guid>
      <dc:creator>goto11</dc:creator>
      <dc:date>2021-01-20T07:47:32Z</dc:date>
    </item>
    <item>
      <title>Re: About Quad SPI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-Quad-SPI/m-p/1219337#M168211</link>
      <description>&lt;P&gt;I know what you mean, Since it shall send Read command before reading, the QSPI READ clock frequency is set same as WRITE one in practice. The DTR(DDR) READ clock frequency is limited by Setup time (Tis = 8.67nS Min) and Hold time (Tih = 0nS Min). The minimum DTR WRITE SCK Clock Period is Tck = 20nS for i.mx7D, and it is enough for Tis = 8.67nS Min and Tih = 0nS Min.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jan 2021 05:35:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-Quad-SPI/m-p/1219337#M168211</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-01-22T05:35:20Z</dc:date>
    </item>
  </channel>
</rss>