<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6ull cannot jtag debugging in emmc startup mode</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-cannot-jtag-debugging-in-emmc-startup-mode/m-p/1217591#M168050</link>
    <description>&lt;P&gt;You can use Serial Downloader mode as Igor suggested. For the details please refer to chapter 8.9 "Serial Downloader" of the Reference Manual.&lt;/P&gt;</description>
    <pubDate>Wed, 20 Jan 2021 04:07:11 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2021-01-20T04:07:11Z</dc:date>
    <item>
      <title>imx6ull cannot jtag debugging in emmc startup mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-cannot-jtag-debugging-in-emmc-startup-mode/m-p/1212915#M167876</link>
      <description>imx6ull cannot jtag debugging in emmc startup mode,jtag show Device "MCIMX6Y2" selected. Connecting to target via JTAG ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. ConfigTargetSettings() start J-Link script: Setting up AP map ConfigTargetSettings() end Could not measure total IR len. TDO is constant high. Cannot connect to target. but Serial Downloader mode can jtag debug why?</description>
      <pubDate>Mon, 18 Jan 2021 03:37:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-cannot-jtag-debugging-in-emmc-startup-mode/m-p/1212915#M167876</guid>
      <dc:creator>debugall</dc:creator>
      <dc:date>2021-01-18T03:37:26Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ull cannot jtag debugging in emmc startup mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-cannot-jtag-debugging-in-emmc-startup-mode/m-p/1217591#M168050</link>
      <description>&lt;P&gt;You can use Serial Downloader mode as Igor suggested. For the details please refer to chapter 8.9 "Serial Downloader" of the Reference Manual.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jan 2021 04:07:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-cannot-jtag-debugging-in-emmc-startup-mode/m-p/1217591#M168050</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2021-01-20T04:07:11Z</dc:date>
    </item>
  </channel>
</rss>