<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMCIMX8M-EVKB: need help getting started with Linux</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1213385#M167942</link>
    <description>&lt;P&gt;I'm trying to use the MCIMX8M-EVKB for the first time and I can't get it to boot Linux from an SD card.&lt;/P&gt;&lt;P&gt;The &lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MQUADEVKBQSG" target="_self"&gt;Quick Start Guide&lt;/A&gt; says to check &lt;A href="http://www.nxp.com/imx8mquadevkB" target="_blank" rel="noopener"&gt;www.nxp.com/imx8mquadevkB&lt;/A&gt; for software and info, but that URL gets a Page Not Found error.&amp;nbsp; Removing the trailing B leads to the main MCIMX8M-EVK page, where I find a link to &lt;A href="https://www.nxp.com/document/guide/get-started-with-the-mcimx8m-evk:GS-MCIMX8M-EVK" target="_self"&gt;Get Started with the MCIMX8M-EVK&lt;/A&gt;.&amp;nbsp; This contains a &lt;EM&gt;Linux&lt;/EM&gt; chapter which explains using a .sdcard file to create a bootable SD card, and suggests using the &lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=L4.9.88_2.0.0_MX8MQ&amp;amp;appType=file1&amp;amp;DOWNLOAD_ID=null&amp;amp;lang_cd=en" target="_blank" rel="noopener"&gt;Linux download page&lt;/A&gt;, which is nothing but a .tar.gz file.&amp;nbsp; This archive contains only one file with "sdcard" in its name - fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard.bz2.&amp;nbsp; I assumed that I should pipe this through bunzip2 and onto an SD card, which I did, and this resulted in the SD card with valid-looking boot and root partitions, which I can read on my Linux development machine.&amp;nbsp; But nothing happens when I boot the EVK with this SD card inserted.&lt;/P&gt;&lt;P&gt;I have the serial cable working - I can boot and interact with the Android image on the eMMC.&amp;nbsp; But when I change SW801 to 1100 and power on (with the SD card inserted) there is no activity on the serial port nor the HDMI output.&amp;nbsp; The red power LED lights but that's the only sign of life.&lt;/P&gt;&lt;P&gt;How do I get a Linux image on an SD card and boot it?&amp;nbsp; I would prefer to use the serial console and not use a monitor.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Mike&lt;/P&gt;</description>
    <pubDate>Mon, 18 Jan 2021 13:54:53 GMT</pubDate>
    <dc:creator>mditto1</dc:creator>
    <dc:date>2021-01-18T13:54:53Z</dc:date>
    <item>
      <title>MCIMX8M-EVKB: need help getting started with Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1213385#M167942</link>
      <description>&lt;P&gt;I'm trying to use the MCIMX8M-EVKB for the first time and I can't get it to boot Linux from an SD card.&lt;/P&gt;&lt;P&gt;The &lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8MQUADEVKBQSG" target="_self"&gt;Quick Start Guide&lt;/A&gt; says to check &lt;A href="http://www.nxp.com/imx8mquadevkB" target="_blank" rel="noopener"&gt;www.nxp.com/imx8mquadevkB&lt;/A&gt; for software and info, but that URL gets a Page Not Found error.&amp;nbsp; Removing the trailing B leads to the main MCIMX8M-EVK page, where I find a link to &lt;A href="https://www.nxp.com/document/guide/get-started-with-the-mcimx8m-evk:GS-MCIMX8M-EVK" target="_self"&gt;Get Started with the MCIMX8M-EVK&lt;/A&gt;.&amp;nbsp; This contains a &lt;EM&gt;Linux&lt;/EM&gt; chapter which explains using a .sdcard file to create a bootable SD card, and suggests using the &lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=L4.9.88_2.0.0_MX8MQ&amp;amp;appType=file1&amp;amp;DOWNLOAD_ID=null&amp;amp;lang_cd=en" target="_blank" rel="noopener"&gt;Linux download page&lt;/A&gt;, which is nothing but a .tar.gz file.&amp;nbsp; This archive contains only one file with "sdcard" in its name - fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard.bz2.&amp;nbsp; I assumed that I should pipe this through bunzip2 and onto an SD card, which I did, and this resulted in the SD card with valid-looking boot and root partitions, which I can read on my Linux development machine.&amp;nbsp; But nothing happens when I boot the EVK with this SD card inserted.&lt;/P&gt;&lt;P&gt;I have the serial cable working - I can boot and interact with the Android image on the eMMC.&amp;nbsp; But when I change SW801 to 1100 and power on (with the SD card inserted) there is no activity on the serial port nor the HDMI output.&amp;nbsp; The red power LED lights but that's the only sign of life.&lt;/P&gt;&lt;P&gt;How do I get a Linux image on an SD card and boot it?&amp;nbsp; I would prefer to use the serial console and not use a monitor.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Mike&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jan 2021 13:54:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1213385#M167942</guid>
      <dc:creator>mditto1</dc:creator>
      <dc:date>2021-01-18T13:54:53Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX8M-EVKB: need help getting started with Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1217102#M168030</link>
      <description>&lt;P&gt;Update:&amp;nbsp; I am able to boot U-boot from eMMC, interrupt to prevent booting of Android, and use these commands to boot Linux from the SD card:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;fatload mmc 1:1 0x40480000 Image
fatload mmc 1:1 0x40470000 fsl-imx8mq-evk.dtb
setenv bootargs root=/dev/mmcblk1p2
booti 0x40480000 - 0x40470000&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't know why the SD card cant be booted directly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 20:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1217102#M168030</guid>
      <dc:creator>mditto1</dc:creator>
      <dc:date>2021-01-19T20:21:10Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX8M-EVKB: need help getting started with Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1218247#M168102</link>
      <description>&lt;P&gt;Hi mditto1,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The quick start guide is a good way to start but it has some missing points, please review the Linux guide that comes with the BSP, chapter 4.3 preparing an SD/MMC card to boot.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel H.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jan 2021 20:30:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1218247#M168102</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-01-20T20:30:51Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX8M-EVKB: need help getting started with Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1218267#M168104</link>
      <description>&lt;P&gt;I had seen that document and tried to find some clues there, but I don't see why those steps wouldn't have already been done to the prepared .sdcard image on the NXP download page.&amp;nbsp; My best guess is that the wrong version/build of U-Boot has been included in the .sdcard image, so I did try the command in 4.3.4 with what seemed like the right U-Boot image, but it didn't help. &amp;nbsp;The image I copied was imx-boot-imx8mqddr4arm2-sd.bin-flash_ddr4_arm2 , should that have worked?&amp;nbsp; Is there anything else needed to get the board to load U-Boot from the SD card, perhaps a boot sector or something?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jan 2021 21:38:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1218267#M168104</guid>
      <dc:creator>mditto1</dc:creator>
      <dc:date>2021-01-20T21:38:38Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX8M-EVKB: need help getting started with Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1218307#M168106</link>
      <description>&lt;P&gt;Hi mditto1,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you review the ROM configures the boot media and attempts to read the image from a predefined address in the boot device, probably the boot media is trying to start from a different address, all of this comes on the reference manual but see the table below:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Selection_429.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135363i2028ACED7C1CA4F8/image-size/large?v=v2&amp;amp;px=999" role="button" title="Selection_429.png" alt="Selection_429.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also please take a look into the next post, hope this help you:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-Boot-process-and-creating-a-bootable-image/ta-p/1101253" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-Boot-process-and-creating-a-bootable-image/ta-p/1101253&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel H.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jan 2021 22:54:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1218307#M168106</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-01-20T22:54:55Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX8M-EVKB: need help getting started with Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1218933#M168176</link>
      <description>&lt;P&gt;Hi, Israel, thanks for the information.&lt;/P&gt;&lt;P&gt;&lt;U&gt;i.MX Linux® User's Guide&lt;/U&gt; section 4.3.4 says boot offset is 33 k for i.MX 8M Quad.&lt;BR /&gt;&lt;U&gt;i.MX8 Boot process and creating a bootable image&lt;/U&gt; table 5-22 says boot offset is 32 k.&lt;BR /&gt;The .sdcard image on the download page has a bootloader image at 33 k.&lt;/P&gt;&lt;P&gt;I've tried both locations, still no signs of life.&amp;nbsp; Can you confirm I am using the right U-Boot image?&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;&lt;STRONG&gt;imx-boot-imx8mqddr4arm2-sd.bin-flash_ddr4_arm2&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;U&gt;i.MX8 Boot process and creating a bootable image&lt;/U&gt; table 5-8 says boot switches should be 0011, I'm assuming that means ON-ON-OFF-OFF as described elsewhere.&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jan 2021 15:44:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1218933#M168176</guid>
      <dc:creator>mditto1</dc:creator>
      <dc:date>2021-01-21T15:44:53Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX8M-EVKB: need help getting started with Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1219895#M168262</link>
      <description>&lt;P&gt;.&lt;/P&gt;</description>
      <pubDate>Sat, 23 Jan 2021 02:03:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1219895#M168262</guid>
      <dc:creator>Luishernandez1</dc:creator>
      <dc:date>2021-01-23T02:03:35Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX8M-EVKB: need help getting started with Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1219897#M168263</link>
      <description>&lt;P&gt;Hi Mike,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;No, that U-boot file is one we usually use to validate our DDR4 boards, please use the imx-boot-imx8mqevk-sd.bin-flash_evk, a tell me if this works for you, follow the same as Linux user's guide 4.3.4 to flash the SD card.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, you can use Yocto to create and compile the image for your device, just to discard problems that may come with your image. Please follow the documentation that comes with the BSP.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps you.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Israel H.&lt;/P&gt;</description>
      <pubDate>Sat, 23 Jan 2021 02:05:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1219897#M168263</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-01-23T02:05:28Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX8M-EVKB: need help getting started with Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1219909#M168265</link>
      <description>&lt;P&gt;No, no difference.&lt;/P&gt;&lt;P&gt;I wonder if it's because I'm using an SDHC card.&amp;nbsp; Maybe the boot ROM doesn't support SDHC but U-Boot does (thus it works when I load U-Boot from eMMC)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 23 Jan 2021 06:50:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1219909#M168265</guid>
      <dc:creator>mditto1</dc:creator>
      <dc:date>2021-01-23T06:50:32Z</dc:date>
    </item>
    <item>
      <title>Re: MCIMX8M-EVKB: need help getting started with Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1228243#M169170</link>
      <description>&lt;P&gt;I found an sdcard image in the L5.4.70_2.3.0_MX8MND3L BSP download, and it just works, no trouble at all.&amp;nbsp; I downloaded it from here:&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab&lt;/A&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;The command to write it to an SD card:&lt;BR /&gt;&lt;/FONT&gt;&lt;FONT face="courier new,courier"&gt;dd if=imx-image-full-imx8mqevk.wic of=/dev/sda bs=1048576&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;I don't know what is wrong with the sdcard image in the "Get Started" and "Linux download" pages, but the one in the BSP package ("&lt;FONT face="courier new,courier"&gt;.wic&lt;/FONT&gt;" file instead of "&lt;FONT face="courier new,courier"&gt;.sdcard&lt;/FONT&gt;") works fine for me and my problem is solved.&lt;/P&gt;&lt;P&gt;Cheers,&lt;BR /&gt;Mike&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 21:08:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCIMX8M-EVKB-need-help-getting-started-with-Linux/m-p/1228243#M169170</guid>
      <dc:creator>mditto1</dc:creator>
      <dc:date>2021-02-08T21:08:33Z</dc:date>
    </item>
  </channel>
</rss>