<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6UL ADC: VrefH input current</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-ADC-VrefH-input-current/m-p/1212371#M167822</link>
    <description>&lt;P&gt;The ADC_VREFH pin behaves as a regular FET gate input, so, its leakage current is negligible.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
    <pubDate>Fri, 15 Jan 2021 11:55:42 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2021-01-15T11:55:42Z</dc:date>
    <item>
      <title>i.MX6UL ADC: VrefH input current</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-ADC-VrefH-input-current/m-p/1209497#M167537</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;We are designing an application with the i.MX6UL's internal ADC in use. An external shut voltage reference is connected to the SoC's VrefH input.&lt;/P&gt;&lt;P&gt;However, the datasheet of the i.MX6UL does not specify the input current on pin VrefH. Thus, I cannot calculate an appropriate bias current for the shunt reference. Is this value known?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Johannes&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 08:20:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-ADC-VrefH-input-current/m-p/1209497#M167537</guid>
      <dc:creator>johannesdev</dc:creator>
      <dc:date>2021-01-11T08:20:22Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL ADC: VrefH input current</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-ADC-VrefH-input-current/m-p/1212371#M167822</link>
      <description>&lt;P&gt;The ADC_VREFH pin behaves as a regular FET gate input, so, its leakage current is negligible.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jan 2021 11:55:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6UL-ADC-VrefH-input-current/m-p/1212371#M167822</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2021-01-15T11:55:42Z</dc:date>
    </item>
  </channel>
</rss>