<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8MQEVK - Linux Yocto BSP setup in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQEVK-Linux-Yocto-BSP-setup/m-p/1211706#M167756</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have setup the Yocto build system for IMX6SX using Linux 4.9.88 as mentioned on the User guide - i.MX Yocto Project User's Guide, Rev. L4.9.88_2.0.0-ga, 05/2018.&lt;/P&gt;&lt;P&gt;For IMX6Sx I completed, the setup.&lt;/P&gt;&lt;P&gt;Can I use the same directory to setup for IMX8MQEVK, just by using DISTRO=&amp;lt;&amp;gt; MACHINE=&amp;lt;&amp;gt; command for imx8m?&lt;/P&gt;&lt;P&gt;or I need to use the different directory/version of toolchain BSP?&lt;/P&gt;&lt;P&gt;Kindly explain in detail, as this IMX/Yocto platform is new to me.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 14 Jan 2021 10:18:51 GMT</pubDate>
    <dc:creator>JKT</dc:creator>
    <dc:date>2021-01-14T10:18:51Z</dc:date>
    <item>
      <title>IMX8MQEVK - Linux Yocto BSP setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQEVK-Linux-Yocto-BSP-setup/m-p/1211706#M167756</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have setup the Yocto build system for IMX6SX using Linux 4.9.88 as mentioned on the User guide - i.MX Yocto Project User's Guide, Rev. L4.9.88_2.0.0-ga, 05/2018.&lt;/P&gt;&lt;P&gt;For IMX6Sx I completed, the setup.&lt;/P&gt;&lt;P&gt;Can I use the same directory to setup for IMX8MQEVK, just by using DISTRO=&amp;lt;&amp;gt; MACHINE=&amp;lt;&amp;gt; command for imx8m?&lt;/P&gt;&lt;P&gt;or I need to use the different directory/version of toolchain BSP?&lt;/P&gt;&lt;P&gt;Kindly explain in detail, as this IMX/Yocto platform is new to me.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 10:18:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQEVK-Linux-Yocto-BSP-setup/m-p/1211706#M167756</guid>
      <dc:creator>JKT</dc:creator>
      <dc:date>2021-01-14T10:18:51Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQEVK - Linux Yocto BSP setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQEVK-Linux-Yocto-BSP-setup/m-p/1218636#M168144</link>
      <description>&lt;P&gt;Yes, you can use if you do have enough disk space. Just use the different name if do not deleted the one you have created.&lt;/P&gt;
&lt;P&gt;$ DISTRO=**** MACHINE=imx8mqevk *** "New directory name"&lt;/P&gt;
&lt;P&gt;$ bitbake ****&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jan 2021 08:19:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQEVK-Linux-Yocto-BSP-setup/m-p/1218636#M168144</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2021-01-21T08:19:36Z</dc:date>
    </item>
  </channel>
</rss>