<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Switching framebuffer data lines for IMX8MM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1210998#M167682</link>
    <description>&lt;P&gt;i.mx8mm only one input buffer up to 1080p, I think you can use duplicates screens, but refer to your document, it seems that you want to use seperate display, I don't think imx8mm could support it,&lt;/P&gt;</description>
    <pubDate>Wed, 13 Jan 2021 08:50:57 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2021-01-13T08:50:57Z</dc:date>
    <item>
      <title>Switching framebuffer data lines for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1210176#M167608</link>
      <description>&lt;P&gt;Hi Team&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to use 2 MIPI DSI LCD connected IMX8MM processor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using a switcher in between to toggle the display between the two. As of now I am able to blank and unblank both the screens. But I want that both the LCDs remain active at the same time. Like the framebuffer data lines be allocated to each of the LCDs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I modify the FB driver to allocate data lines to each of the LCDs individually? Can you help me with the same?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jan 2021 07:46:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1210176#M167608</guid>
      <dc:creator>rajvikamdar</dc:creator>
      <dc:date>2021-01-12T07:46:15Z</dc:date>
    </item>
    <item>
      <title>Re: Switching framebuffer data lines for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1210701#M167650</link>
      <description>&lt;P&gt;what switcher do you use? did you connect switcher to the mipi dsi? i.mx8 series don't support framebuffer driver anymore&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jan 2021 02:13:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1210701#M167650</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-01-13T02:13:12Z</dc:date>
    </item>
    <item>
      <title>Re: Switching framebuffer data lines for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1210870#M167666</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using mipi dsi switcher FSA641-D from ON semiconductor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am not getting how can I switch writing on fb0 from the driver or userspace.&lt;/P&gt;&lt;P&gt;So that the same image can be displayed on LCD after continuous switching between the two LCDs.&lt;/P&gt;&lt;P&gt;MiPI switch works on chip select line, of CS =0 then LCD A will be selected and CS=1&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jan 2021 06:25:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1210870#M167666</guid>
      <dc:creator>rajvikamdar</dc:creator>
      <dc:date>2021-01-13T06:25:58Z</dc:date>
    </item>
    <item>
      <title>Re: Switching framebuffer data lines for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1210998#M167682</link>
      <description>&lt;P&gt;i.mx8mm only one input buffer up to 1080p, I think you can use duplicates screens, but refer to your document, it seems that you want to use seperate display, I don't think imx8mm could support it,&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jan 2021 08:50:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1210998#M167682</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-01-13T08:50:57Z</dc:date>
    </item>
    <item>
      <title>Re: Switching framebuffer data lines for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1211014#M167685</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you tell me how can I use duplicate screens?&lt;/P&gt;&lt;P&gt;And which part of the driver code executes writing DSI from userspace fb0?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jan 2021 09:03:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1211014#M167685</guid>
      <dc:creator>rajvikamdar</dc:creator>
      <dc:date>2021-01-13T09:03:47Z</dc:date>
    </item>
    <item>
      <title>Re: Switching framebuffer data lines for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1213261#M167917</link>
      <description>&lt;P&gt;I don't have such sample code, for imx8mm, don't use frame buffer driver anymore, you can refer to the mipi dsi driver as below:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/drm/imx/sec_mipi_dsim-imx.c?h=imx_4.14.98_2.0.0_ga" target="_blank"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/drm/imx/sec_mipi_dsim-imx.c?h=imx_4.14.98_2.0.0_ga&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jan 2021 10:01:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1213261#M167917</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-01-18T10:01:45Z</dc:date>
    </item>
    <item>
      <title>Re: Switching framebuffer data lines for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1216642#M167986</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can we by any means switch the input buffer? When the image writes on the buffer, we want to switch at that point of time?&lt;/P&gt;&lt;P&gt;Is that possible?&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 07:54:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1216642#M167986</guid>
      <dc:creator>rajvikamdar</dc:creator>
      <dc:date>2021-01-19T07:54:52Z</dc:date>
    </item>
    <item>
      <title>Re: Switching framebuffer data lines for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1219903#M168264</link>
      <description>&lt;P&gt;I mean that maybe the third party bridge can support duplicates screens, for imx8mm, only one display controller which couldn't support two displays&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 23 Jan 2021 03:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Switching-framebuffer-data-lines-for-IMX8MM/m-p/1219903#M168264</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-01-23T03:55:25Z</dc:date>
    </item>
  </channel>
</rss>