<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMIPI CSI interface maximum capability</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-interface-maximum-capability/m-p/1209977#M167581</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; We wanna interface 2x1080p60 YUV422 format camera to IMX8DX processor.&lt;/P&gt;&lt;P&gt;(1)Can MIPI CSI interface support it?&lt;/P&gt;&lt;P&gt;(2)Does SDK have sample code for it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; thx.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 12 Jan 2021 01:55:58 GMT</pubDate>
    <dc:creator>Issac_20200908</dc:creator>
    <dc:date>2021-01-12T01:55:58Z</dc:date>
    <item>
      <title>MIPI CSI interface maximum capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-interface-maximum-capability/m-p/1209977#M167581</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; We wanna interface 2x1080p60 YUV422 format camera to IMX8DX processor.&lt;/P&gt;&lt;P&gt;(1)Can MIPI CSI interface support it?&lt;/P&gt;&lt;P&gt;(2)Does SDK have sample code for it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; thx.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jan 2021 01:55:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-interface-maximum-capability/m-p/1209977#M167581</guid>
      <dc:creator>Issac_20200908</dc:creator>
      <dc:date>2021-01-12T01:55:58Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI CSI interface maximum capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-interface-maximum-capability/m-p/1210049#M167593</link>
      <description>&lt;P&gt;1) refer to the data sheet, The MIPI CSI-2 IP provides MIPI CSI-2 standard camera interface ports. The MIPI CSI-2 interface supports up to 1.5 Gbps for up to 4 data lanes, so the mipi csi can support up to 6Gbps, but one &lt;A href="mailto:1080p@60" target="_blank"&gt;1080p@60&lt;/A&gt; needs 3.54Gbsp, so I thinks imx8dx only can support one &lt;A href="mailto:1080p@60" target="_blank"&gt;1080p@60&lt;/A&gt; camera&lt;/P&gt;
&lt;P&gt;2)I checked imx8qxp sdk, can find the mipi csi driver, the code is under folder devices&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jan 2021 03:42:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-interface-maximum-capability/m-p/1210049#M167593</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-01-12T03:42:11Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI CSI interface maximum capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-interface-maximum-capability/m-p/1210094#M167599</link>
      <description>&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a question on the total bandwidth needed for one 1080p60 YUV422 format video. I added 35% extra blank bits for the MIPI CSI tranfer (a estimation formula in an iMX6Q doc), and got 2.687Gbps. That's&lt;/P&gt;&lt;P&gt;1920x1080x16x1.35=2.687G bps&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How did you get that one &lt;A href="mailto:1080p@60" target="_blank"&gt;1080p@60&lt;/A&gt; needs 3.54G bps?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jan 2021 05:30:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-interface-maximum-capability/m-p/1210094#M167599</guid>
      <dc:creator>Issac_20200908</dc:creator>
      <dc:date>2021-01-12T05:30:24Z</dc:date>
    </item>
    <item>
      <title>Re: MIPI CSI interface maximum capability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-interface-maximum-capability/m-p/1211543#M167732</link>
      <description>&lt;P&gt;the forum you use isn't correct, for the forum you use is for frequency (Mhz), not for bandwidth(bps)&lt;/P&gt;
&lt;P&gt;The required operating frequency of the interface is calculated in the following way:&lt;BR /&gt;F = FH * FW * FPS * BI * DF&lt;BR /&gt;Where&lt;BR /&gt;• FH = frame height (in pixels)&lt;BR /&gt;• FW = Frame width (in pixels)&lt;BR /&gt;• fps = frame rate (frames per second)&lt;BR /&gt;• BI = typically 35% overhead, should be assumed as 1.35. The actual blanking&lt;BR /&gt;intervals are a parameter of the attached device.&lt;BR /&gt;• DF = data format, defines the number of cycles needed to send a single pixel.&lt;BR /&gt;The number of cycles needed to send a single pixel depends on the interface and the data&lt;BR /&gt;format.&lt;BR /&gt;Data format examples:&lt;BR /&gt;• YUV422 over 16 bit = 1 cycle/pixel&lt;BR /&gt;• RGB888 over 8 bit = 3 cycles/pixel&lt;BR /&gt;• RGB565 over 16 bit = 1 cycle/pixel&lt;BR /&gt;• Bayer/Generic data = 1 cycle/pixel&lt;BR /&gt;• YUV422 over 8 bit = 2 cycles/pixel&lt;BR /&gt;• BT.656, YUV422 format = 2 cycles/pixel&lt;BR /&gt;• BT.1120, YUV422 format = 1 cycle/pixel&lt;/P&gt;
&lt;P&gt;sorry for my mistake, I don't find you use yuv422, if you use yuv422 16bits, imx8 can support dual camera, for 1080p, typical frequency is 148.5MHZ, the bandwidth is 148.5MHZx16bpp=2.376Gbps&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 06:49:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIPI-CSI-interface-maximum-capability/m-p/1211543#M167732</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-01-14T06:49:03Z</dc:date>
    </item>
  </channel>
</rss>