<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックBOOT mode iMX8MM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-mode-iMX8MM/m-p/1209787#M167561</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;we have board with imx8m mini.&amp;nbsp;&lt;/P&gt;&lt;P&gt;we set BOOT_MODE1 and BOOT_MODE0 pins to 1 and 0 ( internal boot mode).&lt;/P&gt;&lt;P&gt;We have BT_FUSE_SEL =0 so a boot configuration is done by GPIOs.&lt;/P&gt;&lt;P&gt;We select then BOOT_CFG[14:12] to select eMMC (usdhc1).&lt;/P&gt;&lt;P&gt;SD manufacture mode is not disabled.&lt;/P&gt;&lt;P&gt;This works, the image from eMMC is loaded correctly.&lt;/P&gt;&lt;P&gt;When image on eMMC is not correct and boot is stuck if we insert SD on usbhc2 with valid image this is booted correctly.&lt;/P&gt;&lt;P&gt;Two questions :&lt;/P&gt;&lt;P&gt;1) is the image on SD in this case loaded because of the manufacture SD boot ? or is it because of other reason ? Does the bootloader try eMMC, then SD card, then serial download also when in this internal boot mode ?&lt;/P&gt;&lt;P&gt;2) if we had BT_FUSE_SEL set to 1 and fuses selecting eMMC, rather than GPIOs selecting it , as boot device would the behaviour , falling to SD card boot, be the same in the case the image on emmc was corrupted ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 11 Jan 2021 16:24:06 GMT</pubDate>
    <dc:creator>antonio_santagi</dc:creator>
    <dc:date>2021-01-11T16:24:06Z</dc:date>
    <item>
      <title>BOOT mode iMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-mode-iMX8MM/m-p/1209787#M167561</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;we have board with imx8m mini.&amp;nbsp;&lt;/P&gt;&lt;P&gt;we set BOOT_MODE1 and BOOT_MODE0 pins to 1 and 0 ( internal boot mode).&lt;/P&gt;&lt;P&gt;We have BT_FUSE_SEL =0 so a boot configuration is done by GPIOs.&lt;/P&gt;&lt;P&gt;We select then BOOT_CFG[14:12] to select eMMC (usdhc1).&lt;/P&gt;&lt;P&gt;SD manufacture mode is not disabled.&lt;/P&gt;&lt;P&gt;This works, the image from eMMC is loaded correctly.&lt;/P&gt;&lt;P&gt;When image on eMMC is not correct and boot is stuck if we insert SD on usbhc2 with valid image this is booted correctly.&lt;/P&gt;&lt;P&gt;Two questions :&lt;/P&gt;&lt;P&gt;1) is the image on SD in this case loaded because of the manufacture SD boot ? or is it because of other reason ? Does the bootloader try eMMC, then SD card, then serial download also when in this internal boot mode ?&lt;/P&gt;&lt;P&gt;2) if we had BT_FUSE_SEL set to 1 and fuses selecting eMMC, rather than GPIOs selecting it , as boot device would the behaviour , falling to SD card boot, be the same in the case the image on emmc was corrupted ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 16:24:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-mode-iMX8MM/m-p/1209787#M167561</guid>
      <dc:creator>antonio_santagi</dc:creator>
      <dc:date>2021-01-11T16:24:06Z</dc:date>
    </item>
    <item>
      <title>Re: BOOT mode iMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-mode-iMX8MM/m-p/1211393#M167718</link>
      <description>&lt;P&gt;Hi Antonio,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For the first question, as you said it is load it because is activate the manufacture boot; and also because the boot loader will try to follow the flow boot that you can find on the Reference manual&amp;nbsp;Figure 6-1. Boot flow.&lt;/P&gt;
&lt;P&gt;For the second question is yes, it would be the same result.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this help you.&lt;/P&gt;
&lt;P&gt;Regard,&lt;/P&gt;
&lt;P&gt;Israel H.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 00:13:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-mode-iMX8MM/m-p/1211393#M167718</guid>
      <dc:creator>nxf63675</dc:creator>
      <dc:date>2021-01-14T00:13:55Z</dc:date>
    </item>
  </channel>
</rss>