<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic eMMC HS400 mode in IMX8QXP U-Boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-HS400-mode-in-IMX8QXP-U-Boot/m-p/1209462#M167527</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are trying to enable eMMC HS400 mode in uboot in IMX8QXP based custom board.&lt;BR /&gt;In one board we got the following error when enabling HS400 mode, while in another board it is working fine.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;CPU: NXP i.MX8QXP RevC A35 at 1200 MHz at 43C&lt;/EM&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;Boot: MMC0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DRAM: 1022 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Loading Environment from MMC... Select HS400 failed -70&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;*** Warning - bad CRC, using default environment&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;In: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Out: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Err: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Select HS400 failed -70&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;switch to partitions #0, OK&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmc0(part 0) is current device&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;flash target is MMC:0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Select HS400 failed -70&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;We have tested with values 0 to 7 for fsl,strobe-dll-delay-target value in usdhc node of u-boot device tree but this error still persists.&lt;/P&gt;&lt;P&gt;We suspect HS400 mode switching is failed due to the failure in the tuning process.&lt;/P&gt;&lt;P&gt;We have also checked the following parameters in usdhc node in u-boot device tree.&lt;BR /&gt;1) fsl,start-tuning-tap&lt;BR /&gt;2) fsl,tuning-step&lt;BR /&gt;We are trying to find out the range of values that can be given to these parameters for testing.&lt;BR /&gt;Referring the u-boot source code in driver/mmc/fsl_esdhc_imx.c, following parameters are read from the device tree and updated in TUNING_CTRL register. But when we refer the IMX8QXP reference manual(IMX8DQXPRM.pdf), we could not find any details&amp;nbsp;of TUNING_CTRL register.&lt;/P&gt;&lt;P&gt;Could you please give any information about TUNING_CTRL register?.&lt;/P&gt;&lt;P&gt;Could you please give any hints to resolve this issue.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Mon, 11 Jan 2021 06:51:42 GMT</pubDate>
    <dc:creator>masood_ahamed</dc:creator>
    <dc:date>2021-01-11T06:51:42Z</dc:date>
    <item>
      <title>eMMC HS400 mode in IMX8QXP U-Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-HS400-mode-in-IMX8QXP-U-Boot/m-p/1209462#M167527</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are trying to enable eMMC HS400 mode in uboot in IMX8QXP based custom board.&lt;BR /&gt;In one board we got the following error when enabling HS400 mode, while in another board it is working fine.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;CPU: NXP i.MX8QXP RevC A35 at 1200 MHz at 43C&lt;/EM&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;Boot: MMC0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;DRAM: 1022 MiB&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Loading Environment from MMC... Select HS400 failed -70&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;*** Warning - bad CRC, using default environment&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;In: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Out: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Err: serial&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Select HS400 failed -70&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;switch to partitions #0, OK&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;mmc0(part 0) is current device&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;flash target is MMC:0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Select HS400 failed -70&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;We have tested with values 0 to 7 for fsl,strobe-dll-delay-target value in usdhc node of u-boot device tree but this error still persists.&lt;/P&gt;&lt;P&gt;We suspect HS400 mode switching is failed due to the failure in the tuning process.&lt;/P&gt;&lt;P&gt;We have also checked the following parameters in usdhc node in u-boot device tree.&lt;BR /&gt;1) fsl,start-tuning-tap&lt;BR /&gt;2) fsl,tuning-step&lt;BR /&gt;We are trying to find out the range of values that can be given to these parameters for testing.&lt;BR /&gt;Referring the u-boot source code in driver/mmc/fsl_esdhc_imx.c, following parameters are read from the device tree and updated in TUNING_CTRL register. But when we refer the IMX8QXP reference manual(IMX8DQXPRM.pdf), we could not find any details&amp;nbsp;of TUNING_CTRL register.&lt;/P&gt;&lt;P&gt;Could you please give any information about TUNING_CTRL register?.&lt;/P&gt;&lt;P&gt;Could you please give any hints to resolve this issue.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 06:51:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-HS400-mode-in-IMX8QXP-U-Boot/m-p/1209462#M167527</guid>
      <dc:creator>masood_ahamed</dc:creator>
      <dc:date>2021-01-11T06:51:42Z</dc:date>
    </item>
    <item>
      <title>Re: eMMC HS400 mode in IMX8QXP U-Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-HS400-mode-in-IMX8QXP-U-Boot/m-p/1209483#M167532</link>
      <description>&lt;P&gt;Hi masood_ahamed&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;if issue appears only on one board it may be related to manufacturing process, for&lt;/P&gt;
&lt;P&gt;example poor soldering. One can try to resolder chip. Also this may be related to&lt;/P&gt;
&lt;P&gt;board noise, one can recheck power supplies using&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_2" href="https://www.nxp.com/webapp/Download?colCode=IMX8HWDG" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8QuadMax/i.MX 8QuadXPlus Hardware Developer’s Guide&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;gt;Could you please give any information about TUNING_CTRL register?.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I am afraid such details are not available, sorry.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 07:46:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-HS400-mode-in-IMX8QXP-U-Boot/m-p/1209483#M167532</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-01-11T07:46:12Z</dc:date>
    </item>
  </channel>
</rss>