<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックcompile BUSYBOX for IMX8MM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/compile-BUSYBOX-for-IMX8MM/m-p/1209454#M167526</link>
    <description>&lt;P&gt;use .config in busybox to "make" "make install".Generate "busybox" file. Different from file(busybox.nosuid,busybox.suid) in rootfs.There is a problem with the replacement file.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can only yocto compile busybox?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 11 Jan 2021 06:44:18 GMT</pubDate>
    <dc:creator>xfg</dc:creator>
    <dc:date>2021-01-11T06:44:18Z</dc:date>
    <item>
      <title>compile BUSYBOX for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/compile-BUSYBOX-for-IMX8MM/m-p/1209454#M167526</link>
      <description>&lt;P&gt;use .config in busybox to "make" "make install".Generate "busybox" file. Different from file(busybox.nosuid,busybox.suid) in rootfs.There is a problem with the replacement file.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can only yocto compile busybox?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 06:44:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/compile-BUSYBOX-for-IMX8MM/m-p/1209454#M167526</guid>
      <dc:creator>xfg</dc:creator>
      <dc:date>2021-01-11T06:44:18Z</dc:date>
    </item>
    <item>
      <title>Re: compile BUSYBOX for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/compile-BUSYBOX-for-IMX8MM/m-p/1209474#M167529</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Who can use yocto to compile support Chinese BusyBox provided&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 07:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/compile-BUSYBOX-for-IMX8MM/m-p/1209474#M167529</guid>
      <dc:creator>xfg</dc:creator>
      <dc:date>2021-01-11T07:16:51Z</dc:date>
    </item>
    <item>
      <title>Re: compile BUSYBOX for IMX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/compile-BUSYBOX-for-IMX8MM/m-p/1209711#M167556</link>
      <description>&lt;P&gt;Hello xfg,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please use the attached file to replace sources/poky/bitbake/lib/bb/&lt;A href="https://utils.py" target="_blank" rel="nofollow noopener noreferrer"&gt;utils.py&lt;/A&gt;, which have already applied the patch &lt;A href="https://patchwork.openembedded.org/patch/122361/" target="_blank" rel="nofollow noopener noreferrer"&gt;https://patchwork.openembedded.org/patch/122361/&lt;/A&gt;. &lt;BR /&gt;&lt;BR /&gt;Please add the following in sources/meta-freescale/recipes-fsl/images/&lt;A href="https://fsl-image-core.bb" target="_blank" rel="nofollow noopener noreferrer"&gt;fsl-image-core.bb&lt;/A&gt; &lt;BR /&gt;&lt;BR /&gt;GLIBC_GENERATE_LOCALES = "zh_CN.UTF-8 en_GB.UTF-8 en_US.UTF-8" &lt;BR /&gt;IMAGE_LINGUAS = "zh-cn" &lt;BR /&gt;LOCALE_UTF8_ONLY="1" &lt;BR /&gt;&lt;BR /&gt;The regenerate rootfs filesystem with "bitbake fsl-image-core". &lt;BR /&gt;&lt;BR /&gt;Please refer to the following on the target board. &lt;BR /&gt;root@t2080rdb:~# locale -a &lt;BR /&gt;C &lt;BR /&gt;zh_CN&lt;BR /&gt;POSIX &lt;BR /&gt;root@t2080rdb:~# export LANG=zh_CN.UTF-8 &lt;BR /&gt;root@t2080rdb:~# export LC_ALL=zh_CN.UTF-8 &lt;BR /&gt;root@t2080rdb:~# locale&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 14:34:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/compile-BUSYBOX-for-IMX8MM/m-p/1209711#M167556</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-01-11T14:34:35Z</dc:date>
    </item>
  </channel>
</rss>