<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHow we can invalidation the Power saving state in PCIe Gen1?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-we-can-invalidation-the-Power-saving-state-in-PCIe-Gen1/m-p/1208018#M167392</link>
    <description>&lt;P&gt;Hi community&lt;/P&gt;&lt;P&gt;I am using a custom board that design based on NXP i.MX6Q sabreauto board,&lt;BR /&gt;and we need to run PCIe device on our custom board.&lt;/P&gt;&lt;P&gt;We must use Yocto Sumo(linux kernel 4.14.78) environment.&lt;BR /&gt;We would like to invalidation the Power saving state of PCIe(L0s,L1).&lt;/P&gt;&lt;P&gt;How we can invalidation the Power saving state(not transition from L0) in PCIe Gen1?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Toshihiro Kambe&lt;/P&gt;</description>
    <pubDate>Thu, 07 Jan 2021 05:41:21 GMT</pubDate>
    <dc:creator>toshihiro_kambe</dc:creator>
    <dc:date>2021-01-07T05:41:21Z</dc:date>
    <item>
      <title>How we can invalidation the Power saving state in PCIe Gen1?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-we-can-invalidation-the-Power-saving-state-in-PCIe-Gen1/m-p/1208018#M167392</link>
      <description>&lt;P&gt;Hi community&lt;/P&gt;&lt;P&gt;I am using a custom board that design based on NXP i.MX6Q sabreauto board,&lt;BR /&gt;and we need to run PCIe device on our custom board.&lt;/P&gt;&lt;P&gt;We must use Yocto Sumo(linux kernel 4.14.78) environment.&lt;BR /&gt;We would like to invalidation the Power saving state of PCIe(L0s,L1).&lt;/P&gt;&lt;P&gt;How we can invalidation the Power saving state(not transition from L0) in PCIe Gen1?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Toshihiro Kambe&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jan 2021 05:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-we-can-invalidation-the-Power-saving-state-in-PCIe-Gen1/m-p/1208018#M167392</guid>
      <dc:creator>toshihiro_kambe</dc:creator>
      <dc:date>2021-01-07T05:41:21Z</dc:date>
    </item>
    <item>
      <title>Re: How we can invalidation the Power saving state in PCIe Gen1?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-we-can-invalidation-the-Power-saving-state-in-PCIe-Gen1/m-p/1208862#M167468</link>
      <description>&lt;P&gt;Hi Toshihiro ,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b" data-language-for-alternatives="en" data-language-to-translate-into="zh-CN" data-phrase-index="0"&gt;&lt;SPAN&gt;L1 &amp;amp; L0s are not related to GEN1/GEN2. For PCIE, as long as RC and EP support it, it can be enabled.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;
&lt;P&gt;B.R,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jan 2021 09:53:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-we-can-invalidation-the-Power-saving-state-in-PCIe-Gen1/m-p/1208862#M167468</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2021-01-08T09:53:30Z</dc:date>
    </item>
  </channel>
</rss>