<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Add network manager component in the BSP Fail in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Add-network-manager-component-in-the-BSP-Fail/m-p/1207322#M167326</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I tried successfully with add following to local.conf&amp;nbsp; :&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;IMAGE_INSTALL += "networkmanager networkmanager-nmtui networkmanager-bash-completion"&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Zhiming&lt;/P&gt;</description>
    <pubDate>Wed, 06 Jan 2021 07:08:49 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2021-01-06T07:08:49Z</dc:date>
    <item>
      <title>Add network manager component in the BSP Fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Add-network-manager-component-in-the-BSP-Fail/m-p/1207263#M167319</link>
      <description>&lt;P&gt;HI, My BSP is L5.4.47_2.2.0 version. we would like to add network manager (nmcli) in the BSP.&lt;/P&gt;&lt;P&gt;Below is our conf file.&lt;/P&gt;&lt;P&gt;# Add additional software&lt;BR /&gt;IMAGE_INSTALL_append = " packagegroup-qt5-webengine nginx spawn-fcgi qtvirtualkeyboard networkmanager"&lt;/P&gt;&lt;P&gt;But we bitbake the imx-image-full has error messages.&lt;/P&gt;&lt;P&gt;The root cause is packagegroup-core-tools-testapps needs connman-client component.&lt;/P&gt;&lt;P&gt;As I know, the connman component and network manager component cannot exists at the same time.&lt;/P&gt;&lt;P&gt;How can we fix this problem?&lt;/P&gt;&lt;P&gt;ERROR: imx-image-full-1.0-r0 do_rootfs: Unable to install packages. Command '/home/hank/WP6000/build-xwayland/tmp/work/wp6000-poky-linux/imx-image-full/1.0-r0/recipe-sysroot-native/usr/bin/apt-get install --force-yes --allow-unauthenticated --no-remove apt dpkg jailhouse networkmanager nginx opencv-apps opencv-samples packagegroup-base-extended packagegroup-core-boot packagegroup-core-full-cmdline packagegroup-core-nfs-server packagegroup-core-ssh-dropbear packagegroup-core-tools-debug packagegroup-core-tools-profile packagegroup-core-tools-testapps packagegroup-fsl-gstreamer1.0 packagegroup-fsl-gstreamer1.0-full packagegroup-fsl-tools-audio packagegroup-fsl-tools-benchmark packagegroup-fsl-tools-gpu packagegroup-fsl-tools-gpu-external packagegroup-fsl-tools-testapps packagegroup-imx-ml packagegroup-qt5-imx packagegroup-qt5-webengine packagegroup-tools-bluetooth psplash python3-opencv libqt5virtualkeyboard5 run-postinsts spawn-fcgi weston-init weston-xwayland xterm' returned 100:&lt;BR /&gt;Reading package lists...&lt;BR /&gt;Building dependency tree...&lt;BR /&gt;Reading state information...&lt;BR /&gt;Some packages could not be installed. This may mean that you have&lt;BR /&gt;requested an impossible situation or if you are using the unstable&lt;BR /&gt;distribution that some required packages have not yet been created&lt;BR /&gt;or been moved out of Incoming.&lt;BR /&gt;The following information may help to resolve the situation:&lt;/P&gt;&lt;P&gt;The following packages have unmet dependencies:&lt;BR /&gt;packagegroup-core-tools-testapps : Depends: connman-client but it is not going to be installed&lt;BR /&gt;Depends: connman-tools but it is not going to be installed&lt;BR /&gt;E: Unable to correct problems, you have held broken packages.&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/hank/WP6000/build-xwayland/tmp/work/wp6000-poky-linux/imx-image-full/1.0-r0/temp/log.do_rootfs.21162&lt;BR /&gt;ERROR: Task (/home/hank/WP6000/sources/meta-imx/meta-sdk/dynamic-layers/qt5-layer/recipes-fsl/images/imx-image-full.bb:do_rootfs) failed with exit code '1'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jan 2021 05:39:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Add-network-manager-component-in-the-BSP-Fail/m-p/1207263#M167319</guid>
      <dc:creator>hankwang</dc:creator>
      <dc:date>2021-01-06T05:39:38Z</dc:date>
    </item>
    <item>
      <title>Re: Add network manager component in the BSP Fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Add-network-manager-component-in-the-BSP-Fail/m-p/1207322#M167326</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I tried successfully with add following to local.conf&amp;nbsp; :&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;IMAGE_INSTALL += "networkmanager networkmanager-nmtui networkmanager-bash-completion"&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jan 2021 07:08:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Add-network-manager-component-in-the-BSP-Fail/m-p/1207322#M167326</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2021-01-06T07:08:49Z</dc:date>
    </item>
  </channel>
</rss>