<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8dx usb2 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-usb2/m-p/1206855#M167282</link>
    <description>&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;Is it possible to use cdns3 for USB2.0? The second USB2.0 port of imx8dx, according to the device tree configuration of cdns3, the second USB cannot be used. My USB only has DP DN. There are no other auxiliary devices. I haven't found a suitable modification method yet. If there is a good modification method, please tell me in time.&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;</description>
    <pubDate>Tue, 05 Jan 2021 11:44:34 GMT</pubDate>
    <dc:creator>songhongliang</dc:creator>
    <dc:date>2021-01-05T11:44:34Z</dc:date>
    <item>
      <title>imx8dx usb2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-usb2/m-p/1204048#M166940</link>
      <description>&lt;P&gt;HI&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to use the second usb of imx8dx, but I don't know how to configure it. Is there a patch or help me complete the function together.&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 08:22:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8dx-usb2/m-p/1204048#M166940</guid>
      <dc:creator>songhongliang</dc:creator>
      <dc:date>2020-12-24T08:22:08Z</dc:date>
    </item>
    <item>
      <title>Re: imx8dx usb2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-usb2/m-p/1204776#M167034</link>
      <description>&lt;P&gt;&lt;SPAN style="font-size: 15px; color: #000000; font-family: arial, helvetica, sans-serif;"&gt;imx8dx use usbotg3 for usb2, try to change the source code about usbotg3 in the In fsl-imx8dxp.dtsi and fsl-imx8dxp.dtsi, you need to change according to your HW, I don't have such example for you&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-size: 15px; color: #000000; font-family: arial, helvetica, sans-serif;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Dec 2020 07:01:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8dx-usb2/m-p/1204776#M167034</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-12-29T07:01:00Z</dc:date>
    </item>
    <item>
      <title>Re: imx8dx usb2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-usb2/m-p/1204780#M167035</link>
      <description>&lt;P&gt;hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;The usb2 of imx8dx is usb2.0, the hardware is the same as the official reference schematic diagram, as shown in the picture, there are not too many other components.&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;</description>
      <pubDate>Tue, 29 Dec 2020 07:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8dx-usb2/m-p/1204780#M167035</guid>
      <dc:creator>songhongliang</dc:creator>
      <dc:date>2020-12-29T07:25:51Z</dc:date>
    </item>
    <item>
      <title>Re: imx8dx usb2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-usb2/m-p/1206679#M167264</link>
      <description>&lt;P&gt;sorry I missed this picture before, for usb_otg2, I got information:&lt;/P&gt;
&lt;P&gt;"imx8dx has two USB ports (one for chipidea, one for cdns3), and both are enabled, see arch/arm64/boot/dts/freescale/imx8x-mek.dtsi detail please."&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jan 2021 08:17:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8dx-usb2/m-p/1206679#M167264</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-01-05T08:17:14Z</dc:date>
    </item>
    <item>
      <title>Re: imx8dx usb2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-usb2/m-p/1206855#M167282</link>
      <description>&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;Is it possible to use cdns3 for USB2.0? The second USB2.0 port of imx8dx, according to the device tree configuration of cdns3, the second USB cannot be used. My USB only has DP DN. There are no other auxiliary devices. I haven't found a suitable modification method yet. If there is a good modification method, please tell me in time.&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jan 2021 11:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8dx-usb2/m-p/1206855#M167282</guid>
      <dc:creator>songhongliang</dc:creator>
      <dc:date>2021-01-05T11:44:34Z</dc:date>
    </item>
    <item>
      <title>Re: imx8dx usb2</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8dx-usb2/m-p/1207217#M167314</link>
      <description>&lt;P&gt;.MX8QX/DX there are two USB controllers:&lt;/P&gt;
&lt;P&gt;- One is USB2 compatible and the IP comes from ChipIdea (the same USB IP used on mx5/mx6/mx7)&lt;/P&gt;
&lt;P&gt;- One is USB3 compatible and the IP comes from Cadence.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jan 2021 03:19:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8dx-usb2/m-p/1207217#M167314</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-01-06T03:19:57Z</dc:date>
    </item>
  </channel>
</rss>