<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Hardware design IMX8QM and DDR4 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Hardware-design-IMX8QM-and-DDR4/m-p/1205552#M167129</link>
    <description>&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P&gt;I am designing a mini PC on an IMX8QM processor.&lt;BR /&gt;I need help choosing and connecting DDR4 SDRAM.&lt;BR /&gt;I want to use SDRAM MT40A series from Micron manufacturer. But I cannot choose between MT40A512M8 and MT40A256M16.&lt;BR /&gt;The document "i.MX8 QM / i.MX8 QXP Hardware Developer's Guide" provides examples for DDR3L and LPDDR4 only.&lt;BR /&gt;DDR design is not yet available in Config Tools for i.MX Version 8.0.&lt;BR /&gt;The most productive document is the schematic "MCIMX8QM-CPU MEK Platform", page 14 shows connection to LPDDR4 - MT53E768M32, indicating the pins for DDR4. I started making a circuit with MT40A256M16, then with MT40A512M8, but every time I missed some pins, for example ODT1 or DMI0_A.&lt;BR /&gt;Then in the schematic I read "The processor requires x16 for each chip inside the DRAM package. The x8 configuration is not compatible."&lt;BR /&gt;Does this note mean that I cannot use MT40A512M8? But why then is MT53E768M32 used in the example? After all, if I understand correctly there requires x32.&lt;BR /&gt;Please tell me which DDR4 SDRAM to choose (you can buy from 1 unit, not 2000 units) and examples of connection and settings.&lt;/P&gt;</description>
    <pubDate>Fri, 01 Jan 2021 17:29:55 GMT</pubDate>
    <dc:creator>timur_kh</dc:creator>
    <dc:date>2021-01-01T17:29:55Z</dc:date>
    <item>
      <title>Hardware design IMX8QM and DDR4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hardware-design-IMX8QM-and-DDR4/m-p/1205552#M167129</link>
      <description>&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P&gt;I am designing a mini PC on an IMX8QM processor.&lt;BR /&gt;I need help choosing and connecting DDR4 SDRAM.&lt;BR /&gt;I want to use SDRAM MT40A series from Micron manufacturer. But I cannot choose between MT40A512M8 and MT40A256M16.&lt;BR /&gt;The document "i.MX8 QM / i.MX8 QXP Hardware Developer's Guide" provides examples for DDR3L and LPDDR4 only.&lt;BR /&gt;DDR design is not yet available in Config Tools for i.MX Version 8.0.&lt;BR /&gt;The most productive document is the schematic "MCIMX8QM-CPU MEK Platform", page 14 shows connection to LPDDR4 - MT53E768M32, indicating the pins for DDR4. I started making a circuit with MT40A256M16, then with MT40A512M8, but every time I missed some pins, for example ODT1 or DMI0_A.&lt;BR /&gt;Then in the schematic I read "The processor requires x16 for each chip inside the DRAM package. The x8 configuration is not compatible."&lt;BR /&gt;Does this note mean that I cannot use MT40A512M8? But why then is MT53E768M32 used in the example? After all, if I understand correctly there requires x32.&lt;BR /&gt;Please tell me which DDR4 SDRAM to choose (you can buy from 1 unit, not 2000 units) and examples of connection and settings.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Jan 2021 17:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hardware-design-IMX8QM-and-DDR4/m-p/1205552#M167129</guid>
      <dc:creator>timur_kh</dc:creator>
      <dc:date>2021-01-01T17:29:55Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware design IMX8QM and DDR4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hardware-design-IMX8QM-and-DDR4/m-p/1205564#M167134</link>
      <description>&lt;P&gt;Hi timur_kh&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;i.MX8QM does not support DDR4 as described in datasheet, for example&amp;nbsp; Table 1, 4&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_2" href="https://www.nxp.com/docs/en/data-sheet/IMX8QMAEC.pdf" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8QuadMax Automotive and Infotainment Applications Processors &lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sat, 02 Jan 2021 00:58:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hardware-design-IMX8QM-and-DDR4/m-p/1205564#M167134</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-01-02T00:58:57Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware design IMX8QM and DDR4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hardware-design-IMX8QM-and-DDR4/m-p/1205577#M167138</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN class=""&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066" target="_self"&gt;igorpadykov&lt;/A&gt;!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The comparison table states that the i.MX8QM supports LPDDR4 and DDR4. The i.MX8QM schematic also contains DDR4.Hence there is hope for DDR4 support!)&lt;/P&gt;&lt;P&gt;Or the comparison table contains a typo &lt;LI-EMOJI id="lia_disappointed-face" title=":disappointed_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-8-processors:IMX8-SERIES" target="_self"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-8-processors:IMX8-SERIES&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 02 Jan 2021 04:13:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hardware-design-IMX8QM-and-DDR4/m-p/1205577#M167138</guid>
      <dc:creator>timur_kh</dc:creator>
      <dc:date>2021-01-02T04:13:50Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware design IMX8QM and DDR4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hardware-design-IMX8QM-and-DDR4/m-p/1205642#M167148</link>
      <description>&lt;P&gt;correct&amp;nbsp;&lt;SPAN&gt;comparison table :&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/supporting-information/IMX8LAYERCMPR.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/supporting-information/IMX8LAYERCMPR.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 03 Jan 2021 10:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hardware-design-IMX8QM-and-DDR4/m-p/1205642#M167148</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-01-03T10:37:13Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware design IMX8QM and DDR4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Hardware-design-IMX8QM-and-DDR4/m-p/1208029#M167393</link>
      <description>&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jan 2021 05:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Hardware-design-IMX8QM-and-DDR4/m-p/1208029#M167393</guid>
      <dc:creator>timur_kh</dc:creator>
      <dc:date>2021-01-07T05:54:29Z</dc:date>
    </item>
  </channel>
</rss>