<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Boot i.MX8M with DDR4 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX8M-with-DDR4/m-p/1205273#M167107</link>
    <description>&lt;P&gt;Hi,Sir:&lt;/P&gt;&lt;P&gt;We are debugging i.MX8M with DDR4, and passed the DDR Stress Test in attached.But i.MX8M is still in resetting&amp;nbsp; when checking the&amp;nbsp; log as below.&lt;/P&gt;&lt;P&gt;From the log, I guess that: just fix the config of DDR4, not the FW of DDR4, then download the FW of LPDDR4 after reset.&amp;nbsp; So how to fix the FW of LPDDR4 with DDR4?&amp;nbsp;&lt;/P&gt;&lt;P&gt;And checking the DDR Tool User guide, not only copy the DDR4_timing to &lt;EM&gt;board/freescale/imx8mq_evk/ ,&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;but also need to copy the FW of DDR4 to image ,but how to compile?&lt;/P&gt;</description>
    <pubDate>Wed, 30 Dec 2020 13:57:20 GMT</pubDate>
    <dc:creator>lizboxy</dc:creator>
    <dc:date>2020-12-30T13:57:20Z</dc:date>
    <item>
      <title>Boot i.MX8M with DDR4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX8M-with-DDR4/m-p/1205273#M167107</link>
      <description>&lt;P&gt;Hi,Sir:&lt;/P&gt;&lt;P&gt;We are debugging i.MX8M with DDR4, and passed the DDR Stress Test in attached.But i.MX8M is still in resetting&amp;nbsp; when checking the&amp;nbsp; log as below.&lt;/P&gt;&lt;P&gt;From the log, I guess that: just fix the config of DDR4, not the FW of DDR4, then download the FW of LPDDR4 after reset.&amp;nbsp; So how to fix the FW of LPDDR4 with DDR4?&amp;nbsp;&lt;/P&gt;&lt;P&gt;And checking the DDR Tool User guide, not only copy the DDR4_timing to &lt;EM&gt;board/freescale/imx8mq_evk/ ,&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;but also need to copy the FW of DDR4 to image ,but how to compile?&lt;/P&gt;</description>
      <pubDate>Wed, 30 Dec 2020 13:57:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX8M-with-DDR4/m-p/1205273#M167107</guid>
      <dc:creator>lizboxy</dc:creator>
      <dc:date>2020-12-30T13:57:20Z</dc:date>
    </item>
    <item>
      <title>Re: Boot i.MX8M with DDR4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX8M-with-DDR4/m-p/1205971#M167180</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/123296"&gt;@lizboxy&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; use&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/1104467&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="color: #3366ff;"&gt;MSCALE_DDR_Tool_User_Guide&lt;/SPAN&gt;&amp;nbsp; (in the DDR Tool package) describes how to add &lt;BR /&gt;support for new memory, in particular section 4.3 (Building u-boot image) explains&lt;BR /&gt;how to build all the needed software. &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jan 2021 08:22:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX8M-with-DDR4/m-p/1205971#M167180</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2021-01-04T08:22:54Z</dc:date>
    </item>
  </channel>
</rss>