<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6SoloX Linux &amp;amp; FreeRTOS shared resources</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SoloX-Linux-amp-FreeRTOS-shared-resources/m-p/1205269#M167106</link>
    <description>&lt;P&gt;Although, the fault was connected with incorrect area in my ld file, i find this link very useful.&lt;BR /&gt;Thank you Igor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 30 Dec 2020 13:26:04 GMT</pubDate>
    <dc:creator>o_scherbinin</dc:creator>
    <dc:date>2020-12-30T13:26:04Z</dc:date>
    <item>
      <title>i.MX6SoloX Linux &amp; FreeRTOS shared resources</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SoloX-Linux-amp-FreeRTOS-shared-resources/m-p/1204166#M166954</link>
      <description>&lt;P&gt;hello. i am using iMX6 SABRESD board.&lt;BR /&gt;i need FreeRTOS and Linux systems for this board loaded in RAM (DDR). Linux is placed at the beginning of RAM and FreeRTOS in the second half.&lt;BR /&gt;Then first u-boot ups m4 core (FreeRTOS) and it works fine till Linux starts and m4 loses its console. I can see that a fault&lt;BR /&gt;occures when Linux initializes NVIC.&lt;BR /&gt;The intended for m4 serial device is disabled in the device tree (using of m4 dts file).&lt;BR /&gt;I would like to know what is correct way work with two systmes at the same time.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;With best wishes.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 16:48:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SoloX-Linux-amp-FreeRTOS-shared-resources/m-p/1204166#M166954</guid>
      <dc:creator>o_scherbinin</dc:creator>
      <dc:date>2020-12-24T16:48:06Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6SoloX Linux &amp; FreeRTOS shared resources</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SoloX-Linux-amp-FreeRTOS-shared-resources/m-p/1204652#M167004</link>
      <description>&lt;P&gt;Hi o_scherbinin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for debugging hints one can look at similar issue on below link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/GPT-capture-sample-on-M4-seems-to-hang-on-Linux-boot/m-p/902416" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/GPT-capture-sample-on-M4-seems-to-hang-on-Linux-boot/m-p/902416&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 29 Dec 2020 01:09:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SoloX-Linux-amp-FreeRTOS-shared-resources/m-p/1204652#M167004</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-12-29T01:09:11Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6SoloX Linux &amp; FreeRTOS shared resources</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SoloX-Linux-amp-FreeRTOS-shared-resources/m-p/1205269#M167106</link>
      <description>&lt;P&gt;Although, the fault was connected with incorrect area in my ld file, i find this link very useful.&lt;BR /&gt;Thank you Igor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Dec 2020 13:26:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SoloX-Linux-amp-FreeRTOS-shared-resources/m-p/1205269#M167106</guid>
      <dc:creator>o_scherbinin</dc:creator>
      <dc:date>2020-12-30T13:26:04Z</dc:date>
    </item>
  </channel>
</rss>