<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Linux crashes while opening /dev/console with ttymxc0</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Dead-lock-occurred-while-opening-dev-console-with-ttymxc0/m-p/1204809#M167041</link>
    <description>&lt;P&gt;Yes, my board is referenced to Sabre SD board.&amp;nbsp; But there is no SN74LVC2G126 between i.MX6SX UART and USB bridge.&amp;nbsp; And UART1 is used as the I/O port which is same as NXP board.&lt;/P&gt;</description>
    <pubDate>Tue, 29 Dec 2020 08:00:01 GMT</pubDate>
    <dc:creator>zhb1984</dc:creator>
    <dc:date>2020-12-29T08:00:01Z</dc:date>
    <item>
      <title>Dead lock occurred while opening /dev/console with ttymxc0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dead-lock-occurred-while-opening-dev-console-with-ttymxc0/m-p/1204664#M167010</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using i.MX6SoloX to develop application with custom board.&amp;nbsp; U-Boot and Linux porting have been done.&amp;nbsp; Everything is OK except that Linux hung while opening /dev/console with ttymxc0.&amp;nbsp; It tried to do spin_lock_irqsave in imx_uart_startup.&amp;nbsp; But at this point, the lock was already acquired.&amp;nbsp; So dead lock occurred.&lt;/P&gt;&lt;P&gt;Can someone give any advice?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 30 Dec 2020 06:47:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dead-lock-occurred-while-opening-dev-console-with-ttymxc0/m-p/1204664#M167010</guid>
      <dc:creator>zhb1984</dc:creator>
      <dc:date>2020-12-30T06:47:55Z</dc:date>
    </item>
    <item>
      <title>Re: Linux crashes while opening /dev/console with ttymxc0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dead-lock-occurred-while-opening-dev-console-with-ttymxc0/m-p/1204801#M167038</link>
      <description>&lt;P&gt;for your customized board, did your HW is the same as nxp board? did you use the same uart console as nxp board?&lt;/P&gt;</description>
      <pubDate>Tue, 29 Dec 2020 07:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dead-lock-occurred-while-opening-dev-console-with-ttymxc0/m-p/1204801#M167038</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-12-29T07:52:42Z</dc:date>
    </item>
    <item>
      <title>Re: Linux crashes while opening /dev/console with ttymxc0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dead-lock-occurred-while-opening-dev-console-with-ttymxc0/m-p/1204809#M167041</link>
      <description>&lt;P&gt;Yes, my board is referenced to Sabre SD board.&amp;nbsp; But there is no SN74LVC2G126 between i.MX6SX UART and USB bridge.&amp;nbsp; And UART1 is used as the I/O port which is same as NXP board.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Dec 2020 08:00:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dead-lock-occurred-while-opening-dev-console-with-ttymxc0/m-p/1204809#M167041</guid>
      <dc:creator>zhb1984</dc:creator>
      <dc:date>2020-12-29T08:00:01Z</dc:date>
    </item>
    <item>
      <title>Re: Linux crashes while opening /dev/console with ttymxc0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Dead-lock-occurred-while-opening-dev-console-with-ttymxc0/m-p/1207363#M167330</link>
      <description>&lt;P&gt;try to refer to the enclosed file&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jan 2021 08:13:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Dead-lock-occurred-while-opening-dev-console-with-ttymxc0/m-p/1207363#M167330</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2021-01-06T08:13:43Z</dc:date>
    </item>
  </channel>
</rss>