<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX8M Mini Boot Mode with eFuse in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Boot-Mode-with-eFuse/m-p/1204493#M166985</link>
    <description>&lt;P&gt;refer to the chapter 6.1.2.3 Boot From Fuses mode (BOOT_MODE[1:0] = 00b):&lt;/P&gt;
&lt;P&gt;In this mode, the GPIO boot override&lt;BR /&gt;pins are ignored. The boot ROM code uses the boot eFUSE settings only.&lt;/P&gt;
&lt;P&gt;refer to the chapter 6.1.2.5 Internal Boot mode (BOOT_MODE[1:0] = 0b10):&lt;/P&gt;
&lt;P&gt;The GPIO Boot Select FUSE (BT_FUSE_SEL) determines whether the&lt;BR /&gt;ROM uses the GPIO pins for a selected number of configuration parameters or eFUSEs&lt;BR /&gt;in this mode.&lt;BR /&gt;• If BT_FUSE_SEL = 1, all boot options are controlled by the eFUSEs described in&lt;BR /&gt;Table 6-2.&lt;BR /&gt;• If BT_FUSE_SEL = 0, the specific boot configuration parameters may be set using&lt;BR /&gt;the GPIO pins rather than eFUSEs. The fuses that can be overridden when in this&lt;BR /&gt;mode are indicated in the GPIO column of Table 6-2. Table 6-3 provides the details&lt;BR /&gt;of the GPIO pins.&lt;/P&gt;
&lt;P&gt;so if you want to use gpio override mode, you need to set &lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;BOOT_MODE[1:0] = 10&amp;nbsp; and BT_FUSE_SEL = 0&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 28 Dec 2020 08:34:49 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2020-12-28T08:34:49Z</dc:date>
    <item>
      <title>i.MX8M Mini Boot Mode with eFuse</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Boot-Mode-with-eFuse/m-p/1198810#M166423</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;My question is regarding the boot mode selection of the i.MX8M Mini.&lt;/P&gt;&lt;P&gt;We would like to use the BOOT_MODE pins to boot from different boot devices (eMMC, SD, Serial Downloader). If the eFuse GPIO_BT_SEL = 0 is set is the following statement correct?&lt;/P&gt;&lt;P&gt;BOOT_MODE = 00 -&amp;gt; Boot From Fuses (eFuses configured for SD)&lt;/P&gt;&lt;P&gt;BOOT_MODE = 01 -&amp;gt; Serial Downloader&lt;/P&gt;&lt;P&gt;BOOT_MODE = 10 -&amp;gt; Boot From eMMC (Configuration set by GPIOs)&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 09:56:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Boot-Mode-with-eFuse/m-p/1198810#M166423</guid>
      <dc:creator>lumen</dc:creator>
      <dc:date>2020-12-14T09:56:32Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini Boot Mode with eFuse</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Boot-Mode-with-eFuse/m-p/1200276#M166575</link>
      <description>&lt;P&gt;you can refer to the Table 6-14. USDHC boot eFUSE descriptions of Reference Manual,&lt;/P&gt;
&lt;DIV id="bodyDisplay_0" class="lia-message-body lia-component-message-view-widget-body lia-component-body-signature-highlight-escalation lia-component-message-view-widget-body-signature-highlight-escalation"&gt;
&lt;DIV class="lia-message-body-content"&gt;
&lt;P&gt;BOOT_CFG[6:4]=001, BOOT_CFG[15:12]=0010&lt;/P&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;</description>
      <pubDate>Wed, 16 Dec 2020 09:26:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Boot-Mode-with-eFuse/m-p/1200276#M166575</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-12-16T09:26:14Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini Boot Mode with eFuse</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Boot-Mode-with-eFuse/m-p/1201001#M166634</link>
      <description>&lt;P&gt;Hi joanxie,&lt;/P&gt;&lt;P&gt;Thanks for your reply. The boot configuration for the different boot devices is clear to me.&lt;/P&gt;&lt;P&gt;Is it possible to change the different boot devices with BOOT_MODE GPIOS if GPIO_BT_SEL = 0?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 06:57:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Boot-Mode-with-eFuse/m-p/1201001#M166634</guid>
      <dc:creator>lumen</dc:creator>
      <dc:date>2020-12-17T06:57:02Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Mini Boot Mode with eFuse</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Boot-Mode-with-eFuse/m-p/1204493#M166985</link>
      <description>&lt;P&gt;refer to the chapter 6.1.2.3 Boot From Fuses mode (BOOT_MODE[1:0] = 00b):&lt;/P&gt;
&lt;P&gt;In this mode, the GPIO boot override&lt;BR /&gt;pins are ignored. The boot ROM code uses the boot eFUSE settings only.&lt;/P&gt;
&lt;P&gt;refer to the chapter 6.1.2.5 Internal Boot mode (BOOT_MODE[1:0] = 0b10):&lt;/P&gt;
&lt;P&gt;The GPIO Boot Select FUSE (BT_FUSE_SEL) determines whether the&lt;BR /&gt;ROM uses the GPIO pins for a selected number of configuration parameters or eFUSEs&lt;BR /&gt;in this mode.&lt;BR /&gt;• If BT_FUSE_SEL = 1, all boot options are controlled by the eFUSEs described in&lt;BR /&gt;Table 6-2.&lt;BR /&gt;• If BT_FUSE_SEL = 0, the specific boot configuration parameters may be set using&lt;BR /&gt;the GPIO pins rather than eFUSEs. The fuses that can be overridden when in this&lt;BR /&gt;mode are indicated in the GPIO column of Table 6-2. Table 6-3 provides the details&lt;BR /&gt;of the GPIO pins.&lt;/P&gt;
&lt;P&gt;so if you want to use gpio override mode, you need to set &lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;BOOT_MODE[1:0] = 10&amp;nbsp; and BT_FUSE_SEL = 0&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Dec 2020 08:34:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Mini-Boot-Mode-with-eFuse/m-p/1204493#M166985</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-12-28T08:34:49Z</dc:date>
    </item>
  </channel>
</rss>