<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Want to try hard float vivante drivers for MX6? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228612#M16697</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We tested the binaries on a Linaro 12.11 build, we can run es2gears/glmark2 as root, initial figures are marginally better than armel. However these fails to run as a non-root user (ie linaro), I've checked the obvious permissions, groups and&amp;nbsp; xorg.conf and it seems to be ok. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gdb reports the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting program: /usr/bin/es2gears&lt;/P&gt;&lt;P&gt;[Thread debugging using libthread_db enabled]&lt;/P&gt;&lt;P&gt;Using host libthread_db library "/lib/arm-linux-gnueabihf/libthread_db.so.1".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Program received signal SIGSEGV, Segmentation fault.&lt;/P&gt;&lt;P&gt;0x2ad9e8a8 in gcoHAL_QueryChipCount () from /usr/lib/libGAL.so&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also the viv_samples don't run as there seems to be a binary compatibility issue. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have tested the same setup on a Linaro armel build using the softfp binaries and everything runs fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 May 2013 19:54:14 GMT</pubDate>
    <dc:creator>mtx512</dc:creator>
    <dc:date>2013-05-07T19:54:14Z</dc:date>
    <item>
      <title>Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228610#M16695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello MX6 users,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I work for Timesys and have been integrating the Vivante drivers into our LinuxLink tools for mx6. In this thread I'd like to invite you to try out some of our built SDKs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've done a lot of wrangling with our tools and these drivers on X &amp;amp; framebuffer, and am currently working on QT4 &amp;amp; QT5 support. I still wouldn't call myself an expert, but I'd like to learn from your expertise and share these builds to hopefully improve our support out of the box.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a free web build service, but at this time only soft-float can be built the web service, so I'll be uploading built SDKs to dropbox and sharing the links here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H3&gt;About the SDKs:&lt;/H3&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We provide built SDKs as an installer script which can be distributed to developers for building applications with a cross-toolchain. To install the SDK, run the .sh file contained within these published tarballs to install the toolchain and RFS, kernel, to ~/timesys/. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DO NOT run as root (except to extract the RFS tarball).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These have been built on my host which is x86-64 Ubuntu 12.04, and therefore will not be compatible with 32-bit hosts. If anyone wants a 32-bit SDK let me know, I'll run a build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Each sdk installer will create a few items under ~/timesys/&amp;lt;board-name&amp;gt;/: kernel sources, bootloader images, the toolchain, and also a built kernel image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the SDKs include a toolchain, you can use this to build additional applications to run on the target! For this reason, I'm providing minimal RFS images.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The first built SDK is available here&lt;/STRONG&gt;: &lt;A href="https://www.dropbox.com/s/4cbpot1436l4tse/vivante-hardfloat-sdp.tar.xz"&gt;https://www.dropbox.com/s/4cbpot1436l4tse/vivante-hardfloat-sdp.tar.xz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This SDK provides a toolchain, rfs, and kernel with an X desktop. However, I didn't include any real X applications apart from the vivante samples.&lt;/P&gt;&lt;H3&gt;&lt;/H3&gt;&lt;H3&gt;Testing the SDK:&lt;/H3&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use tftp/nfs to boot the SDP (bootargs=console=ttymxc0,115200 video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 ldb=sin1 root=/dev/nfs ip=dhcp) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here's a quick boot log snippet of running a test on the SDP:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Distribution built using LinuxLink by Timesys&lt;BR /&gt;Kernel 3.0.35-ts-armv7l for armv7l&lt;BR /&gt;SABRE_SDP login: root&lt;BR /&gt;No mail.&lt;BR /&gt;root@SABRE_SDP:~$ X &amp;amp;&lt;BR /&gt;[1] 1307&lt;BR /&gt;root@SABRE_SDP:~$ _XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6&lt;BR /&gt;_XSERVTransOpen: transport open failed for inet6/SABRE_SDP:0&lt;BR /&gt;_XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;X.Org X Server 1.11.4&lt;BR /&gt;Release Date: 2012-01-27&lt;BR /&gt;X Protocol Version 11, Revision 0&lt;BR /&gt;Build Operating System: Linux 3.2.0-40-generic x86_64&lt;BR /&gt;Current Operating System: Linux SABRE_SDP 3.0.35-ts-armv7l #1 SMP PREEMPT Tue May 7 08:39:50 EDT 2013 armv7l&lt;BR /&gt;Kernel command line: console=ttymxc0,115200 video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 ldb=sin1 root=/dev/nfs ip=dhcp&lt;BR /&gt;Build Date: 07 May 2013&amp;nbsp; 09:22:06AM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Current version of pixman: 0.28.2&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Before reporting problems, check &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://wiki.x.org"&gt;http://wiki.x.org&lt;/A&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; to make sure that you have the latest version.&lt;BR /&gt;Markers: (--) probed, (**) from config file, (==) default setting,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (++) from command line, (!!) notice, (II) informational,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (WW) warning, (EE) error, (NI) not implemented, (??) unknown.&lt;BR /&gt;(==) Log file: "/var/log/Xorg.0.log", Time: Thu Jan&amp;nbsp; 8 13:12:54 1970&lt;BR /&gt;(==) Using system config directory "/usr/share/X11/xorg.conf.d"&lt;BR /&gt;(EE) AIGLX error: dlopen of /usr/lib/dri/swrast_dri.so failed (/usr/lib/dri/swrast_dri.so: cannot open shared object file: No such file or directory)&lt;BR /&gt;(EE) GLX: could not load software renderer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@SABRE_SDP:~$ export DISPLAY=:0&lt;BR /&gt;root@SABRE_SDP:~$ cd /opt/viv_samples/vdk/&lt;BR /&gt;root@SABRE_SDP:/opt/viv_samples/vdk$ ./tutorial7&lt;BR /&gt;fps: 727.27&lt;BR /&gt;fps: 729.34&lt;BR /&gt;fps: 730.73&lt;BR /&gt;^Croot@SABRE_SDP:/opt/viv_samples/vdk$ &lt;BR /&gt;----snip----&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H4&gt;A few notes about this log: &lt;BR /&gt;X has no session/nothing to start, so I start the server manually. Then set the display and run the tutorials under /opt/viv_samples/&lt;/H4&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using the X drivers, I've been unable to run tiger &amp;amp; vv_launcher without using fullscreen on the SDP. Use these commands to run those samples:&lt;BR /&gt;./tiger -w 1024 -h 768&lt;BR /&gt;./vv_launcher -w 1024 -h 768&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, some of the samples must be run in the directory where they reside--they are coded to use images using relative path.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Later this afternoon I'll be posting the framebuffer only version of the SDK. If you can't wait for a framebuffer-only SDK, the tarball containing both soft &amp;amp; hard float builds is here &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q-1.1.0-ts/gpu-viv-bin-mx6q-1.1.0-ts.tar.gz"&gt;http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q-1.1.0-ts/gpu-viv-bin-mx6q-1.1.0-ts.tar.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FYI, I split these vivante drivers into 2 packages for now, one for X and one for framebuffer only. Hoping to add a directFB build and eventually wayland. For now only the Framebuffer and X versions are available on our repository.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H3&gt;Roadmap&lt;/H3&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're awaiting a new drop of the vivante driver sources which will hopefully improve performance. Also we are aiming for DirectFB &amp;amp; wayland support in the coming weeks, but again that may require new vivante sources. I have a DirectFB build, but it doesn't seem to work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have done some testing with Qt5 and qt4, and will provide SDKs for testing as well as feedback over the next couple of days. I've not had success with the X drivers &amp;amp; QT, but the framebuffer seems to work. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've also had some trouble with the DirectFB builds I've used, but perhaps we can get into that as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you all for the feedback,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy Voltz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2013 16:04:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228610#M16695</guid>
      <dc:creator>avoltz</dc:creator>
      <dc:date>2013-05-07T16:04:19Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228611#M16696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;And now for the framebuffer only version: &lt;A href="https://www.dropbox.com/s/0dpghzo9u1coqt2/vivante-hf-fbonly.tar.xz"&gt;https://www.dropbox.com/s/0dpghzo9u1coqt2/vivante-hf-fbonly.tar.xz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case, the tiger &amp;amp; vv_launcher demos do not require any arguments. Next: QT&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2013 18:16:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228611#M16696</guid>
      <dc:creator>avoltz</dc:creator>
      <dc:date>2013-05-07T18:16:41Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228612#M16697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We tested the binaries on a Linaro 12.11 build, we can run es2gears/glmark2 as root, initial figures are marginally better than armel. However these fails to run as a non-root user (ie linaro), I've checked the obvious permissions, groups and&amp;nbsp; xorg.conf and it seems to be ok. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gdb reports the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting program: /usr/bin/es2gears&lt;/P&gt;&lt;P&gt;[Thread debugging using libthread_db enabled]&lt;/P&gt;&lt;P&gt;Using host libthread_db library "/lib/arm-linux-gnueabihf/libthread_db.so.1".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Program received signal SIGSEGV, Segmentation fault.&lt;/P&gt;&lt;P&gt;0x2ad9e8a8 in gcoHAL_QueryChipCount () from /usr/lib/libGAL.so&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also the viv_samples don't run as there seems to be a binary compatibility issue. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have tested the same setup on a Linaro armel build using the softfp binaries and everything runs fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2013 19:54:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228612#M16697</guid>
      <dc:creator>mtx512</dc:creator>
      <dc:date>2013-05-07T19:54:14Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228613#M16698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just to confirm, it sounds like you have tried our binaries with the Linaro RFS? Have you tried building the es2gears glmark2 samples with one of the SDKs I posted? If you link me to the sources of those examples I can try to build them here and let you know.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2013 20:01:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228613#M16698</guid>
      <dc:creator>avoltz</dc:creator>
      <dc:date>2013-05-07T20:01:10Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228614#M16699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes we tested with a Linaro RFS. Our sources will have been pre-built from &lt;A href="http://packages.ubuntu.com/source/precise/mesa-demos" title="http://packages.ubuntu.com/source/precise/mesa-demos"&gt;Ubuntu – Details of source package mesa-demos in precise&lt;/A&gt; ,as mentioned they run as root and seg fault as non-root. So I'm guessing there seems to be a permission problem somewhere?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2013 20:13:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228614#M16699</guid>
      <dc:creator>mtx512</dc:creator>
      <dc:date>2013-05-07T20:13:49Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228615#M16700</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I haven't used the Linaro RFS, but can you check the permissions on /dev/galcore and /dev/fb0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the RFS from the framebuffer-only SDK I posted above, I needed to run "chmod 666" on those device nodes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2013 20:27:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228615#M16700</guid>
      <dc:creator>avoltz</dc:creator>
      <dc:date>2013-05-07T20:27:18Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228616#M16701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks :smileyhappy: the problem was permission on /dev/galcore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Next issue is that the vivante samples don't run:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@linaro-alip:~/viv_samples/vdk# ./tutorial7&lt;/P&gt;&lt;P&gt;-bash: ./tutorial7: No such file or directory&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Seems to be some kind of libc compatibility issues. Can we compile the samples from scratch?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2013 20:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228616#M16701</guid>
      <dc:creator>mtx512</dc:creator>
      <dc:date>2013-05-07T20:47:11Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228617#M16702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately, I don't think so... Try the RFS from one of the SDKs I posted above, or perhaps yocto.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2013 20:50:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228617#M16702</guid>
      <dc:creator>avoltz</dc:creator>
      <dc:date>2013-05-07T20:50:41Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228618#M16703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you know if the binaries will work against xorg 1.13 if we patch the dri driver?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 May 2013 11:39:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228618#M16703</guid>
      <dc:creator>mtx512</dc:creator>
      <dc:date>2013-05-08T11:39:06Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228619#M16704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately, no. The other driver sources require additional patching. I'm hopeful the next sources I receive will support a newer X, but for now 1.11 is required. Our system builds 1.11 for the mx6 for this reason.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 May 2013 14:05:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228619#M16704</guid>
      <dc:creator>avoltz</dc:creator>
      <dc:date>2013-05-08T14:05:31Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228620#M16705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andy,&lt;/P&gt;&lt;P&gt;I have the same situation here. I am using Boundry Nitrogen6x board. I got Qt5 with your Vivante-libs FB-only running. I could run the "collidingmice" example from qt with eglfs. Then I switched fron kernel 3.0.35_1.1.0 to 3.0.35_4.0.0, now the programm segfaults at the call eglBindAPI(...) in the constructor of the class QEglFSIntegration. To cross-check, I switched back to 3.0.35_1.1.0 and everything was fine again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you verify this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2013 14:53:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228620#M16705</guid>
      <dc:creator>arslan</dc:creator>
      <dc:date>2013-06-10T14:53:00Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228621#M16706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do these libraries require a specific version of galcore?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a version copyright 2013, taken from the gpu-viv/ directory in L3.0.35_4.0.0_130424_source/pkgs/linux-3.0.35/drivers/mxc/, compiled as a module for linnux-3.10.0-rc7.&amp;nbsp; The libraries linked here look like they use 32-bit pointers for the ioctl DRIVER_ARGS data, and the gcsHAL_INTERFACE pointed to is 128 bytes, whereas the version of galcore that ships in L3.0.35_4.0.0_130424 uses 64-bit pointers for ioctl DRIVER_ARGS data and gcsHAL_INTERFACE is 168 bytes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2013 08:29:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228621#M16706</guid>
      <dc:creator>xobs</dc:creator>
      <dc:date>2013-07-02T08:29:07Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228622#M16707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;good job !&lt;/P&gt;&lt;P&gt;very interesting !&lt;/P&gt;&lt;P&gt;I haven't tested yet though, it seems there is no qt related in you sdk.&lt;/P&gt;&lt;P&gt;would you give me sdk that has qt(4.x or 5) and gstreamer ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Aug 2013 05:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228622#M16707</guid>
      <dc:creator>Dennis_Han</dc:creator>
      <dc:date>2013-08-05T05:28:42Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228623#M16708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Timesys has released some more binaries since then:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q-3.0.35-4.0.0/gpu-viv-bin-mx6q-3.0.35-4.0.0.tar.gz"&gt;http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q-3.0.35-4.0.0/gpu-viv-bin-mx6q-3.0.35-4.0.0.tar.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q-3.0.35-4.0.0-ts/gpu-viv-bin-mx6q-3.0.35-4.0.0-ts.tar.gz"&gt;http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q-3.0.35-4.0.0-ts/gpu-viv-bin-mx6q-3.0.35-4.0.0-ts.tar.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://repository.timesys.com/buildsources/g/gpu-viv-x11-bin-mx6q/gpu-viv-x11-bin-mx6q-3.0.35-4.0.0/gpu-viv-x11-bin-mx6q-3.0.35-4.0.0.tar.gz"&gt;http://repository.timesys.com/buildsources/g/gpu-viv-x11-bin-mx6q/gpu-viv-x11-bin-mx6q-3.0.35-4.0.0/gpu-viv-x11-bin-mx6q-3.0.35-4.0.0.tar.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All of them have an &lt;STRONG&gt;armel&lt;/STRONG&gt; and an &lt;STRONG&gt;armhf&lt;/STRONG&gt; directory.&lt;/P&gt;&lt;P&gt;That's very nice, thank you.&lt;/P&gt;&lt;P&gt;But.&lt;/P&gt;&lt;P&gt;In those &lt;STRONG&gt;armhf&lt;/STRONG&gt; directories, among those &lt;STRONG&gt;armhf &lt;/STRONG&gt;libraries there is one doesn't belong to the group an &lt;STRONG&gt;armel&lt;/STRONG&gt; library named &lt;STRONG&gt;libCLC.so&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;This must be a bug if I'm right, because armel binaries pass floating point values in integer registers while armhf binaries pass them in vfp registers. So you can't mix armel binaries/libaries with armhf binaries/libraries.&lt;/P&gt;&lt;P&gt;Would you please check it and fix it, that must be a simple mistake, but it can cause serious and mysterious bugs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2013 20:47:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228623#M16708</guid>
      <dc:creator>TeleLaci</dc:creator>
      <dc:date>2013-08-28T20:47:30Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228624#M16709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got the same problem. Was you able to solve it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2013 11:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228624#M16709</guid>
      <dc:creator>ortogonal</dc:creator>
      <dc:date>2013-09-05T11:47:28Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228625#M16710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do these libraries also work for i.MX6 Solo and Dual Lite CPU? These are equipped with a different 3D core. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Nov 2013 10:21:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228625#M16710</guid>
      <dc:creator>paulgeurts</dc:creator>
      <dc:date>2013-11-15T10:21:48Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228626#M16711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have tried later versions of the libraries on a i.mx6 solo board and they work fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Nov 2013 12:38:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228626#M16711</guid>
      <dc:creator>mtx512</dc:creator>
      <dc:date>2013-11-15T12:38:38Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228627#M16712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone got vivante, wayland and Qt5 to work with hard float binaries? I'm trying this Kontron i.MX6q board which uses different kernel than freescale and none of the soft float vivante binaries work, only this hard float version but only with eglfs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jan 2014 08:11:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228627#M16712</guid>
      <dc:creator>kende</dc:creator>
      <dc:date>2014-01-03T08:11:29Z</dc:date>
    </item>
    <item>
      <title>Re: Want to try hard float vivante drivers for MX6?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228628#M16713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Qt5 works with Matchbox/Sato and hard-float on the Dora release of Yocto.&amp;nbsp; I'm not sure if that uses Wayland or not.&amp;nbsp; I have built and run the Vivante samples for hard-float and framebuffer mode on Dora for the WandBoard.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://groups.google.com/forum/#%21topic/wandboard/PHv-yXyhEWM" title="https://groups.google.com/forum/#%21topic/wandboard/PHv-yXyhEWM"&gt;Google Groups&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, Clay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jan 2014 21:28:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Want-to-try-hard-float-vivante-drivers-for-MX6/m-p/228628#M16713</guid>
      <dc:creator>claymontgomery</dc:creator>
      <dc:date>2014-01-07T21:28:11Z</dc:date>
    </item>
  </channel>
</rss>