<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx8mm : Getting Kernel Panic</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-Getting-Kernel-Panic/m-p/1204177#M166955</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am getting a kernel panic message after that the processor hangs and the only way to recover is to do a power on reset. Is there any other way that once kernel panic happens the processor reboots automatically?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Santhosh&lt;/P&gt;</description>
    <pubDate>Thu, 24 Dec 2020 19:15:33 GMT</pubDate>
    <dc:creator>santhosh2</dc:creator>
    <dc:date>2020-12-24T19:15:33Z</dc:date>
    <item>
      <title>imx8mm : Getting Kernel Panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-Getting-Kernel-Panic/m-p/1204177#M166955</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am getting a kernel panic message after that the processor hangs and the only way to recover is to do a power on reset. Is there any other way that once kernel panic happens the processor reboots automatically?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Santhosh&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 19:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-Getting-Kernel-Panic/m-p/1204177#M166955</guid>
      <dc:creator>santhosh2</dc:creator>
      <dc:date>2020-12-24T19:15:33Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm : Getting Kernel Panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-Getting-Kernel-Panic/m-p/1204644#M166999</link>
      <description>&lt;P&gt;Hi Santhosh&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;in general wdog can be used in such situations, it can reset pmic and all board,&lt;/P&gt;
&lt;P&gt;example can be found in i.MX8M Mini EVK design&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-for-the-i-mx-8m-mini-applications-processor:8MMINILPD4-EVK" target="_blank"&gt;https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-for-the-i-mx-8m-mini-applications-processor:8MMINILPD4-EVK&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Tue, 29 Dec 2020 00:47:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-Getting-Kernel-Panic/m-p/1204644#M166999</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-12-29T00:47:55Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm : Getting Kernel Panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-Getting-Kernel-Panic/m-p/1205108#M167079</link>
      <description>&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Link: &lt;A href="https://www.techrepublic.com/blog/linux-and-open-source/auto-reboot-linux-after-a-kernel-panic/" target="_blank"&gt;https://www.techrepublic.com/blog/linux-and-open-source/auto-reboot-linux-after-a-kernel-panic/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I also configured Linux to automatically reboot on a kernel panic by making a small modification to &lt;EM&gt;/etc/sysctl.conf&lt;/EM&gt;,&lt;/P&gt;&lt;P&gt;Add the following to &lt;EM&gt;/etc/sysctl.conf&lt;/EM&gt;:&lt;/P&gt;&lt;PRE&gt;kernel.panic = 20&lt;/PRE&gt;&lt;P&gt;This tells the kernel that if it encounters a panic, it is to reboot the system after a 20 second delay. By default, the kernel will never reboot when it encounters a panic, but with the above setting you can force it to.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Santhosh&lt;/P&gt;</description>
      <pubDate>Wed, 30 Dec 2020 02:54:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-Getting-Kernel-Panic/m-p/1205108#M167079</guid>
      <dc:creator>santhosh2</dc:creator>
      <dc:date>2020-12-30T02:54:33Z</dc:date>
    </item>
  </channel>
</rss>