<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: EMMC partition from kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/EMMC-partition-from-kernel/m-p/1203883#M166928</link>
    <description>&lt;P&gt;You can use "fdisk" Linux command to manage EMMC partitions. Please refer to chapter 4.3.3 "Partitioning the SD/MMC card" of i.MX Linux User's Guide:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 24 Dec 2020 02:28:25 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2020-12-24T02:28:25Z</dc:date>
    <item>
      <title>EMMC partition from kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EMMC-partition-from-kernel/m-p/1203762#M166916</link>
      <description>&lt;P&gt;Dear NXP,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I unable to create more partition from Linux,&lt;/P&gt;&lt;P&gt;by default,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2" color="#008000"&gt;root@imx8mnevk:~# ls -l /dev/mmcblk2*&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" color="#008000"&gt;brw-rw---- 1 root disk 179, 0 May 26 16:51 /dev/mmcblk2&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" color="#008000"&gt;brw-rw---- 1 root disk 179, 32 May 26 16:51 /dev/mmcblk2boot0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" color="#008000"&gt;brw-rw---- 1 root disk 179, 64 May 26 16:51 /dev/mmcblk2boot1&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" color="#008000"&gt;brw-rw---- 1 root disk 179, 1 May 26 16:51 /dev/mmcblk2p1&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" color="#008000"&gt;brw-rw---- 1 root disk 179, 2 May 26 16:51 /dev/mmcblk2p2&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2" color="#008000"&gt;crw------- 1 root root 237, 0 May 26 16:51 /dev/mmcblk2rpmb&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="andale mono,times" size="4" color="#333333"&gt;I want to create &lt;FONT color="#993300"&gt;&lt;STRONG&gt;mmcblk2p3 to mmcblk2p7&lt;/STRONG&gt;&lt;/FONT&gt;. But, I unable to do it. will you please provide the proper steps or scripts to create EMMC partition from script or Linux commands&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Dec 2020 17:55:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EMMC-partition-from-kernel/m-p/1203762#M166916</guid>
      <dc:creator>vinothkumars</dc:creator>
      <dc:date>2020-12-23T17:55:15Z</dc:date>
    </item>
    <item>
      <title>Re: EMMC partition from kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EMMC-partition-from-kernel/m-p/1203883#M166928</link>
      <description>&lt;P&gt;You can use "fdisk" Linux command to manage EMMC partitions. Please refer to chapter 4.3.3 "Partitioning the SD/MMC card" of i.MX Linux User's Guide:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 02:28:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EMMC-partition-from-kernel/m-p/1203883#M166928</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2020-12-24T02:28:25Z</dc:date>
    </item>
  </channel>
</rss>