<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Winstar LCD integration PROBLEM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Winstar-LCD-integration-PROBLEM/m-p/1203757#M166914</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the reply,&lt;/P&gt;&lt;P&gt;Can you confirm these steps?:&lt;/P&gt;&lt;P&gt;Nothing should be added in uboot configuration&lt;BR /&gt;No video parameters should be added in kernel boot parameters&lt;/P&gt;&lt;P&gt;I attached the datasheet of the LCD display. Because I don't understand what to read exactly or where to find the&amp;nbsp; registers configuration in the datasheet.&lt;/P&gt;&lt;P&gt;In the ili9881c driver there is an init instruction struct that switch pages and configure registers like this:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;struct ili9881c_instr {
enum ili9881c_op op;

union arg {
struct cmd {
u8 cmd;
u8 data;
} cmd;
u8 page;
} arg;
};

#define ILI9881C_SWITCH_PAGE_INSTR(_page) \
{ \
.op = ILI9881C_SWITCH_PAGE, \
.arg = { \
.page = (_page), \
}, \
}

#define ILI9881C_COMMAND_INSTR(_cmd, _data) \
{ \
.op = ILI9881C_COMMAND, \
.arg = { \
.cmd = { \
.cmd = (_cmd), \
.data = (_data), \
}, \
}, \
}

static const struct ili9881c_instr ili9881c_init[] = {
ILI9881C_SWITCH_PAGE_INSTR(3),
ILI9881C_COMMAND_INSTR(0x01, 0x00),
ILI9881C_COMMAND_INSTR(0x02, 0x00),
ILI9881C_COMMAND_INSTR(0x03, 0x73),
ILI9881C_COMMAND_INSTR(0x04, 0x03),
ILI9881C_COMMAND_INSTR(0x05, 0x00),
ILI9881C_COMMAND_INSTR(0x06, 0x06),
ILI9881C_COMMAND_INSTR(0x07, 0x06),
ILI9881C_COMMAND_INSTR(0x08, 0x00),
ILI9881C_COMMAND_INSTR(0x09, 0x18),
ILI9881C_COMMAND_INSTR(0x0a, 0x04),
ILI9881C_COMMAND_INSTR(0x0b, 0x00),
ILI9881C_COMMAND_INSTR(0x0c, 0x02),
ILI9881C_COMMAND_INSTR(0x0d, 0x03),
ILI9881C_COMMAND_INSTR(0x0e, 0x00),
ILI9881C_COMMAND_INSTR(0x0f, 0x25),
ILI9881C_COMMAND_INSTR(0x10, 0x25),
ILI9881C_COMMAND_INSTR(0x11, 0x00),
ILI9881C_COMMAND_INSTR(0x12, 0x00),
ILI9881C_COMMAND_INSTR(0x13, 0x00),
ILI9881C_COMMAND_INSTR(0x14, 0x00),
ILI9881C_COMMAND_INSTR(0x15, 0x00),
ILI9881C_COMMAND_INSTR(0x16, 0x0C),
ILI9881C_COMMAND_INSTR(0x17, 0x00),
ILI9881C_COMMAND_INSTR(0x18, 0x00),
ILI9881C_COMMAND_INSTR(0x19, 0x00),
ILI9881C_COMMAND_INSTR(0x1a, 0x00),
ILI9881C_COMMAND_INSTR(0x1b, 0x00),
ILI9881C_COMMAND_INSTR(0x1c, 0x00),
ILI9881C_COMMAND_INSTR(0x1d, 0x00),
ILI9881C_COMMAND_INSTR(0x1e, 0xC0),
ILI9881C_COMMAND_INSTR(0x1f, 0x80),
ILI9881C_COMMAND_INSTR(0x20, 0x04),
ILI9881C_COMMAND_INSTR(0x21, 0x01),
ILI9881C_COMMAND_INSTR(0x22, 0x00),
ILI9881C_COMMAND_INSTR(0x23, 0x00),
ILI9881C_COMMAND_INSTR(0x24, 0x00),
ILI9881C_COMMAND_INSTR(0x25, 0x00),
ILI9881C_COMMAND_INSTR(0x26, 0x00),
ILI9881C_COMMAND_INSTR(0x27, 0x00),
ILI9881C_COMMAND_INSTR(0x28, 0x33),
ILI9881C_COMMAND_INSTR(0x29, 0x03),
ILI9881C_COMMAND_INSTR(0x2a, 0x00),
ILI9881C_COMMAND_INSTR(0x2b, 0x00),
ILI9881C_COMMAND_INSTR(0x2c, 0x00),
ILI9881C_COMMAND_INSTR(0x2d, 0x00),
ILI9881C_COMMAND_INSTR(0x2e, 0x00),
ILI9881C_COMMAND_INSTR(0x2f, 0x00),
ILI9881C_COMMAND_INSTR(0x30, 0x00),
ILI9881C_COMMAND_INSTR(0x31, 0x00),
ILI9881C_COMMAND_INSTR(0x32, 0x00),
ILI9881C_COMMAND_INSTR(0x33, 0x00),
ILI9881C_COMMAND_INSTR(0x34, 0x04),
ILI9881C_COMMAND_INSTR(0x35, 0x00),
ILI9881C_COMMAND_INSTR(0x36, 0x00),
ILI9881C_COMMAND_INSTR(0x37, 0x00),
ILI9881C_COMMAND_INSTR(0x38, 0x3C),
ILI9881C_COMMAND_INSTR(0x39, 0x00),
ILI9881C_COMMAND_INSTR(0x3a, 0x00),
ILI9881C_COMMAND_INSTR(0x3b, 0x00),
ILI9881C_COMMAND_INSTR(0x3c, 0x00),
ILI9881C_COMMAND_INSTR(0x3d, 0x00),
ILI9881C_COMMAND_INSTR(0x3e, 0x00),
ILI9881C_COMMAND_INSTR(0x3f, 0x00),
ILI9881C_COMMAND_INSTR(0x40, 0x00),
ILI9881C_COMMAND_INSTR(0x41, 0x00),
ILI9881C_COMMAND_INSTR(0x42, 0x00),
ILI9881C_COMMAND_INSTR(0x43, 0x00),
ILI9881C_COMMAND_INSTR(0x44, 0x00),
ILI9881C_COMMAND_INSTR(0x50, 0x01),
ILI9881C_COMMAND_INSTR(0x51, 0x23),
ILI9881C_COMMAND_INSTR(0x52, 0x45),
ILI9881C_COMMAND_INSTR(0x53, 0x67),
ILI9881C_COMMAND_INSTR(0x54, 0x89),
ILI9881C_COMMAND_INSTR(0x55, 0xab),
ILI9881C_COMMAND_INSTR(0x56, 0x01),
ILI9881C_COMMAND_INSTR(0x57, 0x23),
ILI9881C_COMMAND_INSTR(0x58, 0x45),
ILI9881C_COMMAND_INSTR(0x59, 0x67),
ILI9881C_COMMAND_INSTR(0x5a, 0x89),
ILI9881C_COMMAND_INSTR(0x5b, 0xab),
ILI9881C_COMMAND_INSTR(0x5c, 0xcd),
ILI9881C_COMMAND_INSTR(0x5d, 0xef),
ILI9881C_COMMAND_INSTR(0x5e, 0x11),
ILI9881C_COMMAND_INSTR(0x5f, 0x02),
ILI9881C_COMMAND_INSTR(0x60, 0x02),
ILI9881C_COMMAND_INSTR(0x61, 0x02),
ILI9881C_COMMAND_INSTR(0x62, 0x02),
ILI9881C_COMMAND_INSTR(0x63, 0x02),
ILI9881C_COMMAND_INSTR(0x64, 0x02),
ILI9881C_COMMAND_INSTR(0x65, 0x02),
ILI9881C_COMMAND_INSTR(0x66, 0x02),
ILI9881C_COMMAND_INSTR(0x67, 0x02),
ILI9881C_COMMAND_INSTR(0x68, 0x02),
ILI9881C_COMMAND_INSTR(0x69, 0x02),
ILI9881C_COMMAND_INSTR(0x6a, 0x0C),
ILI9881C_COMMAND_INSTR(0x6b, 0x02),
ILI9881C_COMMAND_INSTR(0x6c, 0x0F),
ILI9881C_COMMAND_INSTR(0x6d, 0x0E),
ILI9881C_COMMAND_INSTR(0x6e, 0x0D),
ILI9881C_COMMAND_INSTR(0x6f, 0x06),
ILI9881C_COMMAND_INSTR(0x70, 0x07),
ILI9881C_COMMAND_INSTR(0x71, 0x02),
ILI9881C_COMMAND_INSTR(0x72, 0x02),
ILI9881C_COMMAND_INSTR(0x73, 0x02),
ILI9881C_COMMAND_INSTR(0x74, 0x02),
ILI9881C_COMMAND_INSTR(0x75, 0x02),
ILI9881C_COMMAND_INSTR(0x76, 0x02),
ILI9881C_COMMAND_INSTR(0x77, 0x02),
ILI9881C_COMMAND_INSTR(0x78, 0x02),
ILI9881C_COMMAND_INSTR(0x79, 0x02),
ILI9881C_COMMAND_INSTR(0x7a, 0x02),
ILI9881C_COMMAND_INSTR(0x7b, 0x02),
ILI9881C_COMMAND_INSTR(0x7c, 0x02),
ILI9881C_COMMAND_INSTR(0x7d, 0x02),
ILI9881C_COMMAND_INSTR(0x7e, 0x02),
ILI9881C_COMMAND_INSTR(0x7f, 0x02),
ILI9881C_COMMAND_INSTR(0x80, 0x0C),
ILI9881C_COMMAND_INSTR(0x81, 0x02),
ILI9881C_COMMAND_INSTR(0x82, 0x0F),
ILI9881C_COMMAND_INSTR(0x83, 0x0E),
ILI9881C_COMMAND_INSTR(0x84, 0x0D),
ILI9881C_COMMAND_INSTR(0x85, 0x06),
ILI9881C_COMMAND_INSTR(0x86, 0x07),
ILI9881C_COMMAND_INSTR(0x87, 0x02),
ILI9881C_COMMAND_INSTR(0x88, 0x02),
ILI9881C_COMMAND_INSTR(0x89, 0x02),
ILI9881C_COMMAND_INSTR(0x8A, 0x02),
ILI9881C_SWITCH_PAGE_INSTR(4),
ILI9881C_COMMAND_INSTR(0x6C, 0x15),
ILI9881C_COMMAND_INSTR(0x6E, 0x22),
ILI9881C_COMMAND_INSTR(0x6F, 0x33),
ILI9881C_COMMAND_INSTR(0x3A, 0xA4),
ILI9881C_COMMAND_INSTR(0x8D, 0x0D),
ILI9881C_COMMAND_INSTR(0x87, 0xBA),
ILI9881C_COMMAND_INSTR(0x26, 0x76),
ILI9881C_COMMAND_INSTR(0xB2, 0xD1),
ILI9881C_SWITCH_PAGE_INSTR(1),
ILI9881C_COMMAND_INSTR(0x22, 0x0A),
ILI9881C_COMMAND_INSTR(0x53, 0xDC),
ILI9881C_COMMAND_INSTR(0x55, 0xA7),
ILI9881C_COMMAND_INSTR(0x50, 0x78),
ILI9881C_COMMAND_INSTR(0x51, 0x78),
ILI9881C_COMMAND_INSTR(0x31, 0x02),
ILI9881C_COMMAND_INSTR(0x60, 0x14),
ILI9881C_COMMAND_INSTR(0xA0, 0x2A),
ILI9881C_COMMAND_INSTR(0xA1, 0x39),
ILI9881C_COMMAND_INSTR(0xA2, 0x46),
ILI9881C_COMMAND_INSTR(0xA3, 0x0e),
ILI9881C_COMMAND_INSTR(0xA4, 0x12),
ILI9881C_COMMAND_INSTR(0xA5, 0x25),
ILI9881C_COMMAND_INSTR(0xA6, 0x19),
ILI9881C_COMMAND_INSTR(0xA7, 0x1d),
ILI9881C_COMMAND_INSTR(0xA8, 0xa6),
ILI9881C_COMMAND_INSTR(0xA9, 0x1C),
ILI9881C_COMMAND_INSTR(0xAA, 0x29),
ILI9881C_COMMAND_INSTR(0xAB, 0x85),
ILI9881C_COMMAND_INSTR(0xAC, 0x1C),
ILI9881C_COMMAND_INSTR(0xAD, 0x1B),
ILI9881C_COMMAND_INSTR(0xAE, 0x51),
ILI9881C_COMMAND_INSTR(0xAF, 0x22),
ILI9881C_COMMAND_INSTR(0xB0, 0x2d),
ILI9881C_COMMAND_INSTR(0xB1, 0x4f),
ILI9881C_COMMAND_INSTR(0xB2, 0x59),
ILI9881C_COMMAND_INSTR(0xB3, 0x3F),
ILI9881C_COMMAND_INSTR(0xC0, 0x2A),
ILI9881C_COMMAND_INSTR(0xC1, 0x3a),
ILI9881C_COMMAND_INSTR(0xC2, 0x45),
ILI9881C_COMMAND_INSTR(0xC3, 0x0e),
ILI9881C_COMMAND_INSTR(0xC4, 0x11),
ILI9881C_COMMAND_INSTR(0xC5, 0x24),
ILI9881C_COMMAND_INSTR(0xC6, 0x1a),
ILI9881C_COMMAND_INSTR(0xC7, 0x1c),
ILI9881C_COMMAND_INSTR(0xC8, 0xaa),
ILI9881C_COMMAND_INSTR(0xC9, 0x1C),
ILI9881C_COMMAND_INSTR(0xCA, 0x29),
ILI9881C_COMMAND_INSTR(0xCB, 0x96),
ILI9881C_COMMAND_INSTR(0xCC, 0x1C),
ILI9881C_COMMAND_INSTR(0xCD, 0x1B),
ILI9881C_COMMAND_INSTR(0xCE, 0x51),
ILI9881C_COMMAND_INSTR(0xCF, 0x22),
ILI9881C_COMMAND_INSTR(0xD0, 0x2b),
ILI9881C_COMMAND_INSTR(0xD1, 0x4b),
ILI9881C_COMMAND_INSTR(0xD2, 0x59),
ILI9881C_COMMAND_INSTR(0xD3, 0x3F),
};&lt;/LI-CODE&gt;&lt;P&gt;Can I set those same configurations in the rm67191 cmd_set_table manufacturer_cmd_set[] and use the rm67191 driver?&lt;/P&gt;&lt;P&gt;And, I will upgrade to the 5.4.47 release and try again.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Talel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 23 Dec 2020 17:37:51 GMT</pubDate>
    <dc:creator>talel_hajsalem</dc:creator>
    <dc:date>2020-12-23T17:37:51Z</dc:date>
    <item>
      <title>Winstar LCD integration PROBLEM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Winstar-LCD-integration-PROBLEM/m-p/1203092#M166851</link>
      <description>&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;Hi All,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;We have a 5" LCD display [ Winstar WF50DSYA3MNN0#, datasheet: &lt;A href="https://www.winstar.com.tw/uploads/files/5f2c8bb6f970f8b469ca866f21523592.pdf" target="_blank" rel="noopener"&gt;https://www.winstar.com.tw/uploads/files/5f2c8bb6f970f8b469ca866f21523592.pdf&lt;/A&gt; ] &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;We are trying to integrate it into our custom IMX8MM board, the LCP display is using the MIPI interface and as specified in the datasheet it uses the ILI9881C driver. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;This is our Kernel device tree configuration (following &lt;A href="https://github.com/TechNexion-customization/linux-imx-tn/blob/tn-imx_4.14.98_2.0.0_ga-wip-mipi2lvds/arch/arm64/boot/dts/freescale/imx8mm-pico-pi-ili9881c.dts" target="_blank" rel="noopener"&gt;https://github.com/TechNexion-customization/linux-imx-tn/blob/tn-imx_4.14.98_2.0.0_ga-wip-mipi2lvds/arch/arm64/boot/dts/freescale/imx8mm-pico-pi-ili9881c.dts&lt;/A&gt; )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;&amp;amp;mipi_dsi {
	status = "okay";
	panel@0 {
		compatible = "bananapi,lhr050h41";
		reg = &amp;lt;0&amp;gt;;
		pinctrl-0 = &amp;lt;&amp;amp;pinctrl_lcd_rst&amp;gt;;
		reset-gpio = &amp;lt;&amp;amp;gpio3 25 GPIO_ACTIVE_HIGH&amp;gt;;
		dsi-lanes = &amp;lt;4&amp;gt;;
		video-mode = &amp;lt;0&amp;gt;;	/* 0: burst mode
					 * 1: non-burst mode with sync event
					 * 2: non-burst mode with sync pulse
					 */
		panel-width-mm = &amp;lt;720&amp;gt;;
		panel-height-mm = &amp;lt;1280&amp;gt;;
		status = "okay";
	};
};

&amp;amp;lcdif {
	status = "okay";
};
&amp;amp;vpu_g1 {
status = "okay";
};

&amp;amp;vpu_g2 {
status = "okay";
};

&amp;amp;vpu_h1 {
status = "okay";
};

&amp;amp;gpu {
status = "okay";
};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The "bananapi,lhr050h41" compatible value is taken from the official ILI9881C kernel MIPI DSI driver,&lt;/P&gt;&lt;P&gt;As far as I understand and following the EVK implementation of the rm67191 driver I do not need to add something to uboot bootargs like "video=mxcfb0...", and nothing to be added to Uboot device tree also, the only configuration should be only in the Kernel device tree file.&lt;/P&gt;&lt;P&gt;When booting the Kernel errors occur related to the IMX display-subsystem:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[    4.660791] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    4.667467] [drm] No driver support for vblank timestamp query.
[    4.673536] imx-drm soc@0:bus@32c00000:display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops)
[    4.691442] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200
[    4.698594] ina2xx 2-0041: power monitor ina219 (Rshunt = 20000 uOhm)
[    4.698686] imx_sec_dsim_drv 32e10000.mipi_dsi: Failed to attach bridge: 32e10000.mipi_dsi
[    4.713441] imx_sec_dsim_drv 32e10000.mipi_dsi: failed to bind sec dsim bridge: -517
[    4.719314] ina2xx 2-0042: power monitor ina219 (Rshunt = 20000 uOhm)
[    4.727269] imx-drm soc@0:bus@32c00000:display-subsystem: failed to bind 32e10000.mipi_dsi (ops imx_sec_dsim_ops): -517
[    4.738615] imx-drm soc@0:bus@32c00000:display-subsystem: master bind failed: -517&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;- What is the problem with drm kernel errors?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;I checked the EVK uboot header file and defconfig and they contain VIDEO configuration:&lt;/SPAN&gt;&lt;/P&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;SPAN&gt;&lt;STRONG&gt;&lt;SPAN&gt;imx8mm_evk_defconfig&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/TD&gt;&lt;TD&gt;&lt;SPAN&gt;&lt;STRONG&gt;&lt;SPAN&gt;imx8mm_evk.h&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;SPAN&gt;CONFIG_VIDEO=y&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CONFIG_IMX_SEC_MIPI_DSI=y&lt;/SPAN&gt;&lt;/TD&gt;&lt;TD&gt;&lt;SPAN&gt;#ifdef CONFIG_VIDEO&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define CONFIG_VIDEO_MXS&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define CONFIG_VIDEO_LOGO&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define CONFIG_SPLASH_SCREEN&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define CONFIG_SPLASH_SCREEN_ALIGN&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define CONFIG_CMD_BMP&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define CONFIG_BMP_16BPP&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define CONFIG_VIDEO_BMP_RLE8&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define CONFIG_VIDEO_BMP_LOGO&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define CONFIG_IMX_VIDEO_SKIP&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define CONFIG_RM67191&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif&lt;/SPAN&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;I'm using imx8mmddr3lval yocto MACHINE and working with L5.4.24 release but it does not contain those VIDEO configurations, is that the missing part? If yes, I tried to add it and compilation errors occurred:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;| u-boot-imx/2018.03-r0/git/arch/arm/mach-imx/video.c:13: undefined reference to `displays'
| aarch64-poky-linux-ld.bfd: arch/arm/mach-imx/built-in.o: relocation R_AARCH64_ADR_PREL_PG_HI21 against symbol `displays' which may bind externally can not be used when making a shared object; recompile with -fPIC
| u-boot-imx/2018.03-r0/git/arch/arm/mach-imx/video.c:13:(.text.board_video_skip+0x14): dangerous relocation: unsupported relocation
| u-boot-imx/2018.03-r0/git/arch/arm/mach-imx/video.c:13: undefined reference to `displays'
| u-boot-imx/2018.03-r0/git/arch/arm/mach-imx/video.c:13: undefined reference to `display_count'
| aarch64-poky-linux-ld.bfd: arch/arm/mach-imx/built-in.o: relocation R_AARCH64_ADR_PREL_PG_HI21 against symbol `display_count' which may bind externally can not be used when making a shared object; recompile with -fPIC
| u-boot-imx/2018.03-r0/git/arch/arm/mach-imx/video.c:13:(.text.board_video_skip+0x24): dangerous relocation: unsupported relocation
|u-boot-imx/2018.03-r0/git/arch/arm/mach-imx/video.c:13: undefined reference to `display_count'
|u-boot-imx/2018.03-r0/git/arch/arm/mach-imx/video.c:39: undefined reference to `display_count'
| u-boot-imx/2018.03-r0/git/Makefile:1304: recipe for target 'u-boot' failed&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I'm missing?&lt;/P&gt;&lt;P&gt;Help me, please.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Talel&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 13:48:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Winstar-LCD-integration-PROBLEM/m-p/1203092#M166851</guid>
      <dc:creator>talel_hajsalem</dc:creator>
      <dc:date>2020-12-22T13:48:26Z</dc:date>
    </item>
    <item>
      <title>Re: Winstar LCD integration PROBLEM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Winstar-LCD-integration-PROBLEM/m-p/1203275#M166862</link>
      <description>&lt;P&gt;Hi Talel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;may be recommended to try more new uboot/kernels, like L5.4.47_2.2.0&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/arch/arm/dts/imx8mm-evk.dts?h=imx_v2020.04_5.4.47_2.2.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/arch/arm/dts/imx8mm-evk.dts?h=imx_v2020.04_5.4.47_2.2.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;add custom&amp;nbsp;&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow  is-read-only"&gt;&lt;SPAN class="uiOutputTextArea"&gt;Winstar &lt;/SPAN&gt;&lt;/SPAN&gt; initialization (from its datasheet) in "cmd_set_table manufacturer_cmd_set[]"&lt;/P&gt;
&lt;P&gt;and "struct display_timing default_timing" in&lt;/P&gt;
&lt;P&gt;&lt;A href="https://source.codeaurora.org/external/imx/uboot-imx/tree/drivers/video/raydium-rm67191.c?h=imx_v2020.04_5.4.47_2.2.0" target="_blank"&gt;https://source.codeaurora.org/external/imx/uboot-imx/tree/drivers/video/raydium-rm67191.c?h=imx_v2020.04_5.4.47_2.2.0&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Wed, 23 Dec 2020 00:29:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Winstar-LCD-integration-PROBLEM/m-p/1203275#M166862</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-12-23T00:29:19Z</dc:date>
    </item>
    <item>
      <title>Re: Winstar LCD integration PROBLEM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Winstar-LCD-integration-PROBLEM/m-p/1203757#M166914</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the reply,&lt;/P&gt;&lt;P&gt;Can you confirm these steps?:&lt;/P&gt;&lt;P&gt;Nothing should be added in uboot configuration&lt;BR /&gt;No video parameters should be added in kernel boot parameters&lt;/P&gt;&lt;P&gt;I attached the datasheet of the LCD display. Because I don't understand what to read exactly or where to find the&amp;nbsp; registers configuration in the datasheet.&lt;/P&gt;&lt;P&gt;In the ili9881c driver there is an init instruction struct that switch pages and configure registers like this:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;struct ili9881c_instr {
enum ili9881c_op op;

union arg {
struct cmd {
u8 cmd;
u8 data;
} cmd;
u8 page;
} arg;
};

#define ILI9881C_SWITCH_PAGE_INSTR(_page) \
{ \
.op = ILI9881C_SWITCH_PAGE, \
.arg = { \
.page = (_page), \
}, \
}

#define ILI9881C_COMMAND_INSTR(_cmd, _data) \
{ \
.op = ILI9881C_COMMAND, \
.arg = { \
.cmd = { \
.cmd = (_cmd), \
.data = (_data), \
}, \
}, \
}

static const struct ili9881c_instr ili9881c_init[] = {
ILI9881C_SWITCH_PAGE_INSTR(3),
ILI9881C_COMMAND_INSTR(0x01, 0x00),
ILI9881C_COMMAND_INSTR(0x02, 0x00),
ILI9881C_COMMAND_INSTR(0x03, 0x73),
ILI9881C_COMMAND_INSTR(0x04, 0x03),
ILI9881C_COMMAND_INSTR(0x05, 0x00),
ILI9881C_COMMAND_INSTR(0x06, 0x06),
ILI9881C_COMMAND_INSTR(0x07, 0x06),
ILI9881C_COMMAND_INSTR(0x08, 0x00),
ILI9881C_COMMAND_INSTR(0x09, 0x18),
ILI9881C_COMMAND_INSTR(0x0a, 0x04),
ILI9881C_COMMAND_INSTR(0x0b, 0x00),
ILI9881C_COMMAND_INSTR(0x0c, 0x02),
ILI9881C_COMMAND_INSTR(0x0d, 0x03),
ILI9881C_COMMAND_INSTR(0x0e, 0x00),
ILI9881C_COMMAND_INSTR(0x0f, 0x25),
ILI9881C_COMMAND_INSTR(0x10, 0x25),
ILI9881C_COMMAND_INSTR(0x11, 0x00),
ILI9881C_COMMAND_INSTR(0x12, 0x00),
ILI9881C_COMMAND_INSTR(0x13, 0x00),
ILI9881C_COMMAND_INSTR(0x14, 0x00),
ILI9881C_COMMAND_INSTR(0x15, 0x00),
ILI9881C_COMMAND_INSTR(0x16, 0x0C),
ILI9881C_COMMAND_INSTR(0x17, 0x00),
ILI9881C_COMMAND_INSTR(0x18, 0x00),
ILI9881C_COMMAND_INSTR(0x19, 0x00),
ILI9881C_COMMAND_INSTR(0x1a, 0x00),
ILI9881C_COMMAND_INSTR(0x1b, 0x00),
ILI9881C_COMMAND_INSTR(0x1c, 0x00),
ILI9881C_COMMAND_INSTR(0x1d, 0x00),
ILI9881C_COMMAND_INSTR(0x1e, 0xC0),
ILI9881C_COMMAND_INSTR(0x1f, 0x80),
ILI9881C_COMMAND_INSTR(0x20, 0x04),
ILI9881C_COMMAND_INSTR(0x21, 0x01),
ILI9881C_COMMAND_INSTR(0x22, 0x00),
ILI9881C_COMMAND_INSTR(0x23, 0x00),
ILI9881C_COMMAND_INSTR(0x24, 0x00),
ILI9881C_COMMAND_INSTR(0x25, 0x00),
ILI9881C_COMMAND_INSTR(0x26, 0x00),
ILI9881C_COMMAND_INSTR(0x27, 0x00),
ILI9881C_COMMAND_INSTR(0x28, 0x33),
ILI9881C_COMMAND_INSTR(0x29, 0x03),
ILI9881C_COMMAND_INSTR(0x2a, 0x00),
ILI9881C_COMMAND_INSTR(0x2b, 0x00),
ILI9881C_COMMAND_INSTR(0x2c, 0x00),
ILI9881C_COMMAND_INSTR(0x2d, 0x00),
ILI9881C_COMMAND_INSTR(0x2e, 0x00),
ILI9881C_COMMAND_INSTR(0x2f, 0x00),
ILI9881C_COMMAND_INSTR(0x30, 0x00),
ILI9881C_COMMAND_INSTR(0x31, 0x00),
ILI9881C_COMMAND_INSTR(0x32, 0x00),
ILI9881C_COMMAND_INSTR(0x33, 0x00),
ILI9881C_COMMAND_INSTR(0x34, 0x04),
ILI9881C_COMMAND_INSTR(0x35, 0x00),
ILI9881C_COMMAND_INSTR(0x36, 0x00),
ILI9881C_COMMAND_INSTR(0x37, 0x00),
ILI9881C_COMMAND_INSTR(0x38, 0x3C),
ILI9881C_COMMAND_INSTR(0x39, 0x00),
ILI9881C_COMMAND_INSTR(0x3a, 0x00),
ILI9881C_COMMAND_INSTR(0x3b, 0x00),
ILI9881C_COMMAND_INSTR(0x3c, 0x00),
ILI9881C_COMMAND_INSTR(0x3d, 0x00),
ILI9881C_COMMAND_INSTR(0x3e, 0x00),
ILI9881C_COMMAND_INSTR(0x3f, 0x00),
ILI9881C_COMMAND_INSTR(0x40, 0x00),
ILI9881C_COMMAND_INSTR(0x41, 0x00),
ILI9881C_COMMAND_INSTR(0x42, 0x00),
ILI9881C_COMMAND_INSTR(0x43, 0x00),
ILI9881C_COMMAND_INSTR(0x44, 0x00),
ILI9881C_COMMAND_INSTR(0x50, 0x01),
ILI9881C_COMMAND_INSTR(0x51, 0x23),
ILI9881C_COMMAND_INSTR(0x52, 0x45),
ILI9881C_COMMAND_INSTR(0x53, 0x67),
ILI9881C_COMMAND_INSTR(0x54, 0x89),
ILI9881C_COMMAND_INSTR(0x55, 0xab),
ILI9881C_COMMAND_INSTR(0x56, 0x01),
ILI9881C_COMMAND_INSTR(0x57, 0x23),
ILI9881C_COMMAND_INSTR(0x58, 0x45),
ILI9881C_COMMAND_INSTR(0x59, 0x67),
ILI9881C_COMMAND_INSTR(0x5a, 0x89),
ILI9881C_COMMAND_INSTR(0x5b, 0xab),
ILI9881C_COMMAND_INSTR(0x5c, 0xcd),
ILI9881C_COMMAND_INSTR(0x5d, 0xef),
ILI9881C_COMMAND_INSTR(0x5e, 0x11),
ILI9881C_COMMAND_INSTR(0x5f, 0x02),
ILI9881C_COMMAND_INSTR(0x60, 0x02),
ILI9881C_COMMAND_INSTR(0x61, 0x02),
ILI9881C_COMMAND_INSTR(0x62, 0x02),
ILI9881C_COMMAND_INSTR(0x63, 0x02),
ILI9881C_COMMAND_INSTR(0x64, 0x02),
ILI9881C_COMMAND_INSTR(0x65, 0x02),
ILI9881C_COMMAND_INSTR(0x66, 0x02),
ILI9881C_COMMAND_INSTR(0x67, 0x02),
ILI9881C_COMMAND_INSTR(0x68, 0x02),
ILI9881C_COMMAND_INSTR(0x69, 0x02),
ILI9881C_COMMAND_INSTR(0x6a, 0x0C),
ILI9881C_COMMAND_INSTR(0x6b, 0x02),
ILI9881C_COMMAND_INSTR(0x6c, 0x0F),
ILI9881C_COMMAND_INSTR(0x6d, 0x0E),
ILI9881C_COMMAND_INSTR(0x6e, 0x0D),
ILI9881C_COMMAND_INSTR(0x6f, 0x06),
ILI9881C_COMMAND_INSTR(0x70, 0x07),
ILI9881C_COMMAND_INSTR(0x71, 0x02),
ILI9881C_COMMAND_INSTR(0x72, 0x02),
ILI9881C_COMMAND_INSTR(0x73, 0x02),
ILI9881C_COMMAND_INSTR(0x74, 0x02),
ILI9881C_COMMAND_INSTR(0x75, 0x02),
ILI9881C_COMMAND_INSTR(0x76, 0x02),
ILI9881C_COMMAND_INSTR(0x77, 0x02),
ILI9881C_COMMAND_INSTR(0x78, 0x02),
ILI9881C_COMMAND_INSTR(0x79, 0x02),
ILI9881C_COMMAND_INSTR(0x7a, 0x02),
ILI9881C_COMMAND_INSTR(0x7b, 0x02),
ILI9881C_COMMAND_INSTR(0x7c, 0x02),
ILI9881C_COMMAND_INSTR(0x7d, 0x02),
ILI9881C_COMMAND_INSTR(0x7e, 0x02),
ILI9881C_COMMAND_INSTR(0x7f, 0x02),
ILI9881C_COMMAND_INSTR(0x80, 0x0C),
ILI9881C_COMMAND_INSTR(0x81, 0x02),
ILI9881C_COMMAND_INSTR(0x82, 0x0F),
ILI9881C_COMMAND_INSTR(0x83, 0x0E),
ILI9881C_COMMAND_INSTR(0x84, 0x0D),
ILI9881C_COMMAND_INSTR(0x85, 0x06),
ILI9881C_COMMAND_INSTR(0x86, 0x07),
ILI9881C_COMMAND_INSTR(0x87, 0x02),
ILI9881C_COMMAND_INSTR(0x88, 0x02),
ILI9881C_COMMAND_INSTR(0x89, 0x02),
ILI9881C_COMMAND_INSTR(0x8A, 0x02),
ILI9881C_SWITCH_PAGE_INSTR(4),
ILI9881C_COMMAND_INSTR(0x6C, 0x15),
ILI9881C_COMMAND_INSTR(0x6E, 0x22),
ILI9881C_COMMAND_INSTR(0x6F, 0x33),
ILI9881C_COMMAND_INSTR(0x3A, 0xA4),
ILI9881C_COMMAND_INSTR(0x8D, 0x0D),
ILI9881C_COMMAND_INSTR(0x87, 0xBA),
ILI9881C_COMMAND_INSTR(0x26, 0x76),
ILI9881C_COMMAND_INSTR(0xB2, 0xD1),
ILI9881C_SWITCH_PAGE_INSTR(1),
ILI9881C_COMMAND_INSTR(0x22, 0x0A),
ILI9881C_COMMAND_INSTR(0x53, 0xDC),
ILI9881C_COMMAND_INSTR(0x55, 0xA7),
ILI9881C_COMMAND_INSTR(0x50, 0x78),
ILI9881C_COMMAND_INSTR(0x51, 0x78),
ILI9881C_COMMAND_INSTR(0x31, 0x02),
ILI9881C_COMMAND_INSTR(0x60, 0x14),
ILI9881C_COMMAND_INSTR(0xA0, 0x2A),
ILI9881C_COMMAND_INSTR(0xA1, 0x39),
ILI9881C_COMMAND_INSTR(0xA2, 0x46),
ILI9881C_COMMAND_INSTR(0xA3, 0x0e),
ILI9881C_COMMAND_INSTR(0xA4, 0x12),
ILI9881C_COMMAND_INSTR(0xA5, 0x25),
ILI9881C_COMMAND_INSTR(0xA6, 0x19),
ILI9881C_COMMAND_INSTR(0xA7, 0x1d),
ILI9881C_COMMAND_INSTR(0xA8, 0xa6),
ILI9881C_COMMAND_INSTR(0xA9, 0x1C),
ILI9881C_COMMAND_INSTR(0xAA, 0x29),
ILI9881C_COMMAND_INSTR(0xAB, 0x85),
ILI9881C_COMMAND_INSTR(0xAC, 0x1C),
ILI9881C_COMMAND_INSTR(0xAD, 0x1B),
ILI9881C_COMMAND_INSTR(0xAE, 0x51),
ILI9881C_COMMAND_INSTR(0xAF, 0x22),
ILI9881C_COMMAND_INSTR(0xB0, 0x2d),
ILI9881C_COMMAND_INSTR(0xB1, 0x4f),
ILI9881C_COMMAND_INSTR(0xB2, 0x59),
ILI9881C_COMMAND_INSTR(0xB3, 0x3F),
ILI9881C_COMMAND_INSTR(0xC0, 0x2A),
ILI9881C_COMMAND_INSTR(0xC1, 0x3a),
ILI9881C_COMMAND_INSTR(0xC2, 0x45),
ILI9881C_COMMAND_INSTR(0xC3, 0x0e),
ILI9881C_COMMAND_INSTR(0xC4, 0x11),
ILI9881C_COMMAND_INSTR(0xC5, 0x24),
ILI9881C_COMMAND_INSTR(0xC6, 0x1a),
ILI9881C_COMMAND_INSTR(0xC7, 0x1c),
ILI9881C_COMMAND_INSTR(0xC8, 0xaa),
ILI9881C_COMMAND_INSTR(0xC9, 0x1C),
ILI9881C_COMMAND_INSTR(0xCA, 0x29),
ILI9881C_COMMAND_INSTR(0xCB, 0x96),
ILI9881C_COMMAND_INSTR(0xCC, 0x1C),
ILI9881C_COMMAND_INSTR(0xCD, 0x1B),
ILI9881C_COMMAND_INSTR(0xCE, 0x51),
ILI9881C_COMMAND_INSTR(0xCF, 0x22),
ILI9881C_COMMAND_INSTR(0xD0, 0x2b),
ILI9881C_COMMAND_INSTR(0xD1, 0x4b),
ILI9881C_COMMAND_INSTR(0xD2, 0x59),
ILI9881C_COMMAND_INSTR(0xD3, 0x3F),
};&lt;/LI-CODE&gt;&lt;P&gt;Can I set those same configurations in the rm67191 cmd_set_table manufacturer_cmd_set[] and use the rm67191 driver?&lt;/P&gt;&lt;P&gt;And, I will upgrade to the 5.4.47 release and try again.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Talel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Dec 2020 17:37:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Winstar-LCD-integration-PROBLEM/m-p/1203757#M166914</guid>
      <dc:creator>talel_hajsalem</dc:creator>
      <dc:date>2020-12-23T17:37:51Z</dc:date>
    </item>
  </channel>
</rss>