<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using QuadSPI to access SRAM Memory in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-QuadSPI-to-access-SRAM-Memory/m-p/1203126#M166855</link>
    <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thanks for these hints.&lt;/P&gt;&lt;P&gt;I've seen the following ressource : &lt;A href="https://elixir.bootlin.com/linux/latest/source/drivers/mtd/devices/mchp23k256.c" target="_self"&gt;https://elixir.bootlin.com/linux/latest/source/drivers/mtd/devices/mchp23k256.c&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm wondering if it could be a good start too.&lt;/P&gt;</description>
    <pubDate>Tue, 22 Dec 2020 15:06:41 GMT</pubDate>
    <dc:creator>frk</dc:creator>
    <dc:date>2020-12-22T15:06:41Z</dc:date>
    <item>
      <title>Using QuadSPI to access SRAM Memory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-QuadSPI-to-access-SRAM-Memory/m-p/1199657#M166508</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi everyone,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm actually trying to use the QuadSpi bus to access to a SRAM memory with an&lt;/SPAN&gt; i.MX8m &lt;SPAN&gt;(kernel 5.4.70) but I don't know where to begin with as I didn't find any drivers for the memory in the kernel sources.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The memory I want to use is a 65WVS5128GALL from ISSI.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;How can I map the SRAM to &lt;/SPAN&gt;&lt;SPAN&gt;QuadSpi and see the mtd device in the userspace? Using device tree I assume but without specific driver for the memory?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 12:47:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-QuadSPI-to-access-SRAM-Memory/m-p/1199657#M166508</guid>
      <dc:creator>frk</dc:creator>
      <dc:date>2020-12-15T12:47:18Z</dc:date>
    </item>
    <item>
      <title>Re: Using QuadSPI to access SRAM Memory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-QuadSPI-to-access-SRAM-Memory/m-p/1199961#M166540</link>
      <description>&lt;P&gt;Hi frk&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;unfortunately such devices are not supported in nxp bsps and new driver with&lt;/P&gt;
&lt;P&gt;specific LUT (Look-up Table) for that device should be developed.&lt;/P&gt;
&lt;P&gt;One can start with sect.3.8 SPI NOR Flash Memory Technology Device (MTD)&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A style="box-sizing: border-box; background-color: transparent; color: #215bd6; text-decoration: none; cursor: pointer;" href="https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf" target="_blank" rel="noopener"&gt;i.MX Linux Reference Manual​&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Look-up Table description can be found in sect.10.2.4.3.4 Look-up Table,&lt;/P&gt;
&lt;P&gt;sect.10.2.7.1.3 Fast Read Quad Output (Winbond)&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_3" href="https://www.nxp.com/webapp/Download?colCode=IMX8MDQLQRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Dec 2020 00:51:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-QuadSPI-to-access-SRAM-Memory/m-p/1199961#M166540</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-12-16T00:51:37Z</dc:date>
    </item>
    <item>
      <title>Re: Using QuadSPI to access SRAM Memory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-QuadSPI-to-access-SRAM-Memory/m-p/1203126#M166855</link>
      <description>&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thanks for these hints.&lt;/P&gt;&lt;P&gt;I've seen the following ressource : &lt;A href="https://elixir.bootlin.com/linux/latest/source/drivers/mtd/devices/mchp23k256.c" target="_self"&gt;https://elixir.bootlin.com/linux/latest/source/drivers/mtd/devices/mchp23k256.c&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm wondering if it could be a good start too.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 15:06:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-QuadSPI-to-access-SRAM-Memory/m-p/1203126#M166855</guid>
      <dc:creator>frk</dc:creator>
      <dc:date>2020-12-22T15:06:41Z</dc:date>
    </item>
  </channel>
</rss>