<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: There is a problem in burning the android-10.0.0_2.5.0_image to the EMMC of 8 mmevk in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/There-is-a-problem-in-burning-the-android-10-0-0-2-5-0-image-to/m-p/1202301#M166779</link>
    <description>&lt;P&gt;I have tested on my imx8mm lpddr4 evk board successfully, pls see the screenshot as below:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="joanxie_1-1608535773760.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133162i0C37806F42EE7987/image-size/medium?v=v2&amp;amp;px=400" role="button" title="joanxie_1-1608535773760.png" alt="joanxie_1-1608535773760.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I tested on my win10 PC, and I tested uuu 1.3.124 version and 1.4.43 version&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 21 Dec 2020 07:30:32 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2020-12-21T07:30:32Z</dc:date>
    <item>
      <title>There is a problem in burning the android-10.0.0_2.5.0_image to the EMMC of 8 mmevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/There-is-a-problem-in-burning-the-android-10-0-0-2-5-0-image-to/m-p/1200855#M166614</link>
      <description>&lt;P&gt;Hi NXP team&lt;/P&gt;&lt;P&gt;I am using i.mx 8m mini evk lpddr4 borad to test android-10.0.0_2.5.0_image_8mmevk image .&lt;/P&gt;&lt;P&gt;I know that the demo image of Android 10.0 only supports EMMC boot, but when I use the command(uuu_imx_android_flash.bat -f imx8mm -a -e or uuu_imx_android_flash.bat -f imx8mm -u trusty) to burn, it will fail, and the burning of Android_O8 or Android_ P9 can succeed. What's the problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;H:\imx8mm\android-10.0.0_2.5.0_image_8mmevk&amp;gt;uuu_imx_android_flash.bat -f imx8mm -u trusty&lt;BR /&gt;This script is validated with uuu 1.3.124 version, it is recommended to align wi&lt;BR /&gt;th this version.&lt;BR /&gt;dtbo is supported&lt;BR /&gt;dual slot is supported&lt;BR /&gt;dynamic partition is supported&lt;BR /&gt;generate lines to flash u-boot-imx8mm-trusty.imx to the partition of bootloader0&lt;/P&gt;&lt;P&gt;generate lines to flash partition-table.img to the partition of gpt&lt;BR /&gt;generate lines to flash dtbo-imx8mm.img to the partition of dtbo_a&lt;BR /&gt;generate lines to flash boot.img to the partition of boot_a&lt;BR /&gt;generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_a&lt;BR /&gt;generate lines to flash dtbo-imx8mm.img to the partition of dtbo_b&lt;BR /&gt;generate lines to flash boot.img to the partition of boot_b&lt;BR /&gt;generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_b&lt;BR /&gt;lpmake.exe I 12-17 10:42:53 1140 8700 builder.cpp:937] [liblp]Partition system&lt;BR /&gt;_a will resize from 0 bytes to 919138304 bytes&lt;BR /&gt;lpmake.exe I 12-17 10:42:53 1140 8700 builder.cpp:937] [liblp]Partition system&lt;BR /&gt;_b will resize from 0 bytes to 919138304 bytes&lt;BR /&gt;lpmake.exe I 12-17 10:42:53 1140 8700 builder.cpp:937] [liblp]Partition vendor&lt;BR /&gt;_a will resize from 0 bytes to 76460032 bytes&lt;BR /&gt;lpmake.exe I 12-17 10:42:53 1140 8700 builder.cpp:937] [liblp]Partition vendor&lt;BR /&gt;_b will resize from 0 bytes to 76460032 bytes&lt;BR /&gt;lpmake.exe I 12-17 10:42:53 1140 8700 builder.cpp:937] [liblp]Partition produc&lt;BR /&gt;t_a will resize from 0 bytes to 335372288 bytes&lt;BR /&gt;lpmake.exe I 12-17 10:42:53 1140 8700 builder.cpp:937] [liblp]Partition produc&lt;BR /&gt;t_b will resize from 0 bytes to 335372288 bytes&lt;BR /&gt;generate lines to flash super.img to the partition of super&lt;BR /&gt;uuu script generated, start to invoke uuu with the generated uuu script&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.69-0-g63b1d3c&lt;/P&gt;&lt;P&gt;Your console don't support VT mode, fail back to verbose mode&lt;BR /&gt;Build in config:&lt;BR /&gt;Pctl Chip Vid Pid BcdVersion&lt;BR /&gt;==================================================&lt;BR /&gt;SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8DXL 0x1fc9 0x0147&lt;BR /&gt;SDPS: MX28 0x15a2 0x004f&lt;BR /&gt;SDPS: MX815 0x1fc9 0x013e&lt;BR /&gt;SDPS: MX865 0x1fc9 0x0146&lt;BR /&gt;SDP: MX7D 0x15a2 0x0076&lt;BR /&gt;SDP: MX6Q 0x15a2 0x0054&lt;BR /&gt;SDP: MX6D 0x15a2 0x0061&lt;BR /&gt;SDP: MX6SL 0x15a2 0x0063&lt;BR /&gt;SDP: MX6SX 0x15a2 0x0071&lt;BR /&gt;SDP: MX6UL 0x15a2 0x007d&lt;BR /&gt;SDP: MX6ULL 0x15a2 0x0080&lt;BR /&gt;SDP: MX6SLL 0x1fc9 0x0128&lt;BR /&gt;SDP: MX7ULP 0x1fc9 0x0126&lt;BR /&gt;SDP: MXRT106X 0x1fc9 0x0135&lt;BR /&gt;SDP: MX8MM 0x1fc9 0x0134&lt;BR /&gt;SDP: MX8MQ 0x1fc9 0x012b&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]&lt;BR /&gt;SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]&lt;BR /&gt;FBK: 0x066f 0x9afe&lt;BR /&gt;FBK: 0x066f 0x9bff&lt;BR /&gt;FB: 0x0525 0xa4a5&lt;BR /&gt;FB: 0x18d1 0x0d02&lt;BR /&gt;FB: 0x3016 0x0001&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;New USB Device Attached at 2:2&lt;BR /&gt;2:2&amp;gt;Start Cmd:SDP: boot -f u-boot-imx8mm-evk-uuu.imx.link&lt;BR /&gt;6400%2:2&amp;gt;Okay (0.871s)&lt;BR /&gt;New USB Device Attached at 2:2&lt;BR /&gt;2:2&amp;gt;Start Cmd:SDPV: delay 1000&lt;BR /&gt;2:2&amp;gt;Okay (0.998s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:SDPV: write -f u-boot-imx8mm-evk-uuu.imx.link -skipspl&lt;BR /&gt;2:2&amp;gt;Fail HID(W):LIBUSB_ERROR_IO(0.002s)&lt;BR /&gt;&amp;#27;[?25h&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;H:\imx8mm\android-10.0.0_2.5.0_image_8mmevk&amp;gt;uuu_imx_android_flash.bat -f imx8mm -a -e&lt;BR /&gt;This script is validated with uuu 1.3.124 version, it is recommended to align wi&lt;BR /&gt;th this version.&lt;BR /&gt;dtbo is supported&lt;BR /&gt;dual slot is supported&lt;BR /&gt;dynamic partition is supported&lt;BR /&gt;generate lines to flash u-boot-imx8mm.imx to the partition of bootloader0&lt;BR /&gt;generate lines to flash partition-table.img to the partition of gpt&lt;BR /&gt;generate lines to flash dtbo-imx8mm.img to the partition of dtbo_a&lt;BR /&gt;generate lines to flash boot.img to the partition of boot_a&lt;BR /&gt;generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_a&lt;BR /&gt;lpmake.exe I 12-17 10:16:13 4324 7832 builder.cpp:937] [liblp]Partition system&lt;BR /&gt;_a will resize from 0 bytes to 919138304 bytes&lt;BR /&gt;lpmake.exe I 12-17 10:16:13 4324 7832 builder.cpp:937] [liblp]Partition vendor&lt;BR /&gt;_a will resize from 0 bytes to 76460032 bytes&lt;BR /&gt;lpmake.exe I 12-17 10:16:13 4324 7832 builder.cpp:937] [liblp]Partition produc&lt;BR /&gt;t_a will resize from 0 bytes to 335372288 bytes&lt;BR /&gt;generate lines to flash super.img to the partition of super&lt;BR /&gt;uuu script generated, start to invoke uuu with the generated uuu script&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.69-0-g63b1d3c&lt;/P&gt;&lt;P&gt;Your console don't support VT mode, fail back to verbose mode&lt;BR /&gt;Build in config:&lt;BR /&gt;Pctl Chip Vid Pid BcdVersion&lt;BR /&gt;==================================================&lt;BR /&gt;SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]&lt;BR /&gt;SDPS: MX8DXL 0x1fc9 0x0147&lt;BR /&gt;SDPS: MX28 0x15a2 0x004f&lt;BR /&gt;SDPS: MX815 0x1fc9 0x013e&lt;BR /&gt;SDPS: MX865 0x1fc9 0x0146&lt;BR /&gt;SDP: MX7D 0x15a2 0x0076&lt;BR /&gt;SDP: MX6Q 0x15a2 0x0054&lt;BR /&gt;SDP: MX6D 0x15a2 0x0061&lt;BR /&gt;SDP: MX6SL 0x15a2 0x0063&lt;BR /&gt;SDP: MX6SX 0x15a2 0x0071&lt;BR /&gt;SDP: MX6UL 0x15a2 0x007d&lt;BR /&gt;SDP: MX6ULL 0x15a2 0x0080&lt;BR /&gt;SDP: MX6SLL 0x1fc9 0x0128&lt;BR /&gt;SDP: MX7ULP 0x1fc9 0x0126&lt;BR /&gt;SDP: MXRT106X 0x1fc9 0x0135&lt;BR /&gt;SDP: MX8MM 0x1fc9 0x0134&lt;BR /&gt;SDP: MX8MQ 0x1fc9 0x012b&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]&lt;BR /&gt;SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]&lt;BR /&gt;SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]&lt;BR /&gt;SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]&lt;BR /&gt;FBK: 0x066f 0x9afe&lt;BR /&gt;FBK: 0x066f 0x9bff&lt;BR /&gt;FB: 0x0525 0xa4a5&lt;BR /&gt;FB: 0x18d1 0x0d02&lt;BR /&gt;FB: 0x3016 0x0001&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;New USB Device Attached at 2:2&lt;BR /&gt;2:2&amp;gt;Start Cmd:SDP: boot -f u-boot-imx8mm-evk-uuu.imx.link&lt;BR /&gt;6400%2:2&amp;gt;Okay (1.953s)&lt;BR /&gt;New USB Device Attached at 2:2&lt;BR /&gt;2:2&amp;gt;Start Cmd:SDPV: delay 1000&lt;BR /&gt;2:2&amp;gt;Okay (0.993s)&lt;BR /&gt;2:2&amp;gt;Start Cmd:SDPV: write -f u-boot-imx8mm-evk-uuu.imx.link -skipspl&lt;BR /&gt;2:2&amp;gt;Fail HID(W):LIBUSB_ERROR_IO(0.003s)&lt;BR /&gt;&amp;#27;[?25h&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 03:18:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/There-is-a-problem-in-burning-the-android-10-0-0-2-5-0-image-to/m-p/1200855#M166614</guid>
      <dc:creator>pengluo</dc:creator>
      <dc:date>2020-12-17T03:18:09Z</dc:date>
    </item>
    <item>
      <title>Re: There is a problem in burning the android-10.0.0_2.5.0_image to the EMMC of 8 mmevk</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/There-is-a-problem-in-burning-the-android-10-0-0-2-5-0-image-to/m-p/1202301#M166779</link>
      <description>&lt;P&gt;I have tested on my imx8mm lpddr4 evk board successfully, pls see the screenshot as below:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="joanxie_1-1608535773760.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133162i0C37806F42EE7987/image-size/medium?v=v2&amp;amp;px=400" role="button" title="joanxie_1-1608535773760.png" alt="joanxie_1-1608535773760.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I tested on my win10 PC, and I tested uuu 1.3.124 version and 1.4.43 version&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 07:30:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/There-is-a-problem-in-burning-the-android-10-0-0-2-5-0-image-to/m-p/1202301#M166779</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-12-21T07:30:32Z</dc:date>
    </item>
  </channel>
</rss>