<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is it possible to interface two displays with MIPI interface in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-interface-two-displays-with-MIPI-interface/m-p/1202128#M166762</link>
    <description>&lt;P&gt;one can use the command like:&lt;/P&gt;
&lt;P&gt;"gplay-1.0 /unit_tests/test.mp4 --video-sink="kmssink driver-name=imx-dcss" &amp;amp; gplay-1.0 /unit_tests/test.mp4"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 21 Dec 2020 02:17:22 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2020-12-21T02:17:22Z</dc:date>
    <item>
      <title>Is it possible to interface two displays with MIPI interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-interface-two-displays-with-MIPI-interface/m-p/1201645#M166709</link>
      <description>&lt;P&gt;I am trying to interface 2 MIPI DSI displays with IMX8MM. But we are interfacing using MIPI Switcher connected over MIPI DSI interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to display the same image on both the LCDs how can I do that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please help us with the same.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Dec 2020 07:31:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-interface-two-displays-with-MIPI-interface/m-p/1201645#M166709</guid>
      <dc:creator>rajvikamdar</dc:creator>
      <dc:date>2020-12-18T07:31:51Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to interface two displays with MIPI interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-interface-two-displays-with-MIPI-interface/m-p/1202128#M166762</link>
      <description>&lt;P&gt;one can use the command like:&lt;/P&gt;
&lt;P&gt;"gplay-1.0 /unit_tests/test.mp4 --video-sink="kmssink driver-name=imx-dcss" &amp;amp; gplay-1.0 /unit_tests/test.mp4"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 02:17:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-it-possible-to-interface-two-displays-with-MIPI-interface/m-p/1202128#M166762</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2020-12-21T02:17:22Z</dc:date>
    </item>
  </channel>
</rss>