<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 WatchDog Issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/WatchDog-Issue/m-p/1200433#M166592</link>
    <description>&lt;P&gt;Im using&amp;nbsp;MCIMX6Y2CVM08AB processor where&amp;nbsp;GPIO1_IO08 is configured as&amp;nbsp;WDOG_B.&lt;/P&gt;&lt;P&gt;This signal is given to an AND gate which in turn controls the enable of the regulator.&lt;/P&gt;&lt;P&gt;During initial power up (just after production), the AND GATE output is held low because of the initial state of the watchdog.&lt;/P&gt;&lt;P&gt;Is there any solution for this?&lt;/P&gt;&lt;P&gt;Whether this signal will be high by default (without programming)?&lt;/P&gt;&lt;P&gt;Attached is the AND GATE section.&lt;/P&gt;</description>
    <pubDate>Wed, 16 Dec 2020 13:31:36 GMT</pubDate>
    <dc:creator>annie_varshitha</dc:creator>
    <dc:date>2020-12-16T13:31:36Z</dc:date>
    <item>
      <title>WatchDog Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WatchDog-Issue/m-p/1200433#M166592</link>
      <description>&lt;P&gt;Im using&amp;nbsp;MCIMX6Y2CVM08AB processor where&amp;nbsp;GPIO1_IO08 is configured as&amp;nbsp;WDOG_B.&lt;/P&gt;&lt;P&gt;This signal is given to an AND gate which in turn controls the enable of the regulator.&lt;/P&gt;&lt;P&gt;During initial power up (just after production), the AND GATE output is held low because of the initial state of the watchdog.&lt;/P&gt;&lt;P&gt;Is there any solution for this?&lt;/P&gt;&lt;P&gt;Whether this signal will be high by default (without programming)?&lt;/P&gt;&lt;P&gt;Attached is the AND GATE section.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Dec 2020 13:31:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WatchDog-Issue/m-p/1200433#M166592</guid>
      <dc:creator>annie_varshitha</dc:creator>
      <dc:date>2020-12-16T13:31:36Z</dc:date>
    </item>
    <item>
      <title>Re: WatchDog Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WatchDog-Issue/m-p/1200878#M166616</link>
      <description>&lt;P&gt;Hi annie_varshitha&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;in general pin state is described in Table 91. 14 x 14 mm Functional Contact Assignments&lt;/P&gt;
&lt;P&gt;column "Out of Reset Condition" and can not be changed.&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_2" href="https://www.nxp.com/docs/en/data-sheet/IMX6ULLCEC.pdf" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 6ULL Applications Processors for Consumer Products&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 04:03:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WatchDog-Issue/m-p/1200878#M166616</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-12-17T04:03:15Z</dc:date>
    </item>
    <item>
      <title>Re: WatchDog Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WatchDog-Issue/m-p/1201189#M166656</link>
      <description>&lt;P&gt;Could you elaborate on the below statements: when and how is it to be used ?&lt;/P&gt;&lt;P&gt;&amp;gt;WDOG1_ANY : Global WDOG signal&lt;/P&gt;&lt;P&gt;&amp;gt;WDOG1_B : This signal will power down the chip.&lt;/P&gt;&lt;P&gt;&amp;gt;WDOG1_RST_B_DEB : This signal is a reset source for the chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using GPIO1_IO08 as WDOG_B with ALT1 mux option.&lt;/P&gt;&lt;P&gt;But&amp;nbsp; the signal is low (from the processor) even after configuring it.&lt;/P&gt;&lt;P&gt;What would be the reason?&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 10:41:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WatchDog-Issue/m-p/1201189#M166656</guid>
      <dc:creator>annie_varshitha</dc:creator>
      <dc:date>2020-12-17T10:41:24Z</dc:date>
    </item>
    <item>
      <title>Re: WatchDog Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WatchDog-Issue/m-p/1201203#M166657</link>
      <description>&lt;P&gt;please refer to description in Chapter 59&amp;nbsp; Watchdog Timer (WDOG)&lt;/P&gt;
&lt;P&gt;&lt;A id="relatedDocsClick_1" href="https://www.nxp.com/webapp/Download?colCode=IMX6ULLRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;i.MX 6ULL Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;WDOG1_ANY is the global watchdog signal.&lt;/P&gt;
&lt;P&gt;It goes low if “any” of the WDOGx_B signals assert.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 12:07:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WatchDog-Issue/m-p/1201203#M166657</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-12-17T12:07:59Z</dc:date>
    </item>
  </channel>
</rss>