<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Enabling the FIELD_RETURN_LOCK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-the-FIELD-RETURN-LOCK/m-p/1199348#M166469</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/58158"&gt;@nemik&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; I've sent You some comments directly.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
    <pubDate>Tue, 15 Dec 2020 05:21:40 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2020-12-15T05:21:40Z</dc:date>
    <item>
      <title>Enabling the FIELD_RETURN_LOCK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-the-FIELD-RETURN-LOCK/m-p/1199053#M166440</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to enable the&amp;nbsp;FIELD_RETURN_LOCK bit in OCOTP_SW_STICKY register on my "closed" (fused) imx7dsabresd board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I verified that I can only unlock OCOTP features by flashing the bootloader to NAND, otherwise it does not work in SDP mode over USB. I verified this by enabling the SRK REVOKE which did work when flashed, but not over SDP.&lt;/P&gt;&lt;P&gt;However nothing I try seems to let me enable the FIELD_RETURN_LOCK bit as described here:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Known-Limitations-and-Guidelines/Field-Return-dependency-on-OCOTP-Module-clock-in-MPU-and-MCU/ta-p/1123766&amp;nbsp;I'm" target="_blank"&gt;https://community.nxp.com/t5/Known-Limitations-and-Guidelines/Field-Return-dependency-on-OCOTP-Module-clock-in-MPU-and-MCU/ta-p/1123766&amp;nbsp;I'm&lt;/A&gt; also not sure why I can't access that document now, but could a couple of weeks ago. There is a cached version here:&amp;nbsp;&lt;A href="https://webcache.googleusercontent.com/search?q=cache:kkLTvDfCjUsJ:https://community.nxp.com/t5/Known-Limitations-and-Guidelines/Field-Return-dependency-on-OCOTP-Module-clock-in-MPU-and-MCU/ta-p/1123766+&amp;amp;cd=1&amp;amp;hl=en&amp;amp;ct=clnk&amp;amp;gl=us" target="_blank"&gt;https://webcache.googleusercontent.com/search?q=cache:kkLTvDfCjUsJ:https://community.nxp.com/t5/Known-Limitations-and-Guidelines/Field-Return-dependency-on-OCOTP-Module-clock-in-MPU-and-MCU/ta-p/1123766+&amp;amp;cd=1&amp;amp;hl=en&amp;amp;ct=clnk&amp;amp;gl=us&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I test the&amp;nbsp;OCOTP_SW_STICKY using "md 0x303500B0 1" in U-Boot and always get&amp;nbsp;0x18 and did manage to get 0x1C when enabling SRK Revoke, but it did not enable FIELD_RETURN.&lt;/P&gt;&lt;P&gt;My board's UID is "000001266e48126a" and I see this running&lt;/P&gt;&lt;PRE&gt;$ cat /sys/fsl_otp/HW_OCOTP_TESTER0 &lt;BR /&gt;0x6e48126a&lt;BR /&gt;$ cat /sys/fsl_otp/HW_OCOTP_TESTER1 &lt;BR /&gt;0x126&lt;BR /&gt;&lt;BR /&gt;&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;and also when printing it from U-Boot using the tag_serialnr struct.&lt;/P&gt;&lt;P&gt;In my CSF file, I am adding:&lt;/P&gt;&lt;PRE&gt;[Unlock]&lt;BR /&gt;Engine = OCOTP&lt;BR /&gt;Features = FIELD RETURN, SRK REVOKE&lt;BR /&gt;UID = 0x00, 0x00, 0x26, 0x01, 0x48, 0x6e, 0x6a, 0x12&lt;/PRE&gt;&lt;P&gt;and different combinations of the UID but can't seem to turn off the FIELD_RETURN sticky bit.&lt;/P&gt;&lt;P&gt;Any help is appreciated. Thank you,&lt;/P&gt;&lt;P&gt;Nemanja Stefanović&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 16:21:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-the-FIELD-RETURN-LOCK/m-p/1199053#M166440</guid>
      <dc:creator>nemik</dc:creator>
      <dc:date>2020-12-14T16:21:26Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling the FIELD_RETURN_LOCK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-the-FIELD-RETURN-LOCK/m-p/1199348#M166469</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/58158"&gt;@nemik&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; I've sent You some comments directly.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Yuri.&lt;/P&gt;</description>
      <pubDate>Tue, 15 Dec 2020 05:21:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-the-FIELD-RETURN-LOCK/m-p/1199348#M166469</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2020-12-15T05:21:40Z</dc:date>
    </item>
  </channel>
</rss>